Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The following sections list all CAD systems (for which currently interfaces are available) in alphabetical order with their respective commands/menu items.
Every CAD section is built up as follows:
Preceded you see a matrix which shows the available functions for each interface.
The next table shows the respective legend.
Tooltip | ||
![]() |
PARTdataManager start and transferring 3D parts from PARTsolutions to the CAD system. |
|
![]() |
PARTdataManager start and transferring 2D parts from PARTsolutions to the CAD system. |
|
![]() |
||
![]() |
Seamless integration of the PARTsolutions standard and supplier parts library |
|
![]() |
||
![]() |
||
![]() |
||
![]() |
Connection dialog section in PARTdataManager is opened Hidden by default. Information on UI design can be found under Section 2.2.1.6, “Configuring PARTsolutions interface menu and toolbar ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual. |
Tooltip | ||
![]() |
||
![]() |
||
![]() |
Explicitly release PARTsolutions export license (only relevant at Floating licensing). |
|
![]() |
Call PARTadmin in order to perform changes of the interface configuration file |
|
![]() |
Event handling |
Special settings concerning LIVEsearch. See Section 2.6.10, “ LIVEsearch ” -> "Automatischer Aufruf der LIVEsearch" |
Tooltip | ||
![]() |
||
![]() |
Execute Partial Search | Seamless is started and a Partial search is executed. |
![]() |
Search for unmachined parts |
Find unmachined parts for the production of finished parts or finished parts which can be produced from a certain unmachined part. Hidden by default. Information on UI design can be found under Section 2.2.1.6, “Configuring PARTsolutions interface menu and toolbar ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual. |
![]() |
Topology search |
Hidden by default. Information on UI design can be found under Section 2.2.1.6, “Configuring PARTsolutions interface menu and toolbar ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual. |
![]() |
Toggle LIVEsearch | In enabled state, no search is running in background. However, Display LIVEsearch results can be called manually anytime. |
![]() |
Display LIVEsearch results | The results of LIVEsearch are shown for a moment |
![]() |
Note |
---|---|
You can adjust which functions should be displayed in menu and toolbar. Information on this are found under Section 2.2.1.6, “Configuring PARTsolutions interface menu and toolbar ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual. |