Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Possibly it may happen that parts cannot be displayed in ArchiCAD. This is mostly due to mesh errors.
When exporting in mesh format you can select a simplified depiction. This is robust against mesh errors.[3]
You can determine this behaviour via configuration file in general:
[CreationOptions] ForcePlaneBasedMesh=0/1
When exporting with simplified depiction the quality of roundings is worse.[4]
[3] The simplified depiction is not using rounds. The mesh generation is quicker then. If „ForcePlaneBasedMesh“ is not set, the better depiction is used. Then generation is more time consuming. If an error occurs with the better depiction, normally it is intercepted and the simplified depiction is automatically used. Possibly ArchiCAD is not able to draw the object, nevertheless. If the simplified depiction shall be chosen in general, then you can set the key „ForcePlaneBasedMesh“ to 1.
[4] Differentiated color depiction is only possible for mesh based parts. Otherwise only single features such as cylinder, cone, etc. can be colorized.