![]() |
In order to activate the Medusa interface proceed as follows:
Under
..\Medusa\Master_project\product_list.dat
the path of the interface has to be stated.
E.g.:
C:\Programme\cadenas\partsolutions\software\iface\medusa
In a DOS
console the file startmedconfig.bat
with
the parameter -admin
has to be executed.
The file is also found under ..\Medusa\Master_project
.
--> The MEDUSA 5.0.1 configuration service program opens.
In the course of the configuration default values are displayed, which you can adjust (if desired) or confirm via [Return].
In MEDUSA, under View -> Toolbars select the menu item Complete.