Common PARTsolutions configuration files
Settings for the 2D view in PARTdataManager
Details on this can be found under Abschnitt 5.11.3, „2D-Ableitung: eigene Kombinationsansichten (*.dw) erstellen“ in eCATALOGsolutions - Handbuch.
DIN 962 controls how screws and nuts can be adjusted for certain use cases through additional forms and information.
material.cfg (without ERP integration)
Client settings of the PARTapplication Server. See Abschnitt 1.3.9.9.2, „AppServer Client: Konfiguration“.
Server settings of the PARTapplication Server. See Abschnitt 1.3.9.9.3, „AppServer Service: Konfiguration“.
Settings for all PARTsolutions modules, especially PARTdataManager GUI settings
Configuration files for CAD interfaces
CAD specific
configuration files if<cadname>.cfg
and
ifacecommon.cfg
.
See Kapitel 2, PARTsolutions
- CAD Integration - Administration.
Configuration files for ERP integration
Common ERP settings. In the user interface you can find most of the setting options under PARTlinkManager -> Extras menu -> Configure ERP environment.
To see the features embedded into the context of Strategic Parts Management please see Kapitel 4, Strategisches Teilemanagement.
Contains groups (syn. roles) of the single users. In the user interface you can find most of the setting options in the Category tree under Roles.
To see the features embedded into the context of Strategic Parts Management please see Kapitel 4, Strategisches Teilemanagement.
Contains the created users. In the user interface you can find the corresponding settings in the Category tree under User.
To see the features embedded into the context of Strategic Parts Management please see Kapitel 4, Strategisches Teilemanagement.
The configuration file erpcustom.cfg
is used in order
to further customize ERP processing. For example, one important setting
is for the user dialog when adding datasets to the LinkDB.
material_assign.cfg (with ERP integration)
Material specifications for export
See Abschnitt 4.10.1, „material_assign.cfg (mit ERP-Kopplung)“.
Used to establish the nightly transfer of third party system information to PARTsolutions.
Contains settings for Export tables (PARTlinkManager -> Extras menu -> Configure ERP environment -> Export tables tabbed page).
Contains basic settings on Update manager, which normally don't have to be changed. For details on Update manager please see Abschnitt 4.16.3, „Katalogupdate mit ERP-Kopplung - Zuweisungsprobleme mit Update Manager beheben“.
For the database connection data, i.e. Server, Database, in particular the driver class and the URL for the jdbc driver to establish a connection to the database.