![]() |
4.2.7. ERP-Anbindung
aus PARTsolutions via ODBC/JDBC und ERP-Aktivierung
4.2.7.1. dbproxy.cfg
|
|
---|---|
Zurück | Weiter |
![]() |
Hinweis |
---|---|
The
configuration file |
In this file you can specify the ODBC or JDBC database interface for each used operating system.
The driver
selection during the PARTsolutions setup (Database connection selection) results in a
setting in dbproxy.cfg
.
If for testing purposes or by mistake a wrong driver has been selected, set the correct driver in the configuration file or in the corresponding user interface.
Under PARTadmin -> Category PARTsolutions -> ERP environment, in the Database interface dialog area, you can make settings easily via user interface:
Either you determine ODBC or JDBC specifically for each operating system. Or you determine the default interface and then refer to the selection <default> in the list field.
Setting via configuration file:
[COMMON] Driver=DATABASE.ODBCDB [x86] Driver=DATABASE.JDBCDB [Linux] Driver=DATABASE.ODBCDB [AIX] Driver=DATABASE.JDBCDB
Either you determine ODBC or JDBC specifically for each operating system or the one specified in the block [Common] is taken.
Zurück | Nach oben | Weiter |
4.2.7. ERP-Anbindung aus PARTsolutions via ODBC/JDBC und ERP-Aktivierung | Zum Anfang | 4.2.7.2. plinkcommon.cfg -> Block [Common] -> Key "DBName" - Determine ODBC data source name in PARTsolutions |