A bed is a piece of furniture which is used as a place to sleep or relax.
Most modern beds consist of a soft, cushioned mattress on a bed frame, the mattress resting either on a solid base, often wood slats, or a sprung base. Many beds include a box spring inner-sprung base, which is a large mattress-sized box containing wood and springs that provide additional support and suspension for the mattress. Beds are available in many sizes, ranging from infant-sized bassinets and cribs, to small beds for a single child or adult, to large queen and king-size beds designed for two adults. While most beds are single mattresses on a fixed frame, there are other varieties, such as the murphy bed, which folds into a wall, the sofa bed, which folds out of a sofa, and the bunk bed, which provides two mattresses on two tiers. Temporary beds include the inflatable air mattress and the folding camp cot. Some beds contain neither a padded mattress nor a bed frame, such as the hammock, which is considered one of the most comfortable places to rest while swaying side to side. Some beds are made especially for animals.
Beds may have a headboard for resting against, and may have side rails and footboards (or "footers"). "Headboard only" beds may incorporate a "dust ruffle", "bed skirt", or "valance sheet" to hide the bed frame. To support the head, a pillow made of a soft, padded material is usually placed on the top of the mattress. Some form of covering blanket is often used to insulate the sleeper, often bed sheets, a quilt, or a duvet, collectively referred to as bedding. Bedding is the removable non-furniture portion of a bed, which enables these components to be washed or aired out.