powered by CADENAS

Social Share

Luthier (3273 views - Music)

A luthier ( LOO-ti-ər) is someone who builds or repairs string instruments generally consisting of a neck and a sound box. The word "luthier" comes from the French word luth, which means lute. A luthier was originally a maker of lutes, but the term now includes makers of stringed instruments such as the violin or classical guitar. A luthier does not make harps or pianos, as these require different skills and construction methods because their strings are secured to a frame. The craft of making string instruments, or lutherie (sometimes spelled luthiery), is commonly divided into two main categories: makers of stringed instruments that are plucked or strummed, and those that are bowed. Since bowed instruments require a bow, the second category includes a subtype known as a bow maker or archetier. Luthiers may also teach string-instrument making, either through apprenticeship or formal classroom instruction.
Go to Article

Explanation by Hotspot Model

Luthier

Luthier

Luthier
Luthier
Modern luthier's workshop, Cremona (2007)
Occupation
Instrument maker

A luthier (/ˈltiər/ LOO-ti-ər)[1] is someone who builds or repairs string instruments generally consisting of a neck and a sound box. The word "luthier" comes from the French word luth, which means lute. A luthier was originally a maker of lutes, but the term now includes makers of stringed instruments such as the violin or classical guitar. A luthier does not make harps or pianos, as these require different skills and construction methods because their strings are secured to a frame.

The craft of making string instruments, or lutherie (sometimes spelled luthiery), is commonly divided into two main categories: makers of stringed instruments that are plucked or strummed, and those that are bowed.[2] Since bowed instruments require a bow, the second category includes a subtype known as a bow maker or archetier. Luthiers may also teach string-instrument making, either through apprenticeship or formal classroom instruction.

Plucked strings

Lutes

Important luthiers who specialized in the instruments of the lute family (lutes, archlutes, theorbos, vihuelas, etc.):

and in modern times:

Guitars

Two important luthiers of the early 19th century connected with the development of the modern classical guitar are Louis Panormo and Georg Staufer.[3] Antonio Torres Jurado is credited with developing the form of classical guitar still in use today. Christian Frederick Martin of Germany developed a form that evolved into the modern steel-string acoustic guitar.

The American luthier Orville Gibson specialized in mandolins, and is credited with creating the archtop guitar. The important 20th-century American luthiers John D'Angelico and Jimmy D'Aquisto made archtop guitars. Lloyd Loar worked briefly for the Gibson Guitar Corporation making mandolins and guitars. His designs for a family of arch top instruments (mandolin, mandola, guitar, et cetera) are held in high esteem by today's luthiers, who seek to reproduce their sound. Paul Bigsby's innovation of the tremolo arm for archtop and electric guitars is still in use today and may have influenced Leo Fender's design for the Stratocaster solid-body electric guitar, as well as the Jaguar and Jazzmaster. Concurrent with Fender's work, guitarist Les Paul independently developed a solid-body electric guitar. These were the first fretted, solid-body electric guitars—though they were preceded by the cast aluminum "frying pan", a solid-body electric lap steel guitar developed and eventually patented by George Beauchamp, and built by Adolph Rickenbacher.[4] A company founded by luthier Friedrich Gretsch and continued by his son and grandson, Fred and Fred, Jr., originally made banjos, but is more famous today for its electric guitars. Vintage guitars are often sought by collectors.

Bowed strings

Bowed instruments include: cello, crwth, double bass, erhu, fiddle, hudok, mouthbow, nyckelharpa, hurdy-gurdy, rabab, rebec, sarangi, viol (viola da gamba), viola, viola da braccio, viola d'amore, and violin.

The purported "inventor" of the violin is Andrea Amati. Amati was originally a lute maker, but turned to the new instrument form of violin in the mid-16th century. He was the progenitor of the famous Amati family of luthiers active in Cremona, Italy until the 18th century. Andrea Amati had two sons. His eldest was Antonio Amati (circa 1537–1607), and the younger, Girolamo Amati (circa 1561–1630). Girolamo is better known as Hieronymus, and together with his brother, produced many violins with labels inside the instrument reading "A&H". Antonio died having no known offspring, but Hieronymus became a father. His son Nicolò (1596–1684) was himself an important master luthier who had several apprentices of note, including Antonio Stradivari[5] (probably), Andrea Guarneri, Bartolomeo Pasta, Jacob Railich, Giovanni Battista Rogeri, Matthias Klotz, and possibly Jacob Stainer. It is even possible Bartolomeo Cristofori, later inventor of the piano, apprenticed under him (although census data does not support this, which paints this as a possible myth).[6]

Gasparo da Salò of Brescia (Italy) was another important early luthier of the violin family. About 80 of his instruments survive, and around 100 documents that relate to his work. He was also a double bass player and son and nephew of two violin players: Francesco and Agosti, respectively.

Gasparo Duiffopruggar of Füssen, Germany, was once incorrectly credited as the inventor of the violin. He was likely an important maker, but no documentation survives, and no instruments survive that experts unequivocally know are his.

Da Salò made many instruments and exported to France and Spain, and probably to England. He had at least five apprentices: his son Francesco, a helper named Battista, Alexander of Marsiglia, Giacomo Lafranchini and—the most important—Giovanni Paolo Maggini. Maggini inherited da Salò's business in Brescia. Valentino Siani worked with Maggini. In 1620, Maggini moved to Florence.

Luthiers born in the mid-17th century include Giovanni Grancino, Carlo Giuseppe Testore, and his sons Carlo Antonio Testore and Paolo Antonio Testore, all from Milan. From Venice[7] the luthiers Matteo Goffriller, Domenico Montagnana, Sanctus Seraphin, and Carlo Annibale Tononi were principals in the Venetian school of violin making (although the latter began his career in Bologna).[8] The Bergonzi family (pt) of luthiers were the successors to the Amati family in Cremona. David Tecchler, who was born in Austria, later worked in both Venice and Rome.

Important luthiers from the early 18th century include Nicolò Gagliano of Naples, Italy, Carlo Ferdinando Landolfi of Milan, and Giovanni Battista Guadagnini, who roamed throughout Italy during his lifetime. From Austria originally, Leopold Widhalm later established himself in Nürnberg, Germany.

The early 19th-century luthiers of the Mirecourt school of violin making in France were the Vuillaume family, Charles Jean Baptiste Collin-Mezin, and Collin-Mezin's son, Charles Collin-Mezin, Jr., Honore Derazey, Nicolas Lupot, Charles Macoutel, Charles Mennégand, and Pierre Silvestre. Nicola Utili (also known as Nicola da Castel Bolognese) (Ravenna, Italy, March 1888 – May 1962), beside traditional lute works, experimented the making of "pear-shaped" violins.

The Jérôme-Thibouville-Lamy firm started making wind instruments around 1730 at La Couture-Boussey, then moved to Mirecourt around 1760 and started making violins, guitars, mandolins, and musical accessories.

See also



This article uses material from the Wikipedia article "Luthier", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Music

3d,printed,3dprinting,3dprint,music,song,dvd,dcrom,schellak,top hit