powered by CADENAS

Social Share

Harp (4976 views - Music)

The harp is a stringed musical instrument that has a number of individual strings running at an angle to its soundboard; the strings are plucked with the fingers. Harps have been known since antiquity in Asia, Africa and Europe, dating back at least as early as 3500 BC. The instrument had great popularity in Europe during the Middle Ages and Renaissance, where it evolved into a wide range of variants with new technologies, and was disseminated to Europe's colonies, finding particular popularity in Latin America. Although some ancient members of the harp family died out in the Near East and South Asia, descendants of early harps are still played in Myanmar and parts of Africa, and other defunct variants in Europe and Asia have been utilized by musicians in the modern era. Harps vary globally in many ways. In terms of size, many smaller harps can be played on the lap, whereas larger harps are quite heavy and rest on the floor. Different harps may use strings of catgut, nylon, metal, or some combination. While all harps have a neck, resonator, and strings, frame harps have a pillar at their long end to support the strings, while open harps, such as arch harps and bow harps, do not. Modern harps also vary in techniques used to extend the range and chromaticism (e.g., adding sharps and flats) of the strings, such as adjusting a string's note mid-performance with levers or pedals which modify the pitch. The pedal harp is a standard instrument in the orchestra of the Romantic music era (ca. 1800-1910) and the contemporary music era.
Go to Article

Explanation by Hotspot Model

Harp

Harp

Harp

Harp
A medieval harp (left) and a single-action pedal harp (right)
String instrument
Hornbostel–Sachs classification 322–5
(Composite chordophone sounded by the bare fingers)
Playing range

Related instruments

The harp is a stringed musical instrument that has a number of individual strings running at an angle to its soundboard; the strings are plucked with the fingers. Harps have been known since antiquity in Asia, Africa and Europe, dating back at least as early as 3500 BC. The instrument had great popularity in Europe during the Middle Ages and Renaissance, where it evolved into a wide range of variants with new technologies, and was disseminated to Europe's colonies, finding particular popularity in Latin America. Although some ancient members of the harp family died out in the Near East and South Asia, descendants of early harps are still played in Myanmar and parts of Africa, and other defunct variants in Europe and Asia have been utilized by musicians in the modern era.

Harps vary globally in many ways. In terms of size, many smaller harps can be played on the lap, whereas larger harps are quite heavy and rest on the floor. Different harps may use strings of catgut, nylon, metal, or some combination. While all harps have a neck, resonator, and strings, frame harps have a pillar at their long end to support the strings, while open harps, such as arch harps and bow harps, do not. Modern harps also vary in techniques used to extend the range and chromaticism (e.g., adding sharps and flats) of the strings, such as adjusting a string's note mid-performance with levers or pedals which modify the pitch. The pedal harp is a standard instrument in the orchestra of the Romantic music era (ca. 1800-1910) and the contemporary music era.

Origin

Near East

1A Sassanid era mosaic excavated at Bishapur

The earliest harps and lyres were found in Sumer, 3500 BC,[2] and several harps were found in burial pits and royal tombs in Ur.[3] The oldest depictions of harps without a forepillar can be seen adjacent to the Near East, in the wall paintings of ancient Egyptian tombs in the Nile Valley, which date from as early as 3000 BC. These murals show an instrument that closely resembles the hunter's bow, without the pillar that we find in modern harps. [4] The chang flourished in Persia in many forms from its introduction, about 3000 BC, until the 17th century.

Around 1900 BC arched harps in the Iraq–Iran region were replaced by angular harps with vertical or horizontal sound boxes.[5] By the start of the Common Era, "robust, vertical, angular harps", which had become predominant in the Hellenistic world, were cherished in the Sasanian court. In the last century of the Sasanian period, angular harps were redesigned to make them as light as possible ("light, vertical, angular harps"); while they became more elegant, they lost their structural rigidity. At the height of the Persian tradition of illustrated book production (AD 1300–1600), such light harps were still frequently depicted, although their use as musical instruments was reaching its end.[6]

South Asia

The works of the Tamil Sangam literature describe the harp and its variants, as early as 200 BC.[7] Variants were described ranging from 14 to 17 strings, and the instrument used by wandering minstrels for accompaniment.[8] Iconographic evidence in of the yaal appears in temple statues dated as early as 500 BC[citation needed] One of the Sangam works, the Kallaadam recounts how the first yaaḻ harp was inspired by an archer's bow, when he heard the musical sound of its twang.[citation needed]

Another early South Asian harp was the ancient veena; unlike the modern instrument of the same name, the ancient veena was a harp vice the modern lute-type instrument. Some Samudragupta gold coins show of the mid-4th century AD show (presumably) the king Samudragupta himself playing the instrument.[9] The ancient veena survives today in Burma, in the form of the saung harp still played there.[10]

East Asia

The harp was popular in ancient China and neighboring regions, though harps are largely extinct in East Asia in the modern day. The Chinese konghou harp is documented as early as the Spring and Autumn period (770–476 BC), and became extinct during the Ming Dynasty (AD 1368–1644).[citation needed] A similar harp, the gonghu was played in ancient Korea, documented as early as the Goguryeo period (37 BC – AD 686).[11]

Structure and mechanism

Harps are essentially triangular in shape, and are made primarily of wood. Harp strings are made of gut (often replaced in the modern day by nylon) or metal. The top end of each string is secured on the crossbar or neck of the instrument, where each will have a tuning peg or similar device to adjust the pitch of that string.

From the crossbar, the string runs down to the sounding board on the resonating body, where it is secured with a knot; in modern instruments the string's hole is protected with an eyelet to limit wear on the wood. It is the distance between the tuning peg and the soundboard, as well as the tension and weight of the string, which decide the pitch of the string. The body is hollow and when a taut string is plucked, the body resonates, projecting sound.

The longest side of the harp is called the column or pillar, though some earlier harps, such as a "bow harp", lack a pillar entirely. On most harps, the sole purpose of the pillar is to hold up the neck against the great strain of the strings. On harps which have pedals (largely the modern concert harp), the pillar is a hollow column and encloses the rods which adjust the pitch of strings, which are levered by pressing pedals at the base of the instrument.

On harps of earlier design, a given string can play only a single note without retuning the string. In many cases this means that such a harp can only play in one key at a time, and must be manually retuned to play in another key. Various remedies to this limitation evolved: the addition of extra strings to cover chromatic notes (sometimes in separate or angled rows distinct from the main row of strings), the addition of small levers on the crossbar which when actuated raise the pitch of a string by a set interval (usually a semitone), or the use of pedals at the base of the instrument which change the pitch of a string when pressed with the foot. These solutions increase the flexibility of a harp, at the cost of adding complexity, weight, and expense.

Development and history

Europe

While the angle and bow harps held popularity elsewhere, European harps favored the "pillar", a third structural member to support the far ends of the arch and sound box.[12][13][14] A harp with a triangular three-part frame is depicted on 8th-century Pictish stones in Scotland[12][13] and in manuscripts (e.g. the Utrecht Psalter) from the early 9th-century France.[14] The curve of the harp's neck is a result of the proportional shortening of the basic triangular form to keep the strings equidistant; if the strings were proportionately distanced, the strings would be farther apart.

As European harps evolved to play more complex music, a key consideration was some way to facilitate the quick changing of a string's pitch to be able to play more chromatic notes. By the Baroque period, in Italy and Spain, more strings were added to allow for chromatic notes in more complex harps. In Germany in the second half of the 17th century, diatonic single-row harps were fitted with manually turned hooks which fretted individual strings to raise their pitch by a half step. In the 18th century, a link mechanism was developed connecting these hooks with pedals, leading to the invention of the single-action pedal harp.

The first primitive form of pedal harps was developed in the Tyrol region of Austria. Jacob Hochbrucker was the next to design an improved pedal mechanism, around 1720, followed in succession by Krumpholtz, Nadermann, and the Erard company, who came up with the double mechanism, in which a second row of hooks was installed along the neck, capable of raising the pitch of a string by either one or two half steps. While one course of European harps led to greater complexity, resulting largely in the modern pedal harp, other harping traditions maintained simpler diatonic instruments which survived and evolved into modern traditions.

Americas

In the Americas, harps are widely but sparsely distributed, except in certain regions where the harp traditions are very strong. Such important centres include Mexico, the Andean region, Venezuela and Paraguay. They are derived from the Baroque harps that were brought from Spain during the colonial period.[15] Detailed features vary from place to place.

The Paraguayan harp is that country's national instrument, and has gained a worldwide reputation, with international influences alongside folk traditions. Paraguayan harps have around 36 strings, played with the fingernails, and with a narrowing spacing and lower tension than modern Western harps, and have a wide and deep soundbox which tapers to the top.[16]

The harp is also found in Argentina,[17] though in Uruguay it was largely displaced in religious music by the organ by the end of the 18th century.[18] The harp is historically found in Brazil, but mostly in the south of the country.[19]

The Andean harp (Quechua: arpa), also known as Peruan harp or indigenous harp is widespread among peoples living in highlands of the Andes: Quechua and Aymara, mainly in Peru, and also in Bolivia and Ecuador. Andean harp has relatively large size. Its distinguishing feature is significantly increased volume of the resonator box, which gives basses a special richness. Andean harp usually accompanies love dances and songs, such as huayno.[20] One of the most famous performers on the Andean harp was Juan Cayambe (Pimampiro Canton, Imbabura Province, Ecuador[21])

Mexican "jarocha" harp music of Veracruz has also gained some international recognition, evident in the popularity of "la bamba".[original research?] In southern Mexico (Chiapas), there is a very different indigenous style of harp music.[22]

In Venezuela, there are two distinct traditions, the arpa llanera and the arpa central (or arpa mirandina). The modern Venezuelan arpa llanera has 32 strings of nylon (originally, gut). The arpa central is strung with wire in the higher register.[23]

Africa

A number of types of harps are found in Africa, predominantly not of the three-sided frame-harp type found in Europe. A number of these, referred to generically as African harps, are bow or angle harps, which lack forepillars joining the neck to the body.

A number of harp-like instruments in Africa are not easily classified with European categories. Instruments like the West African kora and Mauritanian ardin are sometimes labeled as "spike harp", "bridge harp", or harp lute since their construction includes a bridge which holds the strings laterally, vice vertically entering the soundboard.[24]

South and Southwest Asia

While lyres and zithers have persisted in the Middle East, most of the true harps of the region have become extinct, though some are undergoing initial revivals. The Turkish çeng was a nine-string harp in the Ottoman Empire which became extinct at the end of the 17th century,[25] but has undergone some revival and evolution since the late 20th century. A similar harp, the changi survives in the Svaneti region of Georgia.[26]

In the remote and mountainous Nuristan province of Afghanistan the Kafir harp has been part of the musical traditional for many years.[27] In India, the bin-baia harp survives about the Padhar people of Madhya Pradesh.[26]

East Asia

Saung musician in 1900.

The harp largely became extinct in East Asia by the 17th century; around the year 1000 harps like the vajra began to replace preceding[clarification needed] harps.[28] A few examples survived to the modern era, particularly Burma's saung-gauk, which is considered the national instrument in that country. Though the ancient Chinese konghou has not been directly resurrected, the name has been revived and applied to a modern newly invented instrument based on the Western classical harp, but with the strings doubled back to form two notes per string, allowing advanced techniques such as note-bending.[citation needed]

Modern European and American harps

Concert harp

The pedal or concert harp is a technologically advanced instrument, particularly distinguished by its use of "pedals", foot-controlled devices which can alter the pitch of given strings, making the instrument fully chromatic and thus able to play a wide body of classical repertoire. Pedals were first introduced in 1697 by Jakob Hochbrucker of Bavaria.[29] In 1811 these were upgraded to the "double action" pedal system patented by Sébastien Erard.[30][citation needed]

The addition of pedals broadened the harp's abilities, allowing its gradual entry into the classical orchestra, largely beginning in the 19th century. The harp played little or no role in early classical music (being used only a handful of times by such as Mozart or Beethoven), and its usage by Cesar Franck in his Symphony in D minor (1888) was described as "revolutionary" despite some body of prior classical usage.[31] Entering the 20th century, the pedal harp found use outside of classical music, entering jazz with Casper Reardon,[when?] the Beatles 1967 "She's Leaving Home", and several works by Björk which featured harpist Zeena Parkins.

Folk, lever, and Celtic instruments

In the modern era, there is a family of mid-size harps, generally with nylon strings, and optionally with partial or full levers but without pedals. They range from two to six octaves, and are plucked with the fingers using a similar technique to the pedal harp. Though these harps evoke ties to historical European harps, their specifics are modern, and they are frequently referred to broadly as "Celtic" harps due to their region of revival and popular association, or more generically as "folk" harps due to their use in non-classical music, or as "lever" harps to contrast their modifying mechanism with the larger pedal harp.[32]

The modern Celtic harp began to appear in the early 19th century in Ireland, contemporary with the dying out of earlier forms of Gaelic harp. Dublin pedal harp maker John Egan developed a new type of harp which had gut strings and semitone mechanisms like an orchestral pedal harp; it was small and curved like the historical cláirseach or Irish harp, but its strings were of gut and the soundbox was much lighter.[33] In the 1890s a similar new harp was also developed in Scotland as part of a Gaelic cultural revival.[34] In the mid-20th century Jord Cochevelou developed a variant of the modern Celtic harp which he referred to as the "Breton Celtic harp"; his son Alan Stivell was to become the most influential Breton harper, and a strong influence in the broader world of the Celtic harp.

Multi-course harps

A multi-course harp is a harp with more than one row of strings, as opposed to the more common "single course" harp. On a double-harp, the two rows generally run parallel to each other, one on either side of the neck, and are usually both diatonic (sometimes with levers) with identical notes.

The triple harp originated in Italy in the 16th century, and arrived in Wales in the late 17th century where it established itself in the local tradition as the Welsh harp (telyn deires, "three-row harp").[35] The triple consists of two outer rows of identical diatonic strings with a third set of chromatic strings between them. These strings are off set to permit the harpist to reach past the outer row and pluck an inner string if a chromatic note is needed.

Chromatic-strung harps

Some harps, rather than using pedal or lever devices, achieve chromaticity by simply adding additional strings to cover the notes outside their diatonic home scale. The Welsh triple harp is one such instrument, and two other instruments employing this technique are the cross-strung harp and the inline chromatic harp.

The cross-strung harp has one row of diatonic strings, and a separate row of chromatic notes, angled in an "X" shape so that the row which can be played by the right hand at the top may be played by the left hand at the bottom, and vice versa. This variant was first attested as the arpa de dos órdenes ("two-row harp") in Spain and Portugal, in the 17th century.[36]

The inline chromatic harp is generally a single-course harp with all 12 notes of the chromatic scale appearing in a single row. Single course inline chromatic harps have been produced at least since 1902, when Karl Weigel of Hanover patented a model of inline chromatic harp.[37]

Modern electric harps

Amplified (electro-acoustic) hollow body and solid body electric lever harps are produced by many harpmakers at this time, such as Lyon and Healy Harps out of Chicago, Salvi Harps out of Italy, and Camac Harps out of France. They generally use individual piezo-electric transducers one per string often in combination with small internal microphones to produce a direct output mixed electrical signal. Hollow body instruments can also be played acoustically, while solid body instruments must be amplified. The late-20th century gravikord is a modern purpose-built electric double harp made of stainless steel based on the traditional West African kora.

Terminology and etymology

The modern English word harp comes from the Old English hearpe; akin to Old High German harpha.[38]

A number of non-harp-like instruments are colloquially referred to as "harps". Chordophones like the aeolian harp (wind harp) and the autoharp (with the piano and harpsichord) are not harps, but zithers, because their strings are not perpendicular to their soundboard. Similarly, the many varieties of harp guitar and harp lute, while chordophones, belong to the lute family and are not true harps. All forms of the lyre and kithara are also not harps, but belong to the fourth family of ancient instruments under the chordophones, the lyres.

The term "harp" has also been applied to many instruments which are not chordophones. The vibraphone was (and is still) sometimes referred to as the "vibraharp," though it has no strings and its sound is produced by striking metal bars. In blues music, the harmonica is often casually referred to as a "blues harp" or "harp", but it is a free reed wind instrument, not a stringed instrument, and is therefore not a true harp. The Jew's harp is neither Jewish nor a harp; it is a plucked idiophone and likewise not a stringed instrument. The laser harp is not a stringed instrument at all, but is a harp-shaped synthesized electronic instrument that has laser beams where harps have strings.

As a symbol

Political

Ireland

The harp has been used as a political symbol of Ireland for centuries. Its origin is unknown but from the evidence of the ancient oral and written literature, it has been present in one form or another since at least the 6th century or before. According to tradition, Brian Boru, 'High King' of Ireland (died at the Battle of Clontarf, 1014) played the harp, as did many of the gentry in the country during the period of the Gaelic Lordship of Ireland (ended c. 1607 with the "Flight of the Earls" following the Elizabethan Wars).[citation needed]

In traditional Gaelic society every clan and chief of any consequence would have a resident harp player who would compose eulogies and elegies (later known as "planxties") in honour of the leader and chief men of the clan. The harp was adopted as a symbol of the Kingdom of Ireland on the coinage from 1542, and in the Royal Standard of King James VI and I in 1603 and continued to feature on all English and United Kingdom Royal Standards ever since, though the styles of the harps depicted differed in some respects. It was also used on the Commonwealth Jack of Oliver Cromwell, issued in 1649 and on the Protectorate Jack issued in 1658 as well as on the Lord Protector's Standard issued on the succession of Richard Cromwell in 1658. The harp is also traditionally used on the flag of Leinster.

Since 1922, the government of Ireland has used a similar left-facing harp, based on the Trinity College Harp in the Library of Trinity College Dublin as its state symbol. It first appeared on the Great Seal of the Irish Free State, which in turn was replaced by the coat of arms, the Irish Presidential Standard and the Presidential Seal in the 1937 Constitution of Ireland. The harp emblem is used on official state seals and documents including the Irish passport and has appeared on Irish coinage from the Middle Ages to the current Irish imprints of euro coins. Guinness since 1759, Harp Lager since 1960, Irish Independent since 1961 originally in black but in green since 1972 and Ryanair since 1985.

Elsewhere

St. Maria (Weingarten/Württemberg)

The South Asian Tamil harp yaal is the symbol of City of Jaffna, Sri Lanka, whose legendary root originates from a harp player.[39]

Religious

In the context of Christianity, heaven is sometimes symbolically depicted as populated by angels playing harps, giving the instrument associations of the sacred and heavenly. In the Bible, Genesis 4:21 says that Jubal, the first musician and son of Lamech, invented the harp and flute.[40][41]

Many depictions of King David in Jewish art have him holding or playing a harp, such as a sculpture outside King David's tomb in Jerusalem, Israel.

Corporate

The harp is also used extensively as a corporate logo — for both private company and government organisations. The Irish beer Guinness uses a harp, facing right and less detailed than the version used on the state arms. Relatively new organisations also use the harp, but often modified to reflect a theme relevant to their organisation: Irish airline Ryanair uses a modified harp, and the Irish State Examinations Commission uses it with an educational theme. The harp appears in the logo for League of Ireland football team Finn Harps F.C., Donegal's senior soccer club.

Other organisations in Ireland use the harp, but not always prominently; these include the National University of Ireland and the associated University College Dublin, and the Gaelic Athletic Association. In Northern Ireland the Police Service of Northern Ireland and Queen's University of Belfast use the harp as part of their identity.

In Iraq, the football club Al-Shorta is nicknamed Al-Qeetharah (Assyrian Neo-Aramaic: "the harp"‎), and has a harp on its logo.

See also



This article uses material from the Wikipedia article "Harp", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Music

3d,printed,3dprinting,3dprint,music,song,dvd,dcrom,schellak,top hit