powered by CADENAS

Social Share

Beer (9624 views - Basics)

Beer is the world's oldest and most widely consumed alcoholic drink; it is the third most popular drink overall, after water and tea. The production of beer is called brewing, which involves the fermentation of sugars, mainly derived from cereal grain starches—most commonly from malted barley, although wheat, maize (corn), and rice are widely used. Most beer is flavoured with hops, which add bitterness and act as a natural preservative, though other flavourings such as herbs or fruit may occasionally be included. The fermentation process causes a natural carbonation effect, although this is often removed during processing, and replaced with forced carbonation. Some of humanity's earliest known writings refer to the production and distribution of beer: the Code of Hammurabi included laws regulating beer and beer parlours, and "The Hymn to Ninkasi", a prayer to the Mesopotamian goddess of beer, served as both a prayer and as a method of remembering the recipe for beer in a culture with few literate people. Beer is sold in bottles and cans; it may also be available on draught, particularly in pubs and bars. The brewing industry is a global business, consisting of several dominant multinational companies and many thousands of smaller producers ranging from brewpubs to regional breweries. The strength of beer is usually around 4% to 6% alcohol by volume (abv), although it may vary between 0.5% and 20%, with some breweries creating examples of 40% abv and above. Beer forms part of the culture of beer-drinking nations and is associated with social traditions such as beer festivals, as well as a rich pub culture involving activities like pub crawling, and pub games such as bar billiards. In Canada, the Canadian Government’s Food and Drug Regulations states that beer should have alcohol content that ranges from 1.1% to 8.6%. The regulation also includes that it could be greater than 8.6% and labeled accordingly. Beer in South Korea should have 25% (v/v) or less which means that it has to be 25 mL of alcohol or less per 100 mL of solution and can only be considered ‘lite’ if they have less than 30 kcal per 100ml. More specifically, major ingredients such as malt (barley and wheat), hop, water, starch ingredients have to be allowed by the South Korean Regulations in the brewing process. Beers and other similar variations in Singapore must have at minimum of 1.0% alcohol (v/v) concentration at 20°C. It is often brewed from a mixture of grains like malt, sugars or it's equivalent and hops or other vegetables.
Go to Article

Explanation by Hotspot Model

Beer

Beer

Beer

Licensed under Creative Commons Attribution-Share Alike 2.5 (The original uploader was SilkTork at English Wikipedia).

Beer is the world's oldest[1][2][3] and most widely consumed[4] alcoholic drink; it is the third most popular drink overall, after water and tea.[5] The production of beer is called brewing, which involves the fermentation of sugars, mainly derived from cereal grain starches—most commonly from malted barley, although wheat, maize (corn), and rice are widely used.[6] Most beer is flavoured with hops, which add bitterness and act as a natural preservative, though other flavourings such as herbs or fruit may occasionally be included. The fermentation process causes a natural carbonation effect, although this is often removed during processing, and replaced with forced carbonation.[7] Some of humanity's earliest known writings refer to the production and distribution of beer: the Code of Hammurabi included laws regulating beer and beer parlours,[8] and "The Hymn to Ninkasi", a prayer to the Mesopotamian goddess of beer, served as both a prayer and as a method of remembering the recipe for beer in a culture with few literate people.[9][10]

Beer is sold in bottles and cans; it may also be available on draught, particularly in pubs and bars. The brewing industry is a global business, consisting of several dominant multinational companies and many thousands of smaller producers ranging from brewpubs to regional breweries. The strength of beer is usually around 4% to 6% alcohol by volume (abv), although it may vary between 0.5% and 20%, with some breweries creating examples of 40% abv and above.[11] Beer forms part of the culture of beer-drinking nations and is associated with social traditions such as beer festivals, as well as a rich pub culture involving activities like pub crawling, and pub games such as bar billiards.

In Canada, the Canadian Government’s Food and Drug Regulations states that beer should have alcohol content that ranges from 1.1% to 8.6%. The regulation also includes that it could be greater than 8.6% and labeled accordingly.[12]

Beer in South Korea should have 25% (v/v) or less which means that it has to be 25 mL of alcohol or less  per 100 mL of solution and can only be considered ‘lite’ if they have less than 30 kcal per 100ml. More specifically, major ingredients such as malt (barley and wheat), hop, water, starch ingredients have to be allowed by the South Korean Regulations in the brewing process.[13]

Beers and other similar variations in Singapore must have at minimum of 1.0% alcohol (v/v) concentration at 20°C. It is often brewed from a mixture of grains like malt, sugars or it's equivalent and hops or other vegetables.[14]

History

Beer is one of the world's oldest prepared beverages, possibly dating back to the early Neolithic or 9500 BC[citation needed], when cereal was first farmed,[15] and is recorded in the written history of ancient Iraq and ancient Egypt.[16] Archaeologists speculate that beer was instrumental in the formation of civilisations.[17] Approximately 5000 years ago, workers in the city of Uruk (modern day Iraq) were paid by their employers in beer.[18] During the building of the Great Pyramids in Giza, Egypt, each worker got a daily ration of four to five litres of beer, which served as both nutrition and refreshment that was crucial to the pyramids' construction.[19]

The earliest known chemical evidence of barley beer dates to circa 3500–3100 BC from the site of Godin Tepe in the Zagros Mountains of western Iran.[20][21] Some of the earliest Sumerian writings contain references to beer; examples include a prayer to the goddess Ninkasi, known as "The Hymn to Ninkasi",[22] which served as both a prayer as well as a method of remembering the recipe for beer in a culture with few literate people,[9][10] and the ancient advice (Fill your belly. Day and night make merry) to Gilgamesh, recorded in the Epic of Gilgamesh, by the ale-wife Siduri may, at least in part, have referred to the consumption of beer.[23] The Ebla tablets, discovered in 1974 in Ebla, Syria, show that beer was produced in the city in 2500 BC.[24] A fermented beverage using rice and fruit was made in China around 7000 BC. Unlike sake, mould was not used to saccharify the rice (amylolytic fermentation); the rice was probably prepared for fermentation by mastication or malting.[25][26]

Almost any substance containing sugar can naturally undergo alcoholic fermentation. It is likely that many cultures, on observing that a sweet liquid could be obtained from a source of starch, independently invented beer. Bread and beer increased prosperity to a level that allowed time for development of other technologies and contributed to the building of civilisations.[27][28][29][30]

Beer was spread through Europe by Germanic and Celtic tribes as far back as 3000 BC,[31] and it was mainly brewed on a domestic scale.[32] The product that the early Europeans drank might not be recognised as beer by most people today. Alongside the basic starch source, the early European beers might contain fruits, honey, numerous types of plants, spices and other substances such as narcotic herbs.[33] What they did not contain was hops, as that was a later addition, first mentioned in Europe around 822 by a Carolingian Abbot[34] and again in 1067 by Abbess Hildegard of Bingen.[35]

In 1516, William IV, Duke of Bavaria, adopted the Reinheitsgebot (purity law), perhaps the oldest food-quality regulation still in use in the 21st century, according to which the only allowed ingredients of beer are water, hops and barley-malt.[36] Beer produced before the Industrial Revolution continued to be made and sold on a domestic scale, although by the 7th century AD, beer was also being produced and sold by European monasteries. During the Industrial Revolution, the production of beer moved from artisanal manufacture to industrial manufacture, and domestic manufacture ceased to be significant by the end of the 19th century.[37] The development of hydrometers and thermometers changed brewing by allowing the brewer more control of the process and greater knowledge of the results.

As of 2007, the brewing industry is a global business, consisting of several dominant multinational companies and many thousands of smaller producers ranging from brewpubs to regional breweries.[38] As of 2006, more than 133 billion litres (35 billion gallons), the equivalent of a cube 510 metres on a side, of beer are sold per year, producing total global revenues of $294.5 billion (£147.7 billion).[39] In 2010, China's beer consumption hit 450 million hectolitres (45 billion litres), or nearly twice that of the United States, but only 5 per cent sold were premium draught beers, compared with 50 per cent in France and Germany.[40]

Brewing

The process of making beer is known as brewing. A dedicated building for the making of beer is called a brewery, though beer can be made in the home and has been for much of its history. A company that makes beer is called either a brewery or a brewing company. Beer made on a domestic scale for non-commercial reasons is classified as homebrewing regardless of where it is made, though most homebrewed beer is made in the home. Brewing beer is subject to legislation and taxation in developed countries, which from the late 19th century largely restricted brewing to a commercial operation only. However, the UK government relaxed legislation in 1963, followed by Australia in 1972 and the US in 1978, allowing homebrewing to become a popular hobby.[41]

The purpose of brewing is to convert the starch source into a sugary liquid called wort and to convert the wort into the alcoholic beverage known as beer in a fermentation process effected by yeast.

The first step, where the wort is prepared by mixing the starch source (normally malted barley) with hot water, is known as "mashing". Hot water (known as "liquor" in brewing terms) is mixed with crushed malt or malts (known as "grist") in a mash tun.[42] The mashing process takes around 1 to 2 hours,[43] during which the starches are converted to sugars, and then the sweet wort is drained off the grains. The grains are now washed in a process known as "sparging". This washing allows the brewer to gather as much of the fermentable liquid from the grains as possible. The process of filtering the spent grain from the wort and sparge water is called wort separation. The traditional process for wort separation is lautering, in which the grain bed itself serves as the filter medium. Some modern breweries prefer the use of filter frames which allow a more finely ground grist.[44]

Most modern breweries use a continuous sparge, collecting the original wort and the sparge water together. However, it is possible to collect a second or even third wash with the not quite spent grains as separate batches. Each run would produce a weaker wort and thus a weaker beer. This process is known as second (and third) runnings. Brewing with several runnings is called parti gyle brewing.[45]

The sweet wort collected from sparging is put into a kettle, or "copper" (so called because these vessels were traditionally made from copper),[46] and boiled, usually for about one hour. During boiling, water in the wort evaporates, but the sugars and other components of the wort remain; this allows more efficient use of the starch sources in the beer. Boiling also destroys any remaining enzymes left over from the mashing stage. Hops are added during boiling as a source of bitterness, flavour and aroma. Hops may be added at more than one point during the boil. The longer the hops are boiled, the more bitterness they contribute, but the less hop flavour and aroma remains in the beer.[47]

After boiling, the hopped wort is now cooled, ready for the yeast. In some breweries, the hopped wort may pass through a hopback, which is a small vat filled with hops, to add aromatic hop flavouring and to act as a filter; but usually the hopped wort is simply cooled for the fermenter, where the yeast is added. During fermentation, the wort becomes beer in a process which requires a week to months depending on the type of yeast and strength of the beer. In addition to producing ethanol, fine particulate matter suspended in the wort settles during fermentation. Once fermentation is complete, the yeast also settles, leaving the beer clear.[48]

Fermentation is sometimes carried out in two stages, primary and secondary. Once most of the alcohol has been produced during primary fermentation, the beer is transferred to a new vessel and allowed a period of secondary fermentation. Secondary fermentation is used when the beer requires long storage before packaging or greater clarity.[49] When the beer has fermented, it is packaged either into casks for cask ale or kegs, aluminium cans, or bottles for other sorts of beer.[50]

Ingredients

The basic ingredients of beer are water; a starch source, such as malted barley, able to be saccharified (converted to sugars) then fermented (converted into ethanol and carbon dioxide); a brewer's yeast to produce the fermentation; and a flavouring such as hops.[51] A mixture of starch sources may be used, with a secondary starch source, such as maize (corn), rice or sugar, often being termed an adjunct, especially when used as a lower-cost substitute for malted barley.[52] Less widely used starch sources include millet, sorghum and cassava root in Africa, and potato in Brazil, and agave in Mexico, among others.[53] The amount of each starch source in a beer recipe is collectively called the grain bill.

The Canadian Government’s Food and Drug Regulations requires that the beer should be made by the alcoholic fermentation of yeast. Beer could be made using barley or wheat malt and hops or hop extract in water that is safe to drink. The end result should have the aroma and taste that is associated with beer.[54]

Water

Beer is composed mostly of water. Regions have water with different mineral components; as a result, different regions were originally better suited to making certain types of beer, thus giving them a regional character.[55] For example, Dublin has hard water well-suited to making stout, such as Guinness; while the Plzeň Region has soft water well-suited to making Pilsner (pale lager), such as Pilsner Urquell.[55] The waters of Burton in England contain gypsum, which benefits making pale ale to such a degree that brewers of pale ales will add gypsum to the local water in a process known as Burtonisation.[56]

Starch source

The starch source in a beer provides the fermentable material and is a key determinant of the strength and flavour of the beer. The most common starch source used in beer is malted grain. Grain is malted by soaking it in water, allowing it to begin germination, and then drying the partially germinated grain in a kiln. Malting grain produces enzymes that convert starches in the grain into fermentable sugars.[57] Different roasting times and temperatures are used to produce different colours of malt from the same grain. Darker malts will produce darker beers.[58]

Nearly all beer includes barley malt as the majority of the starch. This is because its fibrous hull remains attached to the grain during threshing. After malting, barley is milled, which finally removes the hull, breaking it into large pieces. These pieces remain with the grain during the mash, and act as a filter bed during lautering, when sweet wort is separated from insoluble grain material. Other malted and unmalted grains (including wheat, rice, oats, and rye, and less frequently, corn and sorghum) may be used. Some brewers have produced gluten-free beer, made with sorghum with no barley malt, for those who cannot consume gluten-containing grains like wheat, barley, and rye.[59]

Hops

Flavouring beer is the sole major commercial use of hops.[60] The flower of the hop vine is used as a flavouring and preservative agent in nearly all beer made today. The flowers themselves are often called "hops".

The first historical mention of the use of hops in beer was from 822 AD in monastery rules written by Adalhard the Elder, also known as Adalard of Corbie,[37][61] though the date normally given for widespread cultivation of hops for use in beer is the thirteenth century.[37][61] Before the thirteenth century, and until the sixteenth century, during which hops took over as the dominant flavouring, beer was flavoured with other plants; for instance, grains of paradise or alehoof. Combinations of various aromatic herbs, berries, and even ingredients like wormwood would be combined into a mixture known as gruit and used as hops are now used.[62] Some beers today, such as Fraoch' by the Scottish Heather Ales company[63] and Cervoise Lancelot by the French Brasserie-Lancelot company,[64] use plants other than hops for flavouring.

Hops contain several characteristics that brewers desire in beer. Hops contribute a bitterness that balances the sweetness of the malt; the bitterness of beers is measured on the International Bitterness Units scale. Hops contribute floral, citrus, and herbal aromas and flavours to beer. Hops have an antibiotic effect that favours the activity of brewer's yeast over less desirable microorganisms and aids in "head retention",[65][66] the length of time that a foamy head created by carbonation will last. The acidity of hops is a preservative.[67][68]

Hop extract

"Hop extract" means an extract derived from hops by a process employing the solvent. The hop extract should not contain more than 2.2 per cent of the solvent used. The solvent listed on Canada’s Food and Drug Regulations website are hexane, methanol, or methylene chloride. Furthermore, carbon dioxide or ethyl alcohol should be kept in an amount consistent with good manufacturing practice.[69]

"Pre-isomerized hop extract" means an extract derived from hops by one of hexane, carbon dioxide, or ethanol for solvent; and the subsequent isolation of the alpha acids and their conversion to isomerized alpha acids using diluted alkali and heat.[69]

Yeast

Yeast is the microorganism that is responsible for fermentation in beer. Yeast metabolises the sugars extracted from grains, which produces alcohol and carbon dioxide, and thereby turns wort into beer. In addition to fermenting the beer, yeast influences the character and flavour.[70]

The dominant types of yeast used to make beer are the top-fermenting Saccharomyces cerevisiae and bottom-fermenting Saccharomyces pastorianus.[71] Brettanomyces ferments lambics,[72] and Torulaspora delbrueckii ferments Bavarian weissbier.[73]

Before the role of yeast in fermentation was understood, fermentation involved wild or airborne yeasts. A few styles such as lambics rely on this method today, but most modern fermentation adds pure yeast cultures.[74]

Clarifying agent

Some brewers add one or more clarifying agents to beer, which typically precipitate (collect as a solid) out of the beer along with protein solids and are found only in trace amounts in the finished product. This process makes the beer appear bright and clean, rather than the cloudy appearance of ethnic and older styles of beer such as wheat beers.[75]

Examples of clarifying agents include isinglass, obtained from swimbladders of fish; Irish moss, a seaweed; kappa carrageenan, from the seaweed Kappaphycus cottonii; Polyclar (artificial); and gelatin.[76] If a beer is marked "suitable for Vegans", it was clarified either with seaweed or with artificial agents.[77]

Other additives

In South Korea, Additives allowed include Milk- related additives such as Milk, Milk Powder, Milk Cream, Casein, Thickening Agents like Arabic Gum, Pectin and Sweeteners such as Acesulfame K, Erythritol, Xylitol etc. Designated uses and tolerance levels of each additive are established on a product-by-product basis regulated by the Korea Ministry of Food & Drug Safety (MFDS) and may differ from the international regulations..[13]

In Singapore, there are strict regulations on the maximum amount of additives allowed in the table below.[78]

Chemical Preservatives (Parts per Million)
Sulphur Dioxide 25
Benzoic Acid 70
Paraben (Methyl or Propyl Para-hydroxybenzoate) 70
Arsenic, Lead, Copper (Parts per Million)
Arsenic 0.2
Lead 0.2
Copper 7
Sweetening Agents (Parts per Million)
Acesulfame-K 450
Saccharin 240
Cyclamates (Cyclamic Acid) 400
Neotame 26
Steviol Glycosides (Steviol) 175
Sucralose 320

Brewing industry

The brewing industry is a global business, consisting of several dominant multinational companies and many thousands of smaller producers ranging from brewpubs to regional breweries.[38] More than 133 billion litres (35 billion gallons) are sold per year—producing total global revenues of $294.5 billion (£147.7 billion) in 2006.[39]

The history of breweries in the 21st century has been one of larger breweries absorbing smaller breweries in order to ensure economy of scale.[clarification needed] In 2002 South African Breweries bought the North American Miller Brewing Company to found SABMiller, becoming the second largest brewery, after North American Anheuser-Bush. In 2004 the Belgian Interbrew was the third largest brewery by volume and the Brazilian AmBev was the fifth largest. They merged into InBev, becoming the largest brewery. In 2007, SABMiller surpassed InBev and Anheuser-Bush when it acquired Royal Grolsch, brewer of Dutch premium beer brand Grolsch in 2007.[80] In 2008, when InBev (the second-largest) bought Anheuser-Busch (the third largest), the new Anheuser-Busch InBev company became again the largest brewer in the world.[81] As of 2015 AB InBev remains the largest brewery, with SABMiller second, and Heineken International third.

A microbrewery, or craft brewery, produces a limited amount of beer. The maximum amount of beer a brewery can produce and still be classed as a microbrewery varies by region and by authority, though is usually around 15,000 barrels (1.8 megalitres, 396 thousand imperial gallons or 475 thousand US gallons) a year.[82] A brewpub is a type of microbrewery that incorporates a pub or other eating establishment. The highest density of breweries in the world, most of them microbreweries, exists in the German Region of Franconia, especially in the district of Upper Franconia, which has about 200 breweries.[83][84] The Benedictine Weihenstephan Brewery in Bavaria, Germany, can trace its roots to the year 768, as a document from that year refers to a hop garden in the area paying a tithe to the monastery. The brewery was licensed by the City of Freising in 1040, and therefore is the oldest working brewery in the world.[85]

Brewing at home is subject to regulation and prohibition in many countries. Restrictions on homebrewing were lifted in the UK in 1963,[86] Australia followed suit in 1972,[87] and the US in 1978, though individual states were allowed to pass their own laws limiting production.[88]

Varieties

While there are many types of beer brewed, the basics of brewing beer are shared across national and cultural boundaries.[89] The traditional European brewing regions—Germany, Belgium, England and the Czech Republic—have local varieties of beer.[90]

English writer Michael Jackson, in his 1977 book The World Guide To Beer, categorised beers from around the world in local style groups suggested by local customs and names.[91] Fred Eckhardt furthered Jackson's work in The Essentials of Beer Style in 1989.

Top-fermented beers are most commonly produced with Saccharomyces cerevisiae, a top-fermenting yeast which clumps and rises to the surface,[92] typically between 15 and 24 °C (60 and 75 °F). At these temperatures, yeast produces significant amounts of esters and other secondary flavour and aroma products, and the result is often a beer with slightly "fruity" compounds resembling apple, pear, pineapple, banana, plum, or prune, among others.[93]

After the introduction of hops into England from Flanders in the 15th century, "ale" referred to an unhopped fermented beverage, "beer" being used to describe a brew with an infusion of hops.[94]

Etymology

The word ale comes from Old English ealu (plural ealoþ), in turn from Proto-Germanic *alu (plural *aluþ), ultimately from the Proto-Indo-European base *h₂elut-, which holds connotations of "sorcery, magic, possession, intoxication".[95][96][97] The word beer comes from Old English bēor, from Proto-Germanic *beuzą, probably from Proto-Indo-European *bʰeusóm, originally "brewer's yeast, beer dregs", although other theories have been provided connecting the word with Old English bēow, "barley", or Latin bibere, "to drink".[98][99] On the currency of two words for the same thing in the Germanic languages, the 12th-century Old Icelandic poem Alvíssmál says, "Ale it is called among men, but among the gods, beer."[100]

Real ale is the term coined by the Campaign for Real Ale (CAMRA) in 1973[101] for "beer brewed from traditional ingredients, matured by secondary fermentation in the container from which it is dispensed, and served without the use of extraneous carbon dioxide". It is applied to bottle conditioned and cask conditioned beers.

Pale ale is a beer which uses a top-fermenting yeast[102] and predominantly pale malt. It is one of the world's major beer styles.

Stout and porter are dark beers made using roasted malts or roast barley, and typically brewed with slow fermenting yeast. There are a number of variations including Baltic porter, dry stout, and Imperial stout. The name "porter" was first used in 1721 to describe a dark brown beer popular with the street and river porters of London.[103] This same beer later also became known as stout, though the word stout had been used as early as 1677.[104] The history and development of stout and porter are intertwined.[105]

Mild ale has a predominantly malty palate. It is usually dark coloured with an abv of 3% to 3.6%, although there are lighter hued milds as well as stronger examples reaching 6% abv and higher.

Wheat beer is brewed with a large proportion of wheat although it often also contains a significant proportion of malted barley. Wheat beers are usually top-fermented (in Germany they have to be by law).[106] The flavour of wheat beers varies considerably, depending upon the specific style.

Lambic, a beer of Belgium, is naturally fermented using wild yeasts, rather than cultivated. Many of these are not strains of brewer's yeast (Saccharomyces cerevisiae) and may have significant differences in aroma and sourness. Yeast varieties such as Brettanomyces bruxellensis and Brettanomyces lambicus are common in lambics. In addition, other organisms such as Lactobacillus bacteria produce acids which contribute to the sourness.[107]

Lager is cool fermented beer. Pale lagers are the most commonly consumed beers in the world. The name "lager" comes from the German "lagern" for "to store", as brewers around Bavaria stored beer in cool cellars and caves during the warm summer months. These brewers noticed that the beers continued to ferment, and to also clear of sediment, when stored in cool conditions.[108]

Lager yeast is a cool bottom-fermenting yeast (Saccharomyces pastorianus) and typically undergoes primary fermentation at 7–12 °C (45–54 °F) (the fermentation phase), and then is given a long secondary fermentation at 0–4 °C (32–39 °F) (the lagering phase). During the secondary stage, the lager clears and mellows. The cooler conditions also inhibit the natural production of esters and other byproducts, resulting in a "cleaner"-tasting beer.[109]

Modern methods of producing lager were pioneered by Gabriel Sedlmayr the Younger, who perfected dark brown lagers at the Spaten Brewery in Bavaria, and Anton Dreher, who began brewing a lager (now known as Vienna lager), probably of amber-red colour, in Vienna in 1840–1841. With improved modern yeast strains, most lager breweries use only short periods of cold storage, typically 1–3 weeks.

Measurement

Beer is measured and assessed by bitterness, by strength and by colour. The perceived bitterness is measured by the International Bitterness Units scale (IBU), defined in co-operation between the American Society of Brewing Chemists and the European Brewery Convention.[110] The international scale was a development of the European Bitterness Units scale, often abbreviated as EBU, and the bitterness values should be identical.[111]

Colour

Beer colour is determined by the malt.[112] The most common colour is a pale amber produced from using pale malts. Pale lager and pale ale are terms used for beers made from malt dried with the fuel coke. Coke was first used for roasting malt in 1642, but it was not until around 1703 that the term pale ale was used.[113][114]

In terms of sales volume, most of today's beer is based on the pale lager brewed in 1842 in the town of Pilsen in the present-day Czech Republic.[115] The modern pale lager is light in colour with a noticeable carbonation (fizzy bubbles) and a typical alcohol by volume content of around 5%. The Pilsner Urquell, Bitburger, and Heineken brands of beer are typical examples of pale lager, as are the American brands Budweiser, Coors, and Miller.

Dark beers are usually brewed from a pale malt or lager malt base with a small proportion of darker malt added to achieve the desired shade. Other colourants—such as caramel—are also widely used to darken beers. Very dark beers, such as stout, use dark or patent malts that have been roasted longer. Some have roasted unmalted barley.[116][117]

Strength

Beer ranges from less than 3% alcohol by volume (abv) to around 14% abv, though this strength can be increased to around 20% by re-pitching with champagne yeast,[118] and to 55% abv by the freeze-distilling process.[119] The alcohol content of beer varies by local practice or beer style.[120] The pale lagers that most consumers are familiar with fall in the range of 4–6%, with a typical abv of 5%.[121] The customary strength of British ales is quite low, with many session beers being around 4% abv.[122] Some beers, such as table beer are of such low alcohol content (1%–4%) that they are served instead of soft drinks in some schools.[123]

The alcohol in beer comes primarily from the metabolism of sugars that are produced during fermentation. The quantity of fermentable sugars in the wort and the variety of yeast used to ferment the wort are the primary factors that determine the amount of alcohol in the final beer. Additional fermentable sugars are sometimes added to increase alcohol content, and enzymes are often added to the wort for certain styles of beer (primarily "light" beers) to convert more complex carbohydrates (starches) to fermentable sugars. Alcohol is a by-product of yeast metabolism and is toxic to the yeast; typical brewing yeast cannot survive at alcohol concentrations above 12% by volume. Low temperatures and too little fermentation time decreases the effectiveness of yeasts and consequently decreases the alcohol content.

The weakest beers are dealcoholized beers, which typically have less than 0.05% alcohol (also called "near beer") and light beers, which usually have 4% alcohol.

The strength of beers has climbed during the later years of the 20th century. Vetter 33, a 10.5% abv (33 degrees Plato, hence Vetter "33") doppelbock, was listed in the 1994 Guinness Book of World Records as the strongest beer at that time,[124][125] though Samichlaus, by the Swiss brewer Hürlimann, had also been listed by the Guinness Book of World Records as the strongest at 14% abv.[126][127][128] Since then, some brewers have used champagne yeasts to increase the alcohol content of their beers. Samuel Adams reached 20% abv with Millennium,[118] and then surpassed that amount to 25.6% abv with Utopias. The strongest beer brewed in Britain was Baz's Super Brew by Parish Brewery, a 23% abv beer.[129][130] In September 2011, the Scottish brewery BrewDog produced Ghost Deer, which, at 28%, they claim to be the world's strongest beer produced by fermentation alone.[131]

The product claimed to be the strongest beer made is Schorschbräu's 2011 Schorschbock 57 with 57,5%.[132][133] It was preceded by The End of History, a 55% Belgian ale,[119] made by BrewDog in 2010. The same company had previously made Sink The Bismarck!, a 41% abv IPA,[134] and Tactical Nuclear Penguin, a 32% abv Imperial stout. Each of these beers are made using the eisbock method of fractional freezing, in which a strong ale is partially frozen and the ice is repeatedly removed, until the desired strength is reached,[135][136] a process that may class the product as spirits rather than beer.[137] The German brewery Schorschbräu's Schorschbock, a 31% abv eisbock,[138][139][140] and Hair of the Dog's Dave, a 29% abv barley wine made in 1994, used the same fractional freezing method.[141] A 60% abv blend of beer with whiskey was jokingly claimed as the strongest beer by a Dutch brewery in July 2010.[142][143]

Serving

Draught

A selection of cask beers

Draught beer from a pressurised keg using a lever-style dispenser and a spout is the most common method of dispensing in bars around the world. A metal keg is pressurised with carbon dioxide (CO2) gas which drives the beer to the dispensing tap or faucet. Some beers may be served with a nitrogen/carbon dioxide mixture. Nitrogen produces fine bubbles, resulting in a dense head and a creamy mouthfeel. Some types of beer can also be found in smaller, disposable kegs called beer balls. In traditional pubs, the pull levers for major beer brands may include the beer's logo and trademark.

In the 1980s, Guinness introduced the beer widget, a nitrogen-pressurised ball inside a can which creates a dense, tight head, similar to beer served from a nitrogen system.[144] The words draft and draught can be used as marketing terms to describe canned or bottled beers containing a beer widget, or which are cold-filtered rather than pasteurised.

Cask-conditioned ales (or cask ales) are unfiltered and unpasteurised beers. These beers are termed "real ale" by the CAMRA organisation. Typically, when a cask arrives in a pub, it is placed horizontally on a frame called a "stillage" which is designed to hold it steady and at the right angle, and then allowed to cool to cellar temperature (typically between 11–13 °C or 52–55 °F),[145] before being tapped and vented—a tap is driven through a (usually rubber) bung at the bottom of one end, and a hard spile or other implement is used to open a hole in the side of the cask, which is now uppermost. The act of stillaging and then venting a beer in this manner typically disturbs all the sediment, so it must be left for a suitable period to "drop" (clear) again, as well as to fully condition — this period can take anywhere from several hours to several days. At this point the beer is ready to sell, either being pulled through a beer line with a hand pump, or simply being "gravity-fed" directly into the glass.

Draught beer's environmental impact can be 68% lower than bottled beer due to packaging differences.[146][147] A life cycle study of one beer brand, including grain production, brewing, bottling, distribution and waste management, shows that the CO2 emissions from a 6-pack of micro-brew beer is about 3 kilograms (6.6 pounds).[148] The loss of natural habitat potential from the 6-pack of micro-brew beer is estimated to be 2.5 square metres (26 square feet).[149] Downstream emissions from distribution, retail, storage and disposal of waste can be over 45% of a bottled micro-brew beer's CO2 emissions.[148] Where legal, the use of a refillable jug, reusable bottle or other reusable containers to transport draught beer from a store or a bar, rather than buying pre-bottled beer, can reduce the environmental impact of beer consumption.[150]

Packaging

Most beers are cleared of yeast by filtering when packaged in bottles and cans.[151] However, bottle conditioned beers retain some yeast—either by being unfiltered, or by being filtered and then reseeded with fresh yeast.[152] It is usually recommended that the beer be poured slowly, leaving any yeast sediment at the bottom of the bottle. However, some drinkers prefer to pour in the yeast; this practice is customary with wheat beers. Typically, when serving a hefeweizen wheat beer, 90% of the contents are poured, and the remainder is swirled to suspend the sediment before pouring it into the glass. Alternatively, the bottle may be inverted prior to opening. Glass bottles are always used for bottle conditioned beers.

Many beers are sold in cans, though there is considerable variation in the proportion between different countries. In Sweden in 2001, 63.9% of beer was sold in cans.[153] People either drink from the can or pour the beer into a glass. A technology developed by Crown Holdings for the 2010 FIFA World Cup is the 'full aperture' can, so named because the entire lid is removed during the opening process, turning the can into a drinking cup.[154] Cans protect the beer from light (thereby preventing "skunked" beer) and have a seal less prone to leaking over time than bottles. Cans were initially viewed as a technological breakthrough for maintaining the quality of a beer, then became commonly associated with less expensive, mass-produced beers, even though the quality of storage in cans is much like bottles.[155] Plastic (PET) bottles are used by some breweries.[156]

Temperature

The temperature of a beer has an influence on a drinker's experience; warmer temperatures reveal the range of flavours in a beer but cooler temperatures are more refreshing. Most drinkers prefer pale lager to be served chilled, a low- or medium-strength pale ale to be served cool, while a strong barley wine or imperial stout to be served at room temperature.[157]

Beer writer Michael Jackson proposed a five-level scale for serving temperatures: well chilled (7 °C or 45 °F) for "light" beers (pale lagers); chilled (8 °C or 46 °F) for Berliner Weisse and other wheat beers; lightly chilled (9 °C or 48 °F) for all dark lagers, altbier and German wheat beers; cellar temperature (13 °C or 55 °F) for regular British ale, stout and most Belgian specialities; and room temperature (15.5 °C or 60 °F) for strong dark ales (especially trappist beer) and barley wine.[158]

Drinking chilled beer began with the development of artificial refrigeration and by the 1870s, was spread in those countries that concentrated on brewing pale lager.[159] Chilling beer makes it more refreshing,[160] though below 15.5 °C the chilling starts to reduce taste awareness[161] and reduces it significantly below 10 °C (50 °F).[162] Beer served unchilled—either cool or at room temperature—reveal more of their flavours. Cask Marque, a non-profit UK beer organisation, has set a temperature standard range of 12°–14 °C (53°–57 °F) for cask ales to be served.[163]

Vessels

Beer is consumed out of a variety of vessels, such as a glass, a beer stein, a mug, a pewter tankard, a beer bottle or a can; or at music festivals and some bars and nightclubs, from a plastic cup. The shape of the glass from which beer is consumed can influence the perception of the beer and can define and accent the character of the style.[164] Breweries offer branded glassware intended only for their own beers as a marketing promotion, as this increases sales of their product.[165]

The pouring process has an influence on a beer's presentation. The rate of flow from the tap or other serving vessel, tilt of the glass, and position of the pour (in the centre or down the side) into the glass all influence the end result, such as the size and longevity of the head, lacing (the pattern left by the head as it moves down the glass as the beer is drunk), and the release of carbonation.[166] A beer tower is a beer dispensing device, usually found in bars and pubs, that consists of a cylinder attached to a beer cooling device at the bottom. Beer is dispensed from the beer tower into a drinking vessel.

Health effects

Short-term effects

Beer contains ethyl alcohol, the same chemical that is present in wine and distilled spirits and as such, beer consumption has short-term psychological and physiological effects on the user. Different concentrations of alcohol in the human body have different effects on a person. The effects of alcohol depend on the amount an individual has drunk, the percentage of alcohol in the beer and the timespan over which the consumption took place, the amount of food eaten and whether an individual has taken other prescription, over-the-counter or street drugs, among other factors. Drinking enough to cause a blood alcohol concentration (BAC) of 0.03%-0.12% typically causes an overall improvement in mood and possible euphoria, increased self-confidence and sociability, decreased anxiety, a flushed, red appearance in the face and impaired judgment and fine muscle coordination. A BAC of 0.09% to 0.25% causes lethargy, sedation, balance problems and blurred vision. A BAC from 0.18% to 0.30% causes profound confusion, impaired speech (e.g., slurred speech), staggering, dizziness and vomiting. A BAC from 0.25% to 0.40% causes stupor, unconsciousness, anterograde amnesia, vomiting (death may occur due to inhalation of vomit (pulmonary aspiration) while unconscious) and respiratory depression (potentially life-threatening). A BAC from 0.35% to 0.80% causes a coma (unconsciousness), life-threatening respiratory depression and possibly fatal alcohol poisoning. As with all alcoholic drinks, drinking while driving, operating an aircraft or heavy machinery increases the risk of an accident; many countries have severe criminal penalties against drunk driving.

Alcohol acts as a magnesium diuretic, causes a prompt, vigorous increase in the urinary excretion of magnesium and other electrolytes.

Long-term effects

The main active ingredient of beer is alcohol, and therefore, the health effects of alcohol apply to beer. Consumption of small quantities of alcohol (less than one drink in women and two in men) is associated with a decreased risk of cardiac disease, stroke and diabetes mellitus.[167] The long term health effects of continuous, moderate or heavy alcohol consumption include the risk of developing alcoholism and alcoholic liver disease.

Alcoholism, also known as "alcohol use disorder", is a broad term for any drinking of alcohol that results in problems.[168] It was previously divided into two types: alcohol abuse and alcohol dependence.[169][170] In a medical context, alcoholism is said to exist when two or more of the following conditions is present: a person drinks large amounts over a long time period, has difficulty cutting down, acquiring and drinking alcohol takes up a great deal of time, alcohol is strongly desired, usage results in not fulfilling responsibilities, usage results in social problems, usage results in health problems, usage results in risky situations, withdrawal occurs when stopping, and alcohol tolerance has occurred with use.[170] Alcoholism reduces a person's life expectancy by around ten years[171] and alcohol use is the third leading cause of early death in the United States.[167] No professional medical association recommends that people who are nondrinkers should start drinking wine.[167][172] A total of 3.3 million deaths (5.9% of all deaths) are believed to be due to alcohol.[173]

Beers vary in their nutritional content.[174] Brewer's yeast is known to be a rich source of nutrients; therefore, as expected, beer can contain significant amounts of nutrients, including magnesium, selenium, potassium, phosphorus, biotin, chromium and B vitamins. Beer is sometimes referred to as "liquid bread".[175]

It is considered that overeating and lack of muscle tone is the main cause of a beer belly, rather than beer consumption. A 2004 study, however, found a link between binge drinking and a beer belly. But with most overconsumption, it is more a problem of improper exercise and overconsumption of carbohydrates than the product itself.[176] Several diet books quote beer as having an undesirably high glycemic index of 110, the same as maltose; however, the maltose in beer undergoes metabolism by yeast during fermentation so that beer consists mostly of water, hop oils and only trace amounts of sugars, including maltose.[177]

Society and culture

In many societies, beer is the most popular alcoholic drink. Various social traditions and activities are associated with beer drinking, such as playing cards, darts, or other pub games; attending beer festivals; engaging in zythology (the study of beer);[178][179] visiting a series of pubs in one evening; visiting breweries; beer-oriented tourism; or rating beer.[180] Drinking games, such as beer pong, are also popular.[181] A relatively new profession is that of the beer sommelier, who informs restaurant patrons about beers and food pairings.

Beer is considered to be a social lubricant in many societies[182][183] and is consumed in countries all over the world. There are breweries in Middle Eastern countries such as Syria, and in some African countries. Sales of beer are four times those of wine, which is the second most popular alcoholic drink.[184]

A study published in the Neuropsychopharmacology journal in 2013 revealed the finding that the flavour of beer alone could provoke dopamine activity in the brain of the male participants, who wanted to drink more as a result. The 49 men in the study were subject to positron emission tomography scans, while a computer-controlled device sprayed minute amounts of beer, water and a sports drink onto their tongues. Compared with the taste of the sports drink, the taste of beer significantly increased the participants desire to drink. Test results indicated that the flavour of the beer triggered a dopamine release, even though alcohol content in the spray was insufficient for the purpose of becoming intoxicated.[185]

Some breweries have developed beers to pair with food.[186][187][188][189] Wine writer Malcolm Gluck disputed the need to pair beer with food, while beer writers Roger Protz and Melissa Cole contested that claim.[190][191][192]

Related drinks

Around the world, there are many traditional and ancient starch-based drinks classed as beer. In Africa, there are various ethnic beers made from sorghum or millet, such as Oshikundu[193] in Namibia and Tella in Ethiopia.[194] Kyrgyzstan also has a beer made from millet; it is a low alcohol, somewhat porridge-like drink called "Bozo".[195] Bhutan, Nepal, Tibet and Sikkim also use millet in Chhaang, a popular semi-fermented rice/millet drink in the eastern Himalayas.[196] Further east in China are found Huangjiu and Choujiu—traditional rice-based beverages related to beer.

The Andes in South America has Chicha, made from germinated maize (corn); while the indigenous peoples in Brazil have Cauim, a traditional beverage made since pre-Columbian times by chewing manioc so that an enzyme (amylase) present in human saliva can break down the starch into fermentable sugars;[197] this is similar to Masato in Peru.[198]

Some beers which are made from bread, which is linked to the earliest forms of beer, are Sahti in Finland, Kvass in Russia and Ukraine, and Bouza in Sudan.

Chemistry

Beer contains the phenolic acids 4-hydroxyphenylacetic acid, vanillic acid, caffeic acid, syringic acid, p-coumaric acid, ferulic acid and sinapic acid. Alkaline hydrolysis experiments show that most of the phenolic acids are present as bound forms and only a small portion can be detected as free compounds.[199] Hops, and beer made with it, contain 8-prenylnaringenin which is a potent phytoestrogen.[200] Hop also contains myrcene, humulene, xanthohumol, isoxanthohumol, myrcenol, linalool, tannins and resin. The alcohol 2M2B is a component of hops brewing.[201]

Barley, in the form of malt, brings the condensed tannins prodelphinidins B3, B9 and C2 into beer. Tryptophol, tyrosol and phenylethanol are aromatic higher alcohols found in beer[202] as secondary products of alcoholic fermentation[203] (products also known as congeners) by Saccharomyces cerevisiae.

See also



This article uses material from the Wikipedia article "Beer", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Basics

3d,cad,model,library,download,drawing,step,cad blocks,basics,university,highschool,college,grammer school,statistics,3dprinted