powered by CADENAS

Social Share

Amazon

Rock and roll (1410 views - Music)

Rock and roll (often written as rock & roll or rock 'n' roll) is a genre of popular music that originated and evolved in the United States during the late 1940s and early 1950s from musical styles such as gospel, jump blues, jazz, boogie woogie, and rhythm and blues, along with country music. While elements of what was to become rock and roll can be heard in blues records from the 1920s and in country records of the 1930s, the genre did not acquire its name until 1954.According to Greg Kot, "rock and roll" refers to a style of popular music originating in the U.S. in the 1950s prior to its development by the mid-1960s into "the more encompassing international style known as rock music, though the latter also continued to be known as rock and roll." For the purpose of differentiation, this article deals with the first definition. In the earliest rock and roll styles, either the piano or saxophone was typically the lead instrument, but these instruments were generally replaced or supplemented by guitar in the middle to late 1950s. The beat is essentially a dance rhythm with an accentuated backbeat, which is almost always provided by a snare drum. Classic rock and roll is usually played with one or two electric guitars (one lead, one rhythm), a double bass or string bass or (after the mid-1950s) an electric bass guitar, and a drum kit.Beyond simply a musical style, rock and roll, as seen in movies, in fan magazines and on television, influenced lifestyles, fashion, attitudes, and language. In addition, rock and roll may have contributed to the civil rights movement because both African-American and white American teens enjoyed the music. It went on to spawn various genres, often without the initially characteristic backbeat, that are now more commonly called simply "rock music" or "rock".
Go to Article

Explanation by Hotspot Model

Youtube


    

Rock and roll

Rock and roll

Rock and roll (often written as rock & roll or rock 'n' roll) is a genre of popular music that originated and evolved in the United States during the late 1940s and early 1950s[1][2] from musical styles such as gospel, jump blues, jazz, boogie woogie, and rhythm and blues,[3] along with country music.[4] While elements of what was to become rock and roll can be heard in blues records from the 1920s[5] and in country records of the 1930s,[4] the genre did not acquire its name until 1954.[6][7]

According to Greg Kot, "rock and roll" refers to a style of popular music originating in the U.S. in the 1950s prior to its development by the mid-1960s into "the more encompassing international style known as rock music, though the latter also continued to be known as rock and roll."[8] For the purpose of differentiation, this article deals with the first definition.

In the earliest rock and roll styles, either the piano or saxophone was typically the lead instrument, but these instruments were generally replaced or supplemented by guitar in the middle to late 1950s.[9] The beat is essentially a dance rhythm[10] with an accentuated backbeat, which is almost always provided by a snare drum.[11] Classic rock and roll is usually played with one or two electric guitars (one lead, one rhythm), a double bass or string bass or (after the mid-1950s) an electric bass guitar, and a drum kit.[9]

Beyond simply a musical style, rock and roll, as seen in movies, in fan magazines and on television, influenced lifestyles, fashion, attitudes, and language. In addition, rock and roll may have contributed to the civil rights movement because both African-American and white American teens enjoyed the music.[12] It went on to spawn various genres, often without the initially characteristic backbeat, that are now more commonly called simply "rock music" or "rock".

Terminology

The term "rock and roll" now has at least two different meanings, both in common usage. The American Heritage Dictionary[13] and the Merriam-Webster Dictionary[14] both define rock and roll as synonymous with rock music. Encyclopædia Britannica, on the other hand, regards it as the music that originated in the mid-1950s and later developed "into the more encompassing international style known as rock music".[8]

The phrase "rocking and rolling" originally described the movement of a ship on the ocean,[15] but was used by the early twentieth century, both to describe the spiritual fervor of black church rituals[16] and as a sexual analogy. Various gospel, blues and swing recordings used the phrase before it became used more frequently – but still intermittently – in the 1940s, on recordings and in reviews of what became known as "rhythm and blues" music aimed at a black audience.[16]

In 1934, the song "Rock and Roll" by the Boswell Sisters appeared in the film Transatlantic Merry-Go-Round. In 1942, Billboard magazine columnist Maurie Orodenker started to use the term "rock-and-roll" to describe upbeat recordings such as "Rock Me" by Sister Rosetta Tharpe.[17] By 1943, the "Rock and Roll Inn" in South Merchantville, New Jersey, was established as a music venue.[18] In 1951, Cleveland, Ohio disc jockey Alan Freed began playing this music style while popularizing the phrase to describe it.[19]

Early rock and roll

Origins

The origins of rock and roll have been fiercely debated by commentators and historians of music.[20] There is general agreement that it arose in the Southern United States – a region which would produce most of the major early rock and roll acts – through the meeting of various influences that embodied a merging of the African musical tradition with European instrumentation.[21] The migration of many former slaves and their descendants to major urban centers such as St. Louis, Memphis, New York City, Detroit, Chicago, Cleveland, and Buffalo (See: Second Great Migration (African American)) meant that black and white residents were living in close proximity in larger numbers than ever before, and as a result heard each other's music and even began to emulate each other's fashions.[22][23] Radio stations that made white and black forms of music available to both groups, the development and spread of the gramophone record, and African-American musical styles such as jazz and swing which were taken up by white musicians, aided this process of "cultural collision".[24]

The immediate roots of rock and roll lay in the rhythm and blues, then called "race music",[25] and country music of the 1940s and 1950s.[20] Particularly significant influences were jazz, blues, gospel, country, and folk.[20] Commentators differ in their views of which of these forms were most important and the degree to which the new music was a re-branding of African-American rhythm and blues for a white market, or a new hybrid of black and white forms.[26][27][28]

In the 1930s, jazz, and particularly swing, both in urban-based dance bands and blues-influenced country swing (Jimmie Rodgers, Moon Mullican and other similar singers), were among the first music to present African-American sounds for a predominantly white audience.[27][29] One particularly noteworthy example of a jazz song with recognizably rock and roll elements is Big Joe Turner with pianist Pete Johnson's 1939 single Roll 'Em Pete, which is regarded as an important precursor of rock and roll.[30][31][32] The 1940s saw the increased use of blaring horns (including saxophones), shouted lyrics and boogie woogie beats in jazz-based music. During and immediately after World War II, with shortages of fuel and limitations on audiences and available personnel, large jazz bands were less economical and tended to be replaced by smaller combos, using guitars, bass and drums.[20][33] In the same period, particularly on the West Coast and in the Midwest, the development of jump blues, with its guitar riffs, prominent beats and shouted lyrics, prefigured many later developments.[20] In the documentary film Hail! Hail! Rock 'n' Roll, Keith Richards proposes that Chuck Berry developed his brand of rock and roll, by transposing the familiar two-note lead line of jump blues piano directly to the electric guitar, creating what is instantly recognizable as rock guitar. Similarly, country boogie and Chicago electric blues supplied many of the elements that would be seen as characteristic of rock and roll.[20] Inspired by electric blues, Chuck Berry introduced an aggressive guitar sound to rock and roll, and established the electric guitar as its centrepiece,[34] adapting his rock band instrumentation from the basic blues band instrumentation of a lead guitar, second chord instrument, bass and drums.[35]

Rock and roll arrived at a time of considerable technological change, soon after the development of the electric guitar, amplifier and microphone, and the 45 rpm record.[20] There were also changes in the record industry, with the rise of independent labels like Atlantic, Sun and Chess servicing niche audiences and a similar rise of radio stations that played their music.[20] It was the realization that relatively affluent white teenagers were listening to this music that led to the development of what was to be defined as rock and roll as a distinct genre.[20] Because the development of rock and roll was an evolutionary process, no single record can be identified as unambiguously "the first" rock and roll record.[36] Contenders for the title of "first rock and roll record" include "The Fat Man" by Fats Domino (1949),[36] Sister Rosetta Tharpe's "Strange Things Happening Everyday" (1944),[37] Goree Carter's "Rock Awhile" (1949),[38] Jimmy Preston's "Rock the Joint" (1949), which was later covered by Bill Haley & His Comets in 1952,[39] "Rocket 88" by Jackie Brenston and his Delta Cats (Ike Turner and his band The Kings of Rhythm), recorded by Sam Phillips for Sun Records in March 1951.[40] In terms of its wide cultural impact across society in the US and elsewhere, Bill Haley's "Rock Around the Clock",[41] recorded in April 1954 but not a commercial success until the following year, is generally recognized as an important milestone, but it was preceded by many recordings from earlier decades in which elements of rock and roll can be clearly discerned.[36][42][43]

Other artists with early rock and roll hits included Chuck Berry, Bo Diddley, Little Richard, Jerry Lee Lewis, and Gene Vincent.[40] Chuck Berry's 1955 classic "Maybellene" in particular features a distorted electric guitar solo with warm overtones created by his small valve amplifier.[44] However, the use of distortion was predated by electric blues guitarists such as Joe Hill Louis,[45] Guitar Slim,[46] Willie Johnson of Howlin' Wolf's band,[47] and Pat Hare; the latter two also made use of distorted power chords in the early 1950s.[48] Also in 1955, Bo Diddley introduced the "Bo Diddley beat" and a unique electric guitar style,[49] influenced by African and Afro-Cuban music and in turn influencing many later artists.[50][51][52]

Rockabilly

"Rockabilly" usually (but not exclusively) refers to the type of rock and roll music which was played and recorded in the mid-1950s primarily by white singers such as Elvis Presley, Carl Perkins, Johnny Cash, and Jerry Lee Lewis, who drew mainly on the country roots of the music.[53][54] Elvis Presley was greatly influenced and incorporated his style of music with some of the greatest African American musicians like BB King, Chuck Berry and Fats Domino. His style of music combined with black influences created controversy during a turbulent time in history but that did not stop them from creating what we call Rock n Roll.[54] Many other popular rock and roll singers of the time, such as Fats Domino and Little Richard,[55] came out of the black rhythm and blues tradition, making the music attractive to white audiences, and are not usually classed as "rockabilly".

Bill Flagg who is a Connecticut resident, began referring to his mix of hillbilly and rock 'n' roll music as rockabilly around 1953.[56] His song "Guitar Rock" is considered as classic rockabilly.[citation needed]

In July 1954, Elvis Presley recorded the regional hit "That's All Right" at Sam Phillips' Sun Studio in Memphis.[57] Three months earlier, on April 12, 1954, Bill Haley & His Comets recorded "Rock Around the Clock". Although only a minor hit when first released, when used in the opening sequence of the movie Blackboard Jungle a year later, it set the rock and roll boom in motion.[41] The song became one of the biggest hits in history, and frenzied teens flocked to see Haley and the Comets perform it, causing riots in some cities. "Rock Around the Clock" was a breakthrough for both the group and for all of rock and roll music. If everything that came before laid the groundwork, "Rock Around the Clock" introduced the music to a global audience.[58]

In 1956, the arrival of rockabilly was underlined by the success of songs like "Folsom Prison Blues" by Johnny Cash, "Blue Suede Shoes" by Perkins and the #1 hit "Heartbreak Hotel" by Presley.[54] For a few years it became the most commercially successful form of rock and roll. Later rockabilly acts, particularly performing songwriters like Buddy Holly, would be a major influence on British Invasion acts and particularly on the song writing of the Beatles and through them on the nature of later rock music.[59]

Doo wop

Doo wop was one of the most popular forms of 1950s rhythm and blues, often compared with rock and roll, with an emphasis on multi-part vocal harmonies and meaningless backing lyrics (from which the genre later gained its name), which were usually supported with light instrumentation.[60] Its origins were in African-American vocal groups of the 1930s and 40s, such as the Ink Spots and the Mills Brothers, who had enjoyed considerable commercial success with arrangements based on close harmonies.[61] They were followed by 1940s R&B vocal acts such as the Orioles, the Ravens and the Clovers, who injected a strong element of traditional gospel and, increasingly, the energy of jump blues.[61] By 1954, as rock and roll was beginning to emerge, a number of similar acts began to cross over from the R&B charts to mainstream success, often with added honking brass and saxophone, with the Crows, the Penguins, the El Dorados and the Turbans all scoring major hits.[61] Despite the subsequent explosion in records from doo wop acts in the later '50s, many failed to chart or were one-hit wonders. Exceptions included the Platters, with songs including "The Great Pretender" (1955)[62] and the Coasters with humorous songs like "Yakety Yak" (1958),[63] both of which ranked among the most successful rock and roll acts of the era.[61] Towards the end of the decade there were increasing numbers of white, particularly Italian-American, singers taking up Doo Wop, creating all-white groups like the Mystics and Dion and the Belmonts and racially integrated groups like the Del-Vikings and the Impalas.[61] Doo wop would be a major influence on vocal surf music, soul and early Merseybeat, including the Beatles.[61]

Cover versions

Many of the earliest white rock and roll hits were covers or partial re-writes of earlier black rhythm and blues or blues songs.[64] Through the late 1940s and early 1950s, R&B music had been gaining a stronger beat and a wilder style, with artists such as Fats Domino and Johnny Otis speeding up the tempos and increasing the backbeat to great popularity on the juke joint circuit.[65] Before the efforts of Freed and others, black music was taboo on many white-owned radio outlets, but artists and producers quickly recognized the potential of rock and roll.[66] Some of Presley's early recordings were covers of black rhythm and blues or blues songs, such as "That's All Right" (a countrified arrangement of a blues number), "Baby Let's Play House", "Lawdy Miss Clawdy" and "Hound Dog".[67] The racial lines however are rather more clouded by the fact that some of these R&B songs originally recorded by black artists had been written by white songwriters, such as the team of Jerry Leiber and Mike Stoller. Songwriting credits were often unreliable; many publishers, record executives, and even managers (both white and black) would insert their name as composer in order to collect royalty checks.

Covers were customary in the music industry at the time; it was made particularly easy by the compulsory license provision of United States copyright law (still in effect).[68] One of the first relevant successful covers was Wynonie Harris's transformation of Roy Brown's 1947 original jump blues hit "Good Rocking Tonight" into a more showy rocker[69] and the Louis Prima rocker "Oh Babe" in 1950, as well as Amos Milburn's cover of what may have been the first white rock and roll record, Hardrock Gunter's "Birmingham Bounce" in 1949.[70] The most notable trend, however, was white pop covers of black R&B numbers. The more familiar sound of these covers may have been more palatable to white audiences, there may have been an element of prejudice, but labels aimed at the white market also had much better distribution networks and were generally much more profitable.[71] Famously, Pat Boone recorded sanitized versions of songs recorded by the likes of Fats Domino, Little Richard, the Flamingos and Ivory Joe Hunter. Later, as those songs became popular, the original artists' recordings received radio play as well.[72]

The cover versions were not necessarily straightforward imitations. For example, Bill Haley's incompletely bowdlerized cover of "Shake, Rattle and Roll" transformed Big Joe Turner's humorous and racy tale of adult love into an energetic teen dance number,[64][73] while Georgia Gibbs replaced Etta James's tough, sarcastic vocal in "Roll With Me, Henry" (covered as "Dance With Me, Henry") with a perkier vocal more appropriate for an audience unfamiliar with the song to which James's song was an answer, Hank Ballard's "Work With Me, Annie".[74] Elvis' rock and roll version of "Hound Dog", taken mainly from a version recorded by pop band Freddie Bell and the Bellboys, was very different from the blues shouter that Big Mama Thornton had recorded four years earlier.[75][76] Other white artists who recorded cover versions of rhythm & blues songs included Gale Storm [Smiley Lewis' "I Hear You Knockin'"], the Diamonds [The Gladiolas' "Little Darlin'" and Frankie Lymon & the Teenagers' "Why Do Fools Fall in Love?"], the Crew Cuts [the Chords' "Sh-Boom" and Nappy Brown's "Don't Be Angry"], the Fountain Sisters [The Jewels' "Hearts of Stone"} and the Maguire Sisters [The Moonglows' "Sincerely"].

Decline

Some commentators have suggested a decline of rock and roll in the late 1950s and early 1960s.[77][78] By 1959, the deaths of Buddy Holly, The Big Bopper and Ritchie Valens in a plane crash (February 1959), the departure of Elvis for service in the United States Army (March 1958), the retirement of Little Richard to become a preacher (October 1957), the scandal surrounding Jerry Lee Lewis' marriage to his thirteen-year-old cousin (May 1958), the arrest of Chuck Berry (December 1959), and the breaking of the Payola scandal implicating major figures, including Alan Freed, in bribery and corruption in promoting individual acts or songs (November 1959), gave a sense that the initial phase of rock and roll had come to an end.[79]

During the late 1950s and early 1960s, the rawer sounds of Elvis Presley, Gene Vincent, Jerry Lee Lewis and Buddy Holly were commercially superseded by a more polished, commercial style of rock and roll. Marketing frequently emphasized the physical looks of the artist rather than the music, contributing to the successful careers of Rick Nelson, Tommy Sands, Bobby Vee and the Philadelphia trio of Bobby Rydell, Frankie Avalon and Fabian, who all became "teen idols."[citation needed]

Some music historians have also pointed to important and innovative developments that built on rock and roll in this period, including multitrack recording, developed by Les Paul, the electronic treatment of sound by such innovators as Joe Meek, and the "Wall of Sound" productions of Phil Spector,[80] continued desegregation of the charts, the rise of surf music, garage rock and the Twist dance craze.[27] Surf rock in particular, noted for the use of reverb-drenched guitars, became one of the most popular forms of American rock of the 1960s.[81]

British rock and roll

In the 1950s, Britain was well placed to receive American rock and roll music and culture.[82] It shared a common language, had been exposed to American culture through the stationing of troops in the country, and shared many social developments, including the emergence of distinct youth sub-cultures, which in Britain included the Teddy Boys and the rockers.[83] Trad Jazz became popular, and many of its musicians were influenced by related American styles, including boogie woogie and the blues.[84] The skiffle craze, led by Lonnie Donegan, utilised amateurish versions of American folk songs and encouraged many of the subsequent generation of rock and roll, folk, R&B and beat musicians to start performing.[85] At the same time British audiences were beginning to encounter American rock and roll, initially through films including Blackboard Jungle (1955) and Rock Around the Clock (1955).[86] Both movies contained the Bill Haley & His Comets hit "Rock Around the Clock", which first entered the British charts in early 1955 – four months before it reached the US pop charts – topped the British charts later that year and again in 1956, and helped identify rock and roll with teenage delinquency.[87] American rock and roll acts such as Elvis Presley, Little Richard, Buddy Holly, Chuck Berry and Carl Perkins thereafter became major forces in the British charts.[citation needed]

The initial response of the British music industry was to attempt to produce copies of American records, recorded with session musicians and often fronted by teen idols.[82] More grassroots British rock and rollers soon began to appear, including Wee Willie Harris and Tommy Steele.[82] During this period American Rock and Roll remained dominant; however, in 1958 Britain produced its first "authentic" rock and roll song and star, when Cliff Richard reached number 2 in the charts with "Move It".[88] At the same time, TV shows such as Six-Five Special and Oh Boy! promoted the careers of British rock and rollers like Marty Wilde and Adam Faith.[82] Cliff Richard and his backing band, the Shadows, were the most successful home grown rock and roll based acts of the era.[89] Other leading acts included Billy Fury, Joe Brown, and Johnny Kidd & the Pirates, whose 1960 hit song "Shakin' All Over" became a rock and roll standard.[82]

As interest in rock and roll was beginning to subside in America in the late 1950s and early 1960s, it was taken up by groups in major British urban centres like Liverpool, Manchester, Birmingham, and London.[90] About the same time, a British blues scene developed, initially led by purist blues followers such as Alexis Korner and Cyril Davies who were directly inspired by American musicians such as Robert Johnson, Muddy Waters and Howlin' Wolf.[91] Many groups moved towards the beat music of rock and roll and rhythm and blues from skiffle, like the Quarrymen who became the Beatles, producing a form of rock and roll revivalism that carried them and many other groups to national success from about 1963 and to international success from 1964, known in America as the British Invasion.[92] Groups that followed the Beatles included the beat-influenced Freddie and the Dreamers, Wayne Fontana and the Mindbenders, Herman's Hermits and the Dave Clark Five.[93] Early British rhythm and blues groups with more blues influences include the Animals, the Rolling Stones, and the Yardbirds.[94]

Cultural impact

Rock and roll influenced lifestyles, fashion, attitudes, and language.[95] In addition, rock and roll may have contributed to the civil rights movement because both African-American and white American teens enjoyed the music.[12]

Many early rock and roll songs dealt with issues of cars, school, dating, and clothing. The lyrics of rock and roll songs described events and conflicts that most listeners could relate to through personal experience. Topics such as sex that had generally been considered taboo began to appear in rock and roll lyrics. This new music tried to break boundaries and express emotions that people were actually feeling but had not talked about. An awakening began to take place in American youth culture.[96]

Race

In the crossover of African-American "race music" to a growing white youth audience, the popularization of rock and roll involved both black performers reaching a white audience and white musicians performing African-American music.[97] Rock and roll appeared at a time when racial tensions in the United States were entering a new phase, with the beginnings of the civil rights movement for desegregation, leading to the U.S. Supreme Court ruling that abolished the policy of "separate but equal" in 1954, but leaving a policy which would be extremely difficult to enforce in parts of the United States.[98] The coming together of white youth audiences and black music in rock and roll inevitably provoked strong white racist reactions within the US, with many whites condemning its breaking down of barriers based on color.[12] Many observers saw rock and roll as heralding the way for desegregation, in creating a new form of music that encouraged racial cooperation and shared experience.[99] Many authors have argued that early rock and roll was instrumental in the way both white and black teenagers identified themselves.[100]

Teen culture

Several rock historians have claimed that rock and roll was one of the first music genres to define an age group.[101] It gave teenagers a sense of belonging, even when they were alone.[101] Rock and roll is often identified with the emergence of teen culture among the first baby boomer generation, who had greater relative affluence and leisure time and adopted rock and roll as part of a distinct subculture.[102] This involved not just music, absorbed via radio, record buying, jukeboxes and TV programs like American Bandstand, but also extended to film, clothes, hair, cars and motorbikes, and distinctive language. The youth culture exemplified by rock and roll was a recurring source of concern for older generations, who worried about juvenile delinquency and social rebellion, particularly because to a large extent rock and roll culture was shared by different racial and social groups.[102]

In America, that concern was conveyed even in youth cultural artifacts such as comic books. In "There's No Romance in Rock and Roll" from True Life Romance (1956), a defiant teen dates a rock and roll-loving boy but drops him for one who likes traditional adult music—to her parents' relief.[103] In Britain, where postwar prosperity was more limited, rock and roll culture became attached to the pre-existing Teddy Boy movement, largely working class in origin, and eventually to the rockers.[83] Rock and roll has been seen as reorienting popular music toward a youth market, as in Dion and the Belmonts' "A Teenager in Love" (1960).[104]

Dance styles

From its early 1950s beginnings through the early 1960s, rock and roll spawned new dance crazes[105] including the twist. Teenagers found the syncopated backbeat rhythm especially suited to reviving Big Band-era jitterbug dancing. Sock hops, school and church gym dances, and home basement dance parties became the rage, and American teens watched Dick Clark's American Bandstand to keep up on the latest dance and fashion styles.[106] From the mid-1960s on, as "rock and roll" was rebranded as "rock," later dance genres followed, leading to funk, disco, house, techno, and hip hop.[107]

Notes

  1. ^ Farley, Christopher John (July 6, 2004). "Elvis Rocks But He's Not the First". Time.
  2. ^ Jim Dawson and Steve Propes, What Was the First Rock'n'Roll Record (1992), ISBN 0-571-12939-0.
  3. ^ Christ-Janer, Albert, Charles W. Hughes, and Carleton Sprague Smith, American Hymns Old and New (New York: Columbia University Press, 1980), p. 364, ISBN 0-231-03458-X.
  4. ^ a b Peterson, Richard A. Creating Country Music: Fabricating Authenticity (1999), p. 9, ISBN 0-226-66285-3.
  5. ^ Davis, Francis. The History of the Blues (New York: Hyperion, 1995), ISBN 0-7868-8124-0.
  6. ^ "The Roots of Rock 'n' Roll 1946–1954". 2004. Universal Music Enterprises.
  7. ^ Dawson, Jim & Propes, Steve, What was the first rock 'n' roll record?, Faber & Faber, ISBN 0-571-12939-0, 1992.
  8. ^ a b Kot, Greg, "Rock and roll", in the Encyclopædia Britannica, published online 17 June 2008 and also in print and in the Encyclopædia Britannica Ultimate Reference DVD; Chicago : Encyclopædia Britannica, 2010
  9. ^ a b S. Evans, "The development of the Blues" in A. F. Moore, ed., The Cambridge companion to blues and gospel music (Cambridge: Cambridge University Press, 2002), pp. 40–42.
  10. ^ Busnar, Gene, It’s Rock ’n’ Roll: A musical history of the fabulous fifties, Julian Messner, New York, 1979, p. 45
  11. ^ P. Hurry, M. Phillips, and M. Richards, Heinemann advanced music (Heinemann, 2001), pp. 153–4.
  12. ^ a b c G. C. Altschuler, All shook up: how rock 'n' roll changed America (Oxford: Oxford University Press US, 2003), p. 35.
  13. ^ "Rock music". The American Heritage Dictionary. Bartleby.com. Retrieved December 15, 2008.
  14. ^ "Rock and roll". Merriam-Webster's Online Dictionary. Merriam-Webster Online. Retrieved December 15, 2008.
  15. ^ "The United Service Magazine". October 22, 2017 – via Google Books.
  16. ^ a b "Morgan Wright's HoyHoy.com: The Dawn of Rock 'n Roll". Hoyhoy.com. May 2, 1954. Retrieved April 14, 2012.
  17. ^ Billboard, May 30, 1942, page 25. Other examples are in describing Vaughn Monroe's "Coming Out Party" in the issue of June 27, 1942, page 76; Count Basie's "It's Sand, Man", in the issue of October 3, 1942, page 63; and Deryck Sampson's "Kansas City Boogie-Woogie" in the issue of October 9, 1943, page 67.
  18. ^ Billboard, June 12, 1943, page 19
  19. ^ Bordowitz, Hank (2004). Turning Points in Rock and Roll. New York, New York: Citadel Press. p. 63. ISBN 978-0-8065-2631-7.
  20. ^ a b c d e f g h i Bogdanov, Woodstra & Erlewine 2002, p. 1303
  21. ^ M. T. Bertrand, Race, Rock, and Elvis: Music in American Life (University of Illinois Press, 2000), pp. 21–2.
  22. ^ R. Aquila, That old-time rock & roll: a chronicle of an era, 1954–1963 (Chicago: University of Illinois Press, 2000), pp. 4–6.
  23. ^ J. M. Salem, The late, great Johnny Ace and the transition from R & B to rock 'n' roll Music in American life (University of Illinois Press, 2001), p. 4.
  24. ^ M. T. Bertrand, 'Race, rock, and Elvis Music in American life (University of Illinois Press, 2000), p. 99.
  25. ^ Gilliland 1969, show 3, show 55.
  26. ^ A. Bennett, Rock and popular music: politics, policies, institutions (Routledge, 1993), pp. 236–8.
  27. ^ a b c K. Keightley, "Reconsidering rock" S. Frith, W. Straw and J. Street, eds, The Cambridge companion to pop and rock (Cambridge: Cambridge University Press, 2001), p. 116.
  28. ^ N. Kelley, R&B, rhythm and business: the political economy of Black music (Akashic Books, 2005), p. 134.
  29. ^ E. Wald, How the Beatles Destroyed Rock N Roll: An Alternative History of American Popular Music (Oxford: Oxford University Press, 2009), pp. 111–25.
  30. ^ Nick Tosches, Unsung Heroes of Rock 'n' Roll, Secker & Warburg, 1991, ISBN 0-436-53203-4
  31. ^ Peter J. Silvester, A Left Hand Like God : a history of boogie-woogie piano (1989), ISBN 0-306-80359-3.
  32. ^ M. Campbell, ed., Popular Music in America: And the Beat Goes on (Cengage Learning, 3rd edn, 2008), p. 99. ISBN 0-495-50530-7
  33. ^ P. D. Lopes, The rise of a jazz art world (Cambridge: Cambridge University Press, 2002), p. 132
  34. ^ Michael Campbell & James Brody, Rock and Roll: An Introduction, pages 110-111
  35. ^ Michael Campbell & James Brody, Rock and Roll: An Introduction, pp. 80-81.
  36. ^ a b c Jim Dawson and Steve Propes, What Was The First Rock'n'Roll Record, 1992, ISBN 0-571-12939-0
  37. ^ Williams, R (March 18, 2015). "Sister Rosetta Tharpe: the godmother of rock 'n' roll".
  38. ^ Robert Palmer, "Church of the Sonic Guitar", pp. 13–38 in Anthony DeCurtis, Present Tense, Duke University Press, 1992, p. 19. ISBN 0-8223-1265-4.
  39. ^ Jimmy Preston at AllMusic
  40. ^ a b M. Campbell, ed., Popular Music in America: and the Beat Goes on (Boston, MA: Cengage Learning, 3rd edn., 2008), ISBN 0-495-50530-7, pp. 157–8.
  41. ^ a b Gilliland 1969, show 5, show 55.
  42. ^ Robert Palmer, "Rock Begins", in Rolling Stone Illustrated History of Rock and Roll, 1976/1980, ISBN 0-330-26568-7 (UK edition), pp. 3–14.
  43. ^ Unterberger, Richie. Birth of Rock & Roll at AllMusic. Retrieved March 24, 2012.
  44. ^ Collis, John (2002). Chuck Berry: The Biography. Aurum. p. 38.
  45. ^ DeCurtis, Anthony (1992). Present Tense: Rock & Roll and Culture (4. print. ed.). Durham, N.C.: Duke University Press. ISBN 0822312654. His first venture, the Phillips label, issued only one known release, and it was one of the loudest, most overdriven, and distorted guitar stomps ever recorded, "Boogie in the Park" by Memphis one-man-band Joe Hill Louis, who cranked his guitar while sitting and banging at a rudimentary drum kit.
  46. ^ Aswell, Tom (2010). Louisiana Rocks! The True Genesis of Rock & Roll. Gretna, Louisiana: Pelican Publishing Company. pp. 61–5. ISBN 1589806778..
  47. ^ Dave, Rubin (2007). Inside the Blues, 1942 to 1982. Hal Leonard. p. 61.
  48. ^ Robert Palmer, "Church of the Sonic Guitar", pp. 13–38 in Anthony DeCurtis, Present Tense, Duke University Press, 1992, pp. 24–27. ISBN 0-8223-1265-4.
  49. ^ P. Buckley, The rough guide to rock (Rough Guides, 3rd edn., 2003), p. 21.
  50. ^ "Bo Diddley". The Rock and Roll Hall of Fame and Museum. Retrieved October 27, 2008.
  51. ^ "Bo Diddley". Rolling Stone. 2001. Retrieved April 26, 2012.
  52. ^ Brown, Jonathan (June 3, 2008). "Bo Diddley, guitarist who inspired the Beatles and the Stones, dies aged 79". The Independent. Retrieved April 26, 2012.
  53. ^ Gilliland 1969, shows 7-8.
  54. ^ a b c “Rock and Roll Pilgrims: Reflections on Ritual, Religiosity, and Race at Rockabilly at AllMusic. Retrieved August 6, 2009.
  55. ^ Gilliland 1969, show 6.
  56. ^ "Granville's Bill Flagg pioneered rockabilly". masslive.com. Retrieved 2017-04-28.
  57. ^ Elvis at AllMusic. Retrieved August 6, 2009.
  58. ^ Bill Haley at AllMusic. Retrieved August 6, 2009.
  59. ^ P. Humphries, The Complete Guide to the Music of The Beatles, Volume 2 (Music Sales Group, 1998), p. 29.
  60. ^ F. W. Hoffmann and H. Ferstler, Encyclopedia of recorded sound, Volume 1 (CRC Press, 2nd edn., 2004), pp. 327–8.
  61. ^ a b c d e f Bogdanov, Woodstra & Erlewine 2002, pp. 1306–7
  62. ^ Gilliland 1969, show 5, track 3.
  63. ^ Gilliland 1969, show 13.
  64. ^ a b Gilliland 1969, show 4, track 5.
  65. ^ Ennis, Philip H. (1992), The Seventh Stream – The Emergence of Rocknroll in American Popular Music, Wesleyan University Press, p. 201, ISBN 978-0-8195-6257-9
  66. ^ R. Aquila, That old-time rock & roll: a chronicle of an era, 1954–1963 (Chicago: University of Illinois Press, 2000), p. 6.
  67. ^ C. Deffaa, Blue rhythms: six lives in rhythm and blues (Chicago: University of Illinois Press, 1996), pp. 183–4.
  68. ^ J. V. Martin, Copyright: current issues and laws (Nova Publishers, 2002), pp. 86–8.
  69. ^ G. Lichtenstein and L. Dankner. Musical gumbo: the music of New Orleans (W.W. Norton, 1993), p. 775.
  70. ^ R. Carlin. Country music: a biographical dictionary (Taylor & Francis, 2003), p. 164.
  71. ^ R. Aquila, That old-time rock & roll: a chronicle of an era, 1954–1963 (Chicago: University of Illinois Press, 2000), p. 201.
  72. ^ G. C. Altschuler, All shook up: how rock 'n' roll changed America (Oxford: Oxford University Press US, 2003), pp. 51–2.
  73. ^ R. Coleman, Blue Monday: Fats Domino and the Lost Dawn of Rock 'n' Roll (Da Capo Press, 2007), p. 95.
  74. ^ D. Tyler, Music of the postwar era (Greenwood, 2008), p. 79.
  75. ^ C. L. Harrington, and D. D. Bielby., Popular culture: production and consumption (Wiley-Blackwell, 2001), p. 162.
  76. ^ Gilliland 1969, show 7, track 4.
  77. ^ D. Hatch and S. Millward, From blues to rock: an analytical history of pop music (Manchester: Manchester University Press ND, 1987), p. 110.
  78. ^ M. Campbell, Popular Music in America: And the Beat Goes on: Popular Music in America (Publisher Cengage Learning, 3rd edn., 2008), p. 172.
  79. ^ M. Campbell, ed., Popular Music in America: And the Beat Goes on (Cengage Learning, 3rd edn., 2008), p. 99.
  80. ^ Gilliland 1969, show 21.
  81. ^ "Surf Music Genre Overview - AllMusic". AllMusic.
  82. ^ a b c d e Unterberger, Richie. British Rock & Roll Before the Beatles at AllMusic. Retrieved June 24, 2009.
  83. ^ a b D. O'Sullivan, The Youth Culture London: Taylor & Francis, 1974), pp. 38–9.
  84. ^ J. R. Covach and G. MacDonald Boone, Understanding Rock: Essays in Musical Analysis (Oxford: Oxford University Press, 1997), p. 60.
  85. ^ M. Brocken, The British folk revival, 1944–2002 (Aldershot: Ashgate, 2003), pp. 69–80.
  86. ^ V. Porter, British Cinema of the 1950s: The Decline of Deference (Oxford: Oxford University Press, 2007), p. 192.
  87. ^ T. Gracyk, I Wanna Be Me: Rock Music and the Politics of Identity (Temple University Press, 2001), pp. 117–18.
  88. ^ D. Hatch, S. Millward, From Blues to Rock: an Analytical History of Pop Music (Manchester: Manchester University Press, 1987), p. 78.
  89. ^ A. J. Millard, The electric guitar: a history of an American icon (JHU Press, 2004), p. 150.
  90. ^ Mersey Beat – the founders' story.
  91. ^ V. Bogdanov, C. Woodstra, S. T. Erlewine, eds, All Music Guide to the Blues: The Definitive Guide to the Blues (Backbeat, 3rd edn., 2003), p. 700.
  92. ^ British Invasion at AllMusic. Retrieved August 10, 2009.
  93. ^ Ira A. Robbins (February 7, 1964). "British Invasion (music)". Britannica.com. Retrieved April 14, 2012.
  94. ^ Unterberger, Richie (1996). "Blues rock". In Erlewine, Michael. All Music Guide to the Blues. San Francisco: Miller Freeman Books. p. 378. ISBN 0-87930-424-3.
  95. ^ G. C. Altschuler, All shook up: how rock 'n' roll changed America (Oxford: Oxford University Press US, 2003), p. 121.
  96. ^ Schafer, William J. Rock Music: Where It's Been, What It Means, Where It's Going. Minneapolis: Augsburg Publishing House, 1972.
  97. ^ M. Fisher, Something in the air: radio, rock, and the revolution that shaped a generation (Marc Fisher, 2007), p. 53.
  98. ^ H. Zinn, A people's history of the United States: 1492–present (Pearson Education, 3rd edn., 2003), p. 450.
  99. ^ M. T. Bertrand, Race, rock, and Elvis (University of Illinois Press, 2000), pp. 95–6.
  100. ^ Carson, Mina (2004). Girls Rock!: Fifty Years of Women Making Music. Lexington. p. 24.
  101. ^ a b Padel, Ruth (2000). I'm a Man: Sex, Gods, and Rock 'n' Roll. Faber and Faber. pp. 46–48.
  102. ^ a b M. Coleman, L. H. Ganong, K. Warzinik, Family Life in Twentieth-Century America (Greenwood, 2007), pp. 216–17.
  103. ^ Nolan, Michelle. Love on the Racks (McFarland, 2008) p.150
  104. ^ Lisa A. Lewis, The Adoring Audience: Fan Culture and Popular Media (Routledge, 1992), p. 98.
  105. ^ sixtiescity.com Archived March 24, 2012, at the Wayback Machine. Sixties Dance and Dance Crazes
  106. ^ R. Aquila, That old-time rock & roll: a chronicle of an era, 1954–1963 (University of Illinois Press, 2000), p. 10.
  107. ^ Campbell, Michael; James Brody (1999). Rock and Roll: An Introduction. New York, NY: Schirmer Books. pp. 354–55.


This article uses material from the Wikipedia article "Rock and roll", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Music

3d,printed,3dprinting,3dprint,music,song,dvd,dcrom,schellak,top hit