Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
PARTadmin -> Roles category -> Display index page -> Status indicating bitmaps for table view dialog
Copy the used bitmaps into the $CADENAS_SETUP/bitmaps directory.
Maximum bitmap size is 16 x 16 px.
You can assign as many conditions to status lights (colors and symbols) as you wish.
The function Bitmaps can also be used if no Export condition is used.
Note | |
---|---|
Defining status bitmaps and the export condition (see General index page) are basically two different functions which can interact. |
The following combinations are possible:
Export condition used in the General index page AND no Bitmaps function:
=> The red-green status bitmaps are shown.
Meaning: If the condition, which is inserted under Export condition, meets, then green is shown; if not, then red is shown.
See Section 5.6.5.2.1, “ Tabbed page "General" ” -> Export condition.
Export condition in the General index page not used AND no entries under Bitmaps:
Export condition in the General index page not used AND Bitmaps function used:
=> You can use as much bitmaps (colors) as desired. There is no export restriction.
Export condition in the General index page used AND Bitmaps function used:
=> You can use as many bitmaps (colors) as you like. There is a export restriction. Only parts which meet the export condition may be exported. Please regard that the condition under Export condition and the condition under Bitmaps work together.
The used status bitmaps are according to the ones used in the catalog index.
3 = Dark green = Already usesd at all locations 2 = Middle green = Already used at two locations 1 = Light green = Already uses at on location 0 = Yellow = ERP number available Red = No ERP number available
Tip | |
---|---|
If you want to follow the example by yourself, see the settings in the PLDBDEMO database instance with user "location" in the role "LOC1" |
PARTadmin -> "Roles" category -> "Display" index page: "Status indicating bitmaps for table view" dialog
For example insert the following in the Condition column:
((LOC1.EQ.'x').AND.(LOC2.EQ.'x').AND.(LOC3.EQ.'x'))
Meaning: If each of the "LOC1" AND "LOC2" AND "LOC3" column contain a 'x', then the condition is fulfilled. Then the bitmap defined in the Bitmap column is shown.
In the Tooltip column you insert a placeholder. This term is automatically inserted in the translation table on the Translations index page. You can insert there as many translations as you like. Now when you move the mouse cursor over a status bitmap, the translation is displayed.
The following figure shows the result in PARTdataManager, once in the table view and once in the list view.