A shield is a piece of personal armour held in the hand or mounted on the wrist or forearm. Shields are used to intercept specific attacks, whether from close-ranged weaponry or projectiles such as arrows, by means of active blocks, instead of providing passive protection.
Shields vary greatly in size, ranging from large panels that protect the user's whole body to small models (such as the buckler) that were intended for hand-to-hand-combat use. Shields also vary a great deal in thickness; whereas some shields were made of relatively deep, absorbent, wooden planking to protect soldiers from the impact of spears and crossbow bolts, others were thinner and lighter and designed mainly for deflecting blade strikes. Finally, shields vary greatly in shape, ranging in roundness to angularity, proportional length and width, symmetry and edge pattern; different shapes provide more optimal protection for infantry or cavalry, enhance portability, provide secondary uses such as ship protection or as a weapon and so on.
In prehistory and during the era of the earliest civilisations, shields were made of wood, animal hide, woven reeds or wicker. In classical antiquity, the Barbarian Invasions and the Middle Ages, they were normally constructed of poplar tree, lime or another split-resistant timber, covered in some instances with a material such as leather or rawhide and often reinforced with a metal boss, rim or banding. They were carried by foot soldiers, knights and cavalry.
Depending on time and place, shields could be round, oval, square, rectangular, triangular, bilabial or scalloped. Sometimes they took on the form of kites or flatirons, or had rounded tops on a rectangular base with perhaps an eye-hole, to look through when used with combat. The shield was held by a central grip or by straps that went over or around the user's arm.
Often shields were decorated with a painted pattern or an animal representation to show their army or clan. These designs developed into systematized heraldic devices during the High Middle Ages for purposes of battlefield identification. Even after the introduction of gunpowder and firearms to the battlefield, shields continued to be used by certain groups. In the 18th century, for example, Scottish Highland fighters liked to wield small shields known as targes, and as late as the 19th century, some non-industrialized peoples (such as Zulu warriors) employed them when waging war.
In the 20th and 21st century, shields have been used by military and police units that specialize in anti-terrorist actions, hostage rescue, riot control and siege-breaking. The modern term usually refers to a device that is held in the hand or attached to the arm, as opposed to an armored suit or a bullet-proof vest. Shields are also sometimes mounted on vehicle-mounted weapons to protect the operator.