powered by CADENAS

Social Share

Snow globe (3369 views - Interior Design)

A snow globe (also called a "waterglobe", "snowstorm", or "snowdome") is a transparent sphere, traditionally made of glass, enclosing a miniaturized scene of some sort, often together with a model of a landscape. The sphere also encloses the water in the globe; the water serves as the medium through which the "snow" falls. To activate the snow, the globe is shaken to churn up the white particles. The globe is then placed back in its position and the flakes fall down slowly through the water. Snow globes sometimes have a built-in music box that plays a song. Some snow globes have a design around the outerbase for decoration.
Go to Article

Explanation by Hotspot Model

Snow globe

Snow globe

A snow globe (also called a "waterglobe", "snowstorm",[1] or "snowdome") is a transparent sphere, traditionally made of glass, enclosing a miniaturized scene of some sort, often together with a model of a landscape. The sphere also encloses the water in the globe; the water serves as the medium through which the "snow" falls. To activate the snow, the globe is shaken to churn up the white particles. The globe is then placed back in its position and the flakes fall down slowly through the water. Snow globes sometimes have a built-in music box that plays a song. Some snow globes have a design around the outerbase for decoration.

History

When exactly the first snow globes became well-known remains uncertain, but the popularity seemingly dates to the early 19th century in France. They may have appeared for glass blowers as adjuncts to paperweight, which had become popular a few years earlier. Snow globes were exhibited at the Paris Universal Expo of 1878, and by 1879 at least five or more companies were producing and selling snow globes throughout Europe.

In 1889, a snow globe containing a model of the newly built Eiffel Tower was produced to commemorate the International Exposition in Paris, which marked the centenary of the French Revolution. Snow globes became popular in England during the Victorian era and, in the early 1920s, crossed the Atlantic to the United States of America where they became a popular collectors item. Many of these globes were produced by Atlas Crystal Works, which had factories in Germany and America.

At the end of the 19th century the Austrian Erwin Perzy, a producer of surgical instruments, invented the so-called Schneekugel (snow globe) and got the first patent for it. Originally his goal was to develop an extra bright lightsource for use as a surgical lamp. As he tried to intensify the candlepower of a so-called Schusterkugel (a water filled flask used to focus light since the Middle Ages) with particles made out of different materials for reflection purpose, the effect reminded him of snowfall and it's said that by this he got the idea for a snow globe. He then built his first actual globe with the basilica of Mariazell as a model in it. Because of the great request for his snow globes, Perzy, along with his brother Ludwig opened a shop in Vienna, where the production continues until today as a family business.[2][3] Today the globes get exported throughout the world; the material out of which the "snow" is made is handed down from generation to generation as a production secret (it should float as long as possible in the water before sinking down).

In the United States, the first snow globe-related patent was granted in 1927 to Joseph Garaja of Pittsburgh, Pennsylvania. In 1929, Garaja convinced Novelty Pool Ornaments to manufacture a fish version underwater.

In America, during the 1940s, snow globes were often used for advertising. In Europe, during the 1940s and 1950s, religious snow globes were common gifts for Catholic children. Snow globes have appeared in a number of film scenes, the most famous of which is the opening of the 1941 classic Citizen Kane.

In the 1950s, the globes, which were previously made of glass, became available in plastic. Currently, there are many different types of snow globes available. These globes are produced by a number of countries and range from the mass-produced versions of Hong Kong and China to the finely crafted types still produced in Austria. Snow globes feature diverse scenes, ranging from the typical holiday souvenirs to more eclectic collectibles featuring Christmas scenes, Disney characters, popular icons, animals, military figures, historical scenes, etc. Snow globes have even been used for election campaigns. Since 2000 fashion and luxury brands, such as Louis Vuitton, Ladurée, Sonia Rykiel, or Martin Margiela, got hold of the trend and grew particularly fond of snow globes as collectible totems and emblems of their brand image. Such enthusiasm was reinforced by presence in numerous art collections of contemporary artists Walter Martin & Paloma Muñoz (also known as Martin & Muñoz) who use snow globes as a medium, or museums who paid tribute to famous artists such as French sculptor Auguste Rodin in creating high quality numbered glass dome snow globes.

Contents

Initially snow globes consisted of a heavy lead glass dome which was placed over a ceramic figure or tableau on a black cast ceramic base, filled with water and then sealed. The snow or "flitter" was created by use of bone chips or pieces of porcelain, sand or even sawdust. As they became more sophisticated, the glass became thinner, the bases were lighter (Bakelite was popular during the Art Deco period) and the snow was made out of particles of gold foil or non-soluble soap flakes. For health and safety reasons, white plastic has become more common in the construction of modern snow globes. The liquid has evolved to light oil and then a mixture of water and antifreeze (glycerin or glycol). An added benefit was that glycerin and glycol slowed the descent of the snow. Caution should be taken if a snow globe is broken because the liquid, which can contain antifreeze, can be deadly to cats and dogs if ingested or licked off their fur.[4]

Embellishments

Today's snow globes can include music boxes, moving parts, internal lights, and even electric motors that make the "snow" move so that it is no longer necessary to shake the globe. Some also have central slots for positioning items such as photographs.

Forced-air globes

Beginning in 2005, many U.S. stores sell inflatable snow globes as part of their Christmas décor. These have a base with a blower, forcing air which carries styrofoam pellets from the bottom and through a tube up the back to the top, where they are blown out and fall down inside the front, which is made of transparent vinyl. The rest of the globe, including the characters inside, are made of colorful nylon fabric. These globes are typically large decorations for the front yard, and are lighted internally with a few C7 (nightlight-type) incandescent light bulbs (which are enclosed in plastic spheres to prevent heat damage to the fabric).

A variation on this is the "tornado globe", where small foam objects spin around inside a globe. This is more common for Halloween, where foam bats or sometimes ghosts may fly around the Halloween figures in the middle. These were most common in 2006, and come in both large inflatables, and smaller tabletop versions with rigid plastic globes about 8 to 12 inches or 20 to 30 centimeters in diameter. As with the snow globes, static cling often causes the foam to stick to the plastic (especially vinyl) when humidity is low, while condensation will do the same thing on outdoor inflatables when humidity is high, or rainwater has seeped in while it is deflated.

Cultural references

In modern culture, snow globes often symbolize childhood, innocence, or so-called "happy days". However, they are also sometimes used, with dark humor, to evoke more gruesome scenes.

Film

  • The film Citizen Kane (1941) starts with Charles Foster Kane in a bed holding a snow globe, uttering, "Rosebud ..."; the globe slips from his dying hand and smashes. The film historian Paul Malcolm noted the scattered content of the snow globe parallels the scattered or "dispersed" story of Kane to come in the film.[5]
  • The special edition VHS release of Fargo (1996) included a snow globe which, when shaken, stirred up both snow and "blood".[6]
  • In the film Unfaithful (2002), Edward Sumner (Richard Gere) uses the snow globe he gave as a present to his wife Connie (Diane Lane) as a weapon to kill her lover Paul Martel (Olivier Martinez).
  • The film Coraline, based on a novel by Neil Gaiman, had the child Coraline's parents being imprisoned in a souvenir snow globe of the Detroit Zoo.

The Santa Clause

Publications

  • In Libba Bray's book Going Bovine (2009), snow globes are used periodically as metaphors for the constraints of reality and life as we know it. At the end of the book, the main characters smash them, claiming that they are "freeing the snow globes".[citation needed]
  • In Erica Rand's The Ellis Island Snow Globe (2005), a snow globe from the Ellis Island gift shop is one of the objects that "demonstrate how some narratives are promoted while others are repressed to represent a particular version of United States history and citizenship."[7][8]

Television

  • The series finale of St. Elsewhere famously ends with the implication that the events of the whole series were nothing more than a mere fantasy imagined by Tommy Westphall, an autistic boy whose most treasured possession is a snow globe containing a small model of a building resembling the hospital in which the series is set.[citation needed]
  • In Sons of Anarchy, Season 5, Episode 6 ("Small World"), Jax forms an alliance with Damon Pope and détente among SAMCRO, "black" (the One-Niners), "brown" (the Mayans), and "yellow" (the Triad). Jax then tasks Tig with finding a pipe with which to kill the prison guard who had facilitated the fatal beating by other prisoners of Jax's childhood friend Opie, at Stockton, and who had said the guards were betting on how long it would take Opie to die. Tig can't find a pipe, and instead hands Jax a hammer and a musical "It's a Small World" snow globe. Jax chooses the globe and winds it up; he, Tig, and Chibs slowly circle round the guard as in the ride, Ring a Ring o' Roses, and then Jax beats the guard to death with the globe, all while the globe tinkles the song "It's a Small World (After All)".
  • In 2014, in the final seconds of the last episode of The Late Late Show with Craig Ferguson, a snow globe is shown on his bedside table, accompanied by Journey's song "Don't Stop Believin'". The custom snow globe used was specially created for the CBS production, including the host's likeness in the middle, with his sidekicks Geoff the robot skeleton and Secretariat the pantomime horse.[citation needed]

Art

See also



This article uses material from the Wikipedia article "Snow globe", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Interior Design

3D,interior,architecture,furniture,kitchen,sanitary,bath,design,art