powered by CADENAS

Social Share

Sword (6030 views - History & Epochal Times)

A sword is a bladed weapon intended for slashing or thrusting that is longer than a knife or dagger. The precise definition of the term varies with the historical epoch or the geographical region under consideration. A sword consists of a long blade attached to a hilt. The blade can be straight or curved. Thrusting swords have a pointed tip on the blade, and tend to be straighter; slashing swords have sharpened cutting edge on one or both sides of the blade, and are more likely to be curved. Many swords are designed for both thrusting and slashing. Historically, the sword developed in the Bronze Age, evolving from the dagger; the earliest specimens date to about 1600 BC. The later Iron Age sword remained fairly short and without a crossguard. The spatha, as it developed in the Late Roman army, became the predecessor of the European sword of the Middle Ages, at first adopted as the Migration period sword, and only in the High Middle Ages, developed into the classical arming sword with crossguard. The word sword continues the Old English, sweord. The use of a sword is known as swordsmanship or (in an early modern or modern context) as fencing. In the Early Modern period, western sword design diverged into roughly two forms, the thrusting swords and the sabers. The thrusting swords such as the rapier and eventually the smallsword were designed to impale their targets quickly and inflict deep stab wounds. Their long and straight yet light and well balanced design made them highly maneuverable and deadly in a duel but fairly ineffective when used in a slashing or chopping motion. A well aimed lunge and thrust could end a fight in seconds with just the sword's point, leading to the development of a fighting style which closely resembles modern fencing. The saber (sabre) and similar blades such as the cutlass were built more heavily and were more typically used in warfare. Built for slashing and chopping at multiple enemies, often from horseback, the saber's long curved blade and slightly forward weight balance gave it a deadly character all its own on the battlefield. Most sabers also had sharp points and double edged blades, making them capable of piercing soldier after soldier in a cavalry charge. Sabers continued to see battlefield use until the early 20th century. The US Navy kept tens of thousands of sturdy cutlasses in their armory well into World War II and many were issued to marines in the Pacific as jungle machetes. Non-European weapons called "sword" include single-edged weapons such as the Middle Eastern scimitar, the Chinese dao and the related Japanese katana. The Chinese jian is an example of a non-European double-edged sword, like the European models derived from the double-edged Iron Age sword.
Go to Article

Explanation by Hotspot Model

Sword

Sword

A sword is a bladed weapon intended for slashing or thrusting that is longer than a knife or dagger. The precise definition of the term varies with the historical epoch or the geographical region under consideration. A sword consists of a long blade attached to a hilt. The blade can be straight or curved. Thrusting swords have a pointed tip on the blade, and tend to be straighter; slashing swords have sharpened cutting edge on one or both sides of the blade, and are more likely to be curved. Many swords are designed for both thrusting and slashing.

Historically, the sword developed in the Bronze Age, evolving from the dagger; the earliest specimens date to about 1600 BC. The later Iron Age sword remained fairly short and without a crossguard. The spatha, as it developed in the Late Roman army, became the predecessor of the European sword of the Middle Ages, at first adopted as the Migration period sword, and only in the High Middle Ages, developed into the classical arming sword with crossguard. The word sword continues the Old English, sweord.[1]

The use of a sword is known as swordsmanship or (in an early modern or modern context) as fencing. In the Early Modern period, western sword design diverged into roughly two forms, the thrusting swords and the sabers.

The thrusting swords such as the rapier and eventually the smallsword were designed to impale their targets quickly and inflict deep stab wounds. Their long and straight yet light and well balanced design made them highly maneuverable and deadly in a duel but fairly ineffective when used in a slashing or chopping motion. A well aimed lunge and thrust could end a fight in seconds with just the sword's point, leading to the development of a fighting style which closely resembles modern fencing.

The saber (sabre) and similar blades such as the cutlass were built more heavily and were more typically used in warfare. Built for slashing and chopping at multiple enemies, often from horseback, the saber's long curved blade and slightly forward weight balance gave it a deadly character all its own on the battlefield. Most sabers also had sharp points and double edged blades, making them capable of piercing soldier after soldier in a cavalry charge. Sabers continued to see battlefield use until the early 20th century. The US Navy kept tens of thousands of sturdy cutlasses in their armory well into World War II and many were issued to marines in the Pacific as jungle machetes.

Non-European weapons called "sword" include single-edged weapons such as the Middle Eastern scimitar, the Chinese dao and the related Japanese katana. The Chinese jian is an example of a non-European double-edged sword, like the European models derived from the double-edged Iron Age sword.

History

Ancient history

The first weapons that can be described as "swords" date to around 3300 BC. They have been found in Arslantepe, Turkey, are made from arsenical bronze, and are about 60 cm (24 in) long.[2][3] Some of them are inlaid with silver.

Bronze Age

The sword developed from the knife or dagger. A knife is unlike a dagger in that a knife has only one cutting surface, while a dagger has two cutting surfaces. when the construction of longer blades became possible, from the late 3rd millennium BC in the Middle East, first in arsenic copper, then in tin-bronze.

Blades longer than 60 cm (24 in) were rare and not practical until the late Bronze Age because the tensile strength of bronze is relatively low, and consequently longer blades would bend easily. The development of the sword out of the dagger was gradual; the first weapons that can be classified as swords without any ambiguity are those found in Minoan Crete, dated to about 1700 BC, reaching a total length of more than 100 cm. These are the "type A" swords of the Aegean Bronze Age.

One of the most important, and longest-lasting, types swords of the European Bronze Age was the Naue II type (named for Julius Naue who first described them), also known as Griffzungenschwert (lit. "grip-tongue sword"). This type first appears in c. the 13th century BC in Northern Italy (or a general Urnfield background), and survives well into the Iron Age, with a life-span of about seven centuries. During its lifetime, metallurgy changed from bronze to iron, but not its basic design.

Naue II swords were exported from Europe to the Aegean, and as far afield as Ugarit, beginning about 1200 BC, i.e. just a few decades before the final collapse of the palace cultures in the Bronze Age collapse.[4] Naue II swords could be as long as 85 cm, but most specimens fall into the 60 to 70 cm range. Robert Drews linked the Naue Type II Swords, which spread from Southern Europe into the Mediterranean, with the Bronze Age collapse.[5] Naue II swords, along with Nordic full-hilted swords, were made with functionality and aesthetics in mind. [6]The hilts of these swords were beautifully crafted and often contained false rivets in order to make the sword more visually appealing. Swords coming from northern Denmark and northern Germany usually contained three or more fake rivets in the hilt.[7]

Sword production in China is attested from the Bronze Age Shang Dynasty.[8] The technology for bronze swords reached its high point during the Warring States period and Qin Dynasty. Amongst the Warring States period swords, some unique technologies were used, such as casting high tin edges over softer, lower tin cores, or the application of diamond shaped patterns on the blade (see sword of Goujian). Also unique for Chinese bronzes is the consistent use of high tin bronze (17–21% tin) which is very hard and breaks if stressed too far, whereas other cultures preferred lower tin bronze (usually 10%), which bends if stressed too far. Although iron swords were made alongside bronze, it was not until the early Han period that iron completely replaced bronze.[9]

In South Asia earliest available Bronze age swords of copper were discovered in the Harappan sites, in present-day Pakistan, and date back to 2300 BC[citation needed]. Swords have been recovered in archaeological findings throughout the Ganges-Jamuna Doab region of India, consisting of bronze but more commonly copper.[10] Diverse specimens have been discovered in Fatehgarh, where there are several varieties of hilt.[10] These swords have been variously dated to times between 1700–1400 BC, but were probably used more notably in the opening centuries of the 1st millennium BC.[10]

Iron Age

Iron became increasingly common from the 13th century B.C. Before that the use of swords was less frequent. The iron was not quench-hardened although often containing sufficient carbon, but work-hardened like bronze by hammering. This made them comparable or only slightly better in terms of strength and hardness to bronze swords. They could still bend during use rather than spring back into shape. But the easier production, and the better availability of the raw material for the first time permitted the equipment of entire armies with metal weapons, though Bronze Age Egyptian armies were sometimes fully equipped with bronze weapons.[11]

Ancient swords are often found at burial sites. The sword was often placed on the right side of the corpse. However, there are exceptions to this. A lot of times the sword was kept over the corpse. In many late Iron Age graves, the sword and the scabbard were bent at 180 degrees. It was known as killing the sword. Thus they might have considered swords as the most potent and powerful object.[12]

Greco-Roman antiquity

By the time of Classical Antiquity and the Parthian and Sassanid Empires in Iran, iron swords were common. The Greek xiphos and the Roman gladius are typical examples of the type, measuring some 60 to 70 cm (24 to 28 in).[13][14] The late Roman Empire introduced the longer spatha[15] (the term for its wielder, spatharius, became a court rank in Constantinople), and from this time, the term longsword is applied to swords comparatively long for their respective periods.[16]

Swords from the Parthian and Sassanian Empires were quite long, the blades on some late Sassanian swords being just under a metre long.

Swords were also used to administer various physical punishments, such as non-surgical amputation or capital punishment by decapitation. The use of a sword, an honourable weapon, was regarded in Europe since Roman times as a privilege reserved for the nobility and the upper classes.[17]

The Periplus of the Erythraean Sea mentions swords of Indian iron and steel being exported from India to Greece.[18] Sri Lankan and Indian Blades made of Damascus steel also found their way into Persia.[18]

Persian antiquity

In the first millennium BC the Persian armies used a sword that was originally of Scythian design called the akinaka (acinaces). However, the great conquests of the Persians made the sword more famous as a Persian weapon, to the extent that the true nature of the weapon has been lost somewhat as the name Akinaka has been used to refer to whichever form of sword the Persian army favoured at the time.

It is widely believed that the original akinaka was a 14 to 18 inch double-edged sword. The design was not uniform and in fact identification is made more on the nature of the scabbard than the weapon itself; the scabbard usually has a large, decorative mount allowing it to be suspended from a belt on the wearer’s right side. Because of this, it is assumed that the sword was intended to be drawn with the blade pointing downwards ready for surprise stabbing attacks.

In the 12th century, the Seljuq dynasty had introduced the curved shamshir to Persia, and this was in extensive use by the early 16th century.

Chinese antiquity

Chinese steel swords made their first appearance in the later part of the Western Zhou Dynasty, but were not widely used until the 3rd century BC Han Dynasty.[9] The Chinese Dao (刀 pinyin dāo) is single-edged, sometimes translated as sabre or broadsword, and the Jian (劍or剑 pinyin jiàn) is double-edged. The zhanmadao (literally "horse chopping sword"), an extremely long, anti-cavalry sword from the Song dynasty era.

Middle Ages

Europe

Battle scene from the Morgan Bible of Louis IX showing 13th-century swords

During the Middle Ages sword technology improved, and the sword became a very advanced weapon. It was frequently used by men in battle, particularly during an attack. The spatha type remained popular throughout the Migration period and well into the Middle Ages. Vendel Age spathas were decorated with Germanic artwork (not unlike the Germanic bracteates fashioned after Roman coins). The Viking Age saw again a more standardized production, but the basic design remained indebted to the spatha.[19]

Around the 10th century, the use of properly quenched hardened and tempered steel started to become much more common than in previous periods. The Frankish 'Ulfberht' blades (the name of the maker inlaid in the blade) were of particularly consistent high quality.[20] Charles the Bald tried to prohibit the export of these swords, as they were used by Vikings in raids against the Franks.

Wootz steel which is also known as Damascus steel was a unique and highly prized steel developed on the Indian subcontinent as early as the 5th century BC. Its properties were unique due to the special smelting and reworking of the steel creating networks of iron carbides described as a globular cementite in a matrix of pearlite. The use of Damascus steel in swords became extremely popular in the 16th and 17th centuries.[nb 1][21]

It was only from the 11th century that Norman swords began to develop the crossguard (quillons). During the Crusades of the 12th to 13th century, this cruciform type of arming sword remained essentially stable, with variations mainly concerning the shape of the pommel. These swords were designed as cutting weapons, although effective points were becoming common to counter improvements in armour, especially the 14th-century change from mail to plate armour.[22]

It was during the 14th century, with the growing use of more advanced armour, that the hand and a half sword, also known as a "bastard sword", came into being. It had an extended grip that meant it could be used with either one or two hands. Though these swords did not provide a full two-hand grip they allowed their wielders to hold a shield or parrying dagger in their off hand, or to use it as a two-handed sword for a more powerful blow.[23]

In the Middle Ages, the sword was often used as a symbol of the word of God. The names given to many swords in mythology, literature, and history reflected the high prestige of the weapon and the wealth of the owner.[24]

Greater Middle East

The earliest evidence of curved swords, or scimitars (and other regional variants as the Arabian saif, the Persian shamshir and the Turkic kilij) is from the 9th century, when it was used among soldiers in the Khurasan region of Persia.[25]

East Asia

A Japanese wakizashi of the 17th century, with its koshirae and shirasaya.

As steel technology improved, single-edged weapons became popular throughout Asia. Derived from the Chinese Jian or dao, the Korean hwandudaedo are known from the early medieval Three Kingdoms. Production of the Japanese tachi, a precursor to the katana, is recorded from ca. 900 AD (see Japanese sword).[26]

Japan was famous for the swords it forged in the early 13th century for the class of warrior-nobility known as the Samurai. The types of swords used by the Samurai included the ōdachi (extra long field sword), tachi (long cavalry sword), katana (long sword), and wakizashi (shorter companion sword for katana). Japanese swords that pre-date the rise of the samurai caste include the tsurugi (straight double-edged blade) and chokutō (straight one-edged blade).[27] Japanese swordmaking reached the height of its development in the 15th and 16th centuries, when samurai increasingly found a need for a sword to use in closer quarters, leading to the creation of the modern katana.[28]

Western historians have said that Japanese katana were among the finest cutting weapons in world military history.[29][30][31]

Indian Subcontinent

Khanda is a double-edge straight sword. It is often featured in religious iconography, theatre and art depicting the ancient history of India. Some communities venerate the weapon as a symbol of Shiva. It is a common weapon in the martial arts in the Indian subcontinent.[32] Khanda often appears in Hindu, Buddhist and Sikh scriptures and art.[33] In Sri Lanka, a unique wind furnace was used to produce the high quality steel. This gave the blade a very hard cutting edge and beautiful patterns. For these reasons it became a very popular trading material.[34]

The Urumi:(Tamil: சுருள் பட்டாக்கத்தி surul pattai, lit. curling blade; Sinhalese: එතුණු කඩුව ethunu kaduwa; Hindi: aara) is a longsword with a flexible whip-like blade from India. Originating in the country's southern states, it is thought to have existed as far back as the Maurya dynasty (322–185 BC). The urumi is considered one of the most difficult weapons to master due to the risk of injuring oneself. It is treated as a steel whip,[35] and therefore requires prior knowledge of that weapon.

The Firangi (/fəˈrɪŋɡ/; derived from the Arabic term for a Western European a "Frank") was a sword type which used blades manufactured in Western Europe and imported by the Portuguese, or made locally in imitation of European blades. Because of its length the firangi is usually regarded as primarily a cavalry weapon. The sword has been especially associated with the Marathas, who were famed for their cavalry. However, the firangi was also widely used by Sikhs and Rajputs.[36]

The Talwar:(Hindi:तलवार) is a type of curved sword from India and other countries of the Indian subcontinent, it was adopted by communities such as Rajputs, Sikhs and Marathas, who favored the sword as their main weapon. It became more widespread in the medieval era.[37][38]

Southeast Asia

In Indonesia, the images of Indian style swords can be found in Hindu gods statues from ancient Java circa 8th to 10th century. However the native types of blade known as kris, parang, klewang and golok were more popular as weapons. These daggers are shorter than sword but longer than common dagger.

Kampilan from the Philippines.

In The Philippines, traditional large swords known as the Kampilan and the Panabas were used in combat by the natives. A notable wielder of the kampilan was Lapu-Lapu, the king of Mactan and his warriors who defeated the Spaniards and killed Portuguese explorer Ferdinand Magellan at the Battle of Mactan on 27 April 1521.[39] Traditional swords in the Philippines were immediately banned, but the training in swordsmanship was later hidden from the occupying Spaniards by practices in dances. But because of the banning, Filipinos were forced to use swords that were disguised as farm tools. Bolos and baliswords were used during the revolutions against the colonialists not only because ammunition for guns was scarce, but also for concealability while walking in crowded streets and homes. Bolos were also used by young boys who joined their parents in the revolution and by young girls and their mothers in defending the town while the men were on the battlefields. During the Philippine–American War in events such as the Balangiga Massacre, most of an American company was hacked to death or seriously injured by bolo-wielding guerillas in Balangiga, Samar.[40] When the Japanese took control of the country, several American special operations groups stationed in the Philippines were introduced to the Filipino Martial Arts and swordsmanship, leading to this style reaching America despite the fact that natives were reluctant to allow outsiders in on their fighting secrets.[41]

Late Middle Ages and Renaissance

From around 1300 to 1500, in concert with improved armour, innovative sword designs evolved more and more rapidly. The main transition was the lengthening of the grip, allowing two-handed use, and a longer blade. By 1400, this type of sword, at the time called langes Schwert (longsword) or spadone, was common, and a number of 15th- and 16th-century Fechtbücher offering instructions on their use survive. Another variant was the specialized armour-piercing swords of the estoc type. The longsword became popular due to its extreme reach and its cutting and thrusting abilities.[42]
1548 depiction of a Zweihänder used against pikes in the Battle of Kappel

The estoc became popular because of its ability to thrust into the gaps between plates of armour.[43] The grip was sometimes wrapped in wire or coarse animal hide to provide a better grip and to make it harder to knock a sword out of the user's hand.[44]

A number of manuscripts covering longsword combat and techniques dating from the 13th–16th centuries exist in German,[45] Italian, and English,[46] providing extensive information on longsword combatives as used throughout this period. Many of these are now readily available online.[45][46]

In the 16th century, the large zweihänder was used by the elite German and Swiss mercenaries known as doppelsöldners.[47] Zweihänder, literally translated, means two-hander. The zweihänder possesses a long blade, as well as a huge guard for protection. It is estimated that some zweihänder swords were over 6 feet (1.8 m) long, with the one ascribed to Frisian warrior Pier Gerlofs Donia being 7 feet (2.13 m) long.[48] The gigantic blade length was perfectly designed for manipulating and pushing away enemy pole-arms, which were major weapons around this time, in both Germany and Eastern Europe. Doppelsöldners also used katzbalgers, which means 'cat-gutter'. The katzbalger's S-shaped guard and 2-foot-long (0.61 m) blade made it perfect for bringing in when the fighting became too close to use a zweihänder.[49]

Civilian use of swords became increasingly common during the late Renaissance, with duels being a preferred way to honourably settle disputes. The practice of civilian duelling, with specifically designed civilian swords such as the Italian Cinquedea and Swiss Baselard, became so popular that according to one scholar: "In France during the reign of Henry IV (1589–1610), more than 4,000 French aristocrats were killed in duels in an eighteen-year period...During the reign of Louis XIII (1610–1643)...in a twenty-year period 8,000 pardons were issued for murders associated with duels."[50]

The side-sword was a type of war sword used by infantry during the Renaissance of Europe. This sword was a direct descendant of the arming sword. Quite popular between the 16th and 17th centuries, they were ideal for handling the mix of armoured and unarmoured opponents of that time. A new technique of placing one's finger on the ricasso to improve the grip (a practice that would continue in the rapier) led to the production of hilts with a guard for the finger. This sword design eventually led to the development of the civilian rapier, but it was not replaced by it, and the side-sword continued to be used during the rapier's lifetime. As it could be used for both cutting and thrusting, the term cut and thrust sword is sometimes used interchangeably with side-sword.[51] Also of note is that as rapiers became more popular, attempts were made to hybridize the blade, sacrificing the effectiveness found in each unique weapon design. These are still considered side-swords and are sometimes labeled sword rapier or cutting rapier by modern collectors.

Also of note, side-swords used in conjunction with bucklers became so popular that it caused the term swashbuckler to be coined. This word stems from the new fighting style of the side-sword and buckler which was filled with much "swashing and making a noise on the buckler".[52]

Within the Ottoman Empire, the use of a curved sabre called the Yatagan started in the mid-16th century. It would become the weapon of choice for many in Turkey and the Balkans.[53]

The sword in this time period was the most personal weapon, the most prestigious, and the most versatile for close combat, but it came to decline in military use as technology, such as the crossbow and firearms changed warfare. However, it maintained a key role in civilian self-defence.[54]

Early Modern period

Military sword

A single-edged type of sidearm used by the Hussites was popularized in 16th-century Germany under its Czech name Dusack, also known as Säbel auf Teutsch gefasst ("sabre fitted in the German manner").[55] A closely related weapon is the schnepf or Swiss sabre used in Early Modern Switzerland.[56]

The cut-and-thrust mortuary sword was used after 1625 by cavalry during the English Civil War. This (usually) two-edged sword sported a half-basket hilt with a straight blade some 90–105 cm long. Later in the 17th century, the swords used by cavalry became predominantly single-edged. The so-called walloon sword (épée wallone)[57] was common in the Thirty Years' War and Baroque era.[58] Its hilt was ambidextrous with shell-guards and knuckle-bow that inspired 18th century continental hunting hangers.[59] Following their campaign in the Netherlands in 1672, the French began producing this weapon as their first regulation sword.[60] Weapons of this design were also issued to the Swedish army from the time of Gustavus Adolphus until as late as the 1850s.[61]

Duelling sword

The rapier is believed to have evolved either from the Spanish espada ropera or from the swords of the Italian nobility somewhere in the later part of the 16th century.[62][63] The rapier differed from most earlier swords in that it was not a military weapon but a primarily civilian sword. Both the rapier and the Italian schiavona developed the crossguard into a basket-shaped guard for hand protection.[64] During the 17th and 18th centuries, the shorter smallsword became an essential fashion accessory in European countries and the New World, though in some places such as the Scottish Highlands large swords as the basket-hilted broadsword were preferred, and most wealthy men and military officers carried one slung from a belt. Both the smallsword and the rapier remained popular dueling swords well into the 18th century.[65]

As the wearing of swords fell out of fashion, canes took their place in a gentleman's wardrobe. This developed to the gentlemen in the Victorian era to use the umbrella. Some examples of canes—those known as sword canes or swordsticks—incorporate a concealed blade. The French martial art la canne developed to fight with canes and swordsticks and has now evolved into a sport. The English martial art singlestick is very similar. With the rise of the pistol duel, the duelling sword fell out of fashion long before the practice of duelling itself. By about 1770, English duelists enthusiastically adopted the pistol, and sword duels dwindled.[66] However, the custom of duelling with epées persisted well into the 20th century in France. Such modern duels were not fought to the death, the duellists' aim was instead merely to draw blood from the opponent's sword arm.[67]

Modern history

Military sidearm

Towards the end of its useful life, the sword served more as a weapon of self-defence than for use on the battlefield, and the military importance of swords steadily decreased during the Modern Age. Even as a personal sidearm, the sword began to lose its preeminence in the early 19th century, reflecting the development of reliable handguns.[54]

However, swords were still used in combat, especially in Colonial Wars between native populations and Colonial Empires. For example, during the Aceh War the Acehnese Klewangs, a sword similar to the machete, proved very effective in close quarters combat with Dutch troops, leading the Royal Netherlands East Indies Army to adopt a heavy cutlass, also called klewang (very similar in appearance to the US Navy Model 1917 Cutlass) to counter it. Mobile troops armed with carbines and klewangs succeeded in suppressing Aceh resistance where traditional infantry with rifle and bayonet had failed. From that time on until the 1950s the Royal Dutch East Indies Army, Royal Dutch Army, Royal Dutch Navy and Dutch police used these cutlasses called Klewang.[68][69]

Swords continued in general peacetime use by cavalry of most armies during the years prior to World War I. For example, the British Army formally adopted a completely new design of cavalry sword in 1908, almost the last change in British Army weapons before the outbreak of the war.[70] At the outbreak of World War I infantry officers in all combatant armies still carried swords as part of their field equipment. On mobilization in August 1914 all serving British Army officers were required to have their swords sharpened as the only peacetime use of the weapon had been for saluting on parade.[71] The high visibility and limited practical use of the sword however led to it being abandoned within weeks, although most cavalry continued to carry sabres throughout the War. It was not until the late 1920s and early 1930s that this historic weapon was finally discarded for all but ceremonial purposes by most remaining horse mounted regiments of Europe and the Americas.

In China troops used the long anti-cavalry Miao dao well into the Second Sino-Japanese War. The last units of British heavy cavalry switched to using armoured vehicles as late as 1938. Swords and other dedicated melee weapons were used occasionally by many countries during World War II, but typically as a secondary weapon as they were outclassed by coexisting firearms.[72][73][74]

Ceremonial use

Swords are commonly worn as a ceremonial item by officers in many military and naval services throughout the world. Occasions to wear swords include any event in dress uniforms where the rank-and-file carry arms: parades, reviews, courts-martial, tattoos, and changes of command. They are also commonly worn for officers' weddings, and when wearing dress uniforms to church—although they are rarely actually worn in the church itself.

In the British forces they are also worn for any appearance at Court. In the United States, every Naval officer at or above the rank of Lieutenant Commander is required to own a sword, which can be prescribed for any formal outdoor ceremonial occasion; they are normally worn for changes of command and parades. For some Navy parades, cutlasses are issued to Petty Officers and Chief Petty Officers.

In the U.S. Marine Corps every officer must own a sword, which is prescribed for formal parades and other ceremonies where dress uniforms are worn and the rank-and-file are under arms. On these occasions depending on their billet, Marine Staff Non-Commissioned Officers (E-6 and above) may also be required to carry swords, which have hilts of a pattern similar to U.S. Naval officers' swords but are actually sabres. The USMC Model 1859 NCO Sword is the longest continuously-issued edged weapon in the U.S. inventory

The Marine officer swords are of the Mameluke pattern which was adopted in 1825 in recognition of the Marines' key role in the capture of the Tripolitan city of Derna during the First Barbary War.[75] Taken out of issue for approximately 20 years from 1855 until 1875, it was restored to service in the year of the Corps' centennial and has remained in issue since.

Sword replicas

The production of replicas of historical swords originates with 19th-century historicism.[76] Contemporary replicas can range from cheap factory produced look-alikes to exact recreations of individual artifacts, including an approximation of the historical production methods.

Some kinds of swords are still commonly used today as weapons, often as a side arm for military infantry. The Japanese katana, wakizashi and tanto are carried by some infantry and officers in Japan and other parts of Asia and the kukri is the official melee weapon for Nepal. Other swords in use today are the sabre, the scimitar, the shortsword and the machete.[77]

  • In the case of a rat-tail tang, the maker welds a thin rod to the end of the blade at the crossguard; this rod goes through the grip.[citation needed]
  • In traditional construction, Swordsmiths peened such tangs over the end of the pommel, or occasionally welded the hilt furniture to the tang and threaded the end for screwing on a pommel. This style is often referred to as a "narrow" or "hidden" tang. Modern, less traditional, replicas often feature a threaded pommel or a pommel nut which holds the hilt together and allows dismantling.[citation needed]
  • In a "full" tang (most commonly used in knives and machetes), the tang has about the same width as the blade, and is generally the same shape as the grip.[78] In European or Asian swords sold today, many advertised "full" tangs may actually involve a forged rat-tail tang.

Morphology

The sword consists of the blade and the hilt. The term scabbard applies to the cover for the sword blade when not in use.

Blade

There is considerable variation in the detailed design of sword blades. The diagram opposite shows a typical Medieval European sword.

Early iron blades have rounded points due to the limited metallurgy of the time. These were still effective for thrusting against lightly armoured opponents. As armour advanced, blades were made narrower, stiffer and sharply pointed to defeat the armour by thrusting.

Dedicated cutting blades are wide and thin, and often have grooves known as fullers which lighten the blade at the cost of some of the blade's stiffness. The edges of a cutting sword are almost parallel. Blades oriented for the thrust have thicker blades, sometimes with a distinct midrib for increased stiffness, with a strong taper and an acute point. The geometry of a cutting sword blade allows for acute edge angles. It should be noted, however, that an edge with an acuter angle is more inclined to degrade quickly in combat situations than an edge with a more obtuse angle. Also, an acute edge angle is not the primary factor of a blade's sharpness.[79]

The part of the blade between the center of percussion (CoP) and the point is called the foible (weak) of the blade, and that between the center of balance (CoB) and the hilt is the forte (strong). The section in between the CoP and the CoB is the middle.

The ricasso or shoulder identifies a short section of blade immediately below the guard that is left completely unsharpened. Many swords have no ricasso. On some large weapons, such as the German Zweihänder, a metal cover surrounded the ricasso, and a swordsman might grip it in one hand to wield the weapon more easily in close-quarter combat.[49] The ricasso normally bears the maker's mark.

The tang is the extension of the blade to which the hilt is fitted.

On Japanese blades, the maker's mark appears on the tang under the grip.[80]

Hilt

Hilt of a rapier. In this case, with a swept hilt

The hilt is the collective term for the parts allowing for the handling and control of the blade; these consist of the grip, the pommel, and a simple or elaborate guard, which in post-Viking Age swords could consist of only a crossguard (called a cruciform hilt or quillons). The pommel was originally designed as a stop to prevent the sword slipping from the hand. From around the 11th century onward it became a counterbalance to the blade, allowing a more fluid style of fighting.[dubious ][81] It can also be used as a blunt instrument at close range, and its weight affects the centre of percussion. In later times a sword knot or tassel was sometimes added. By the 17th century, with the growing use of firearms and the accompanying decline in the use of armour, many rapiers and dueling swords had developed elaborate basket hilts, which protect the palm of the wielder and rendered the gauntlet obsolete.[82]

In late medieval and Renaissance era European swords, a flap of leather called the chappe or rain guard was attached to a sword's crossguard at the base of the hilt to protect the mouth of the scabbard and prevent water from entering.[83]

Sword scabbards and suspension

Common accessories to the sword include the scabbard, as well as the sword belt.

  • Scabbard: The scabbard, also known as the sheath, is a protective cover often provided for the sword blade. Over the millennia, scabbards have been made of many materials, including leather, wood, and metals such as brass or steel. The metal fitting where the blade enters the leather or metal scabbard is called the throat, which is often part of a larger scabbard mount, or locket, that bears a carrying ring or stud to facilitate wearing the sword. The blade's point in leather scabbards is usually protected by a metal tip, or chape, which on both leather and metal scabbards is often given further protection from wear by an extension called a drag, or shoe.[84]
  • Sword belt: A sword belt is a belt with an attachment for the sword's scabbard, used to carry it when not in use. It is usually fixed to the scabbard of the sword, providing a fast means of drawing the sword in battle. Examples of sword belts include the Balteus used by the Roman legionary.[85]

Typology

Sword typology is based on morphological criteria on one hand (blade shape (cross-section, taper, and length), shape and size of the hilt and pommel) and age and place of origin on the other (Bronze Age, Iron Age, European (medieval, early modern, modern), Asian).

The relatively comprehensive Oakeshott typology was created by historian and illustrator Ewart Oakeshott as a way to define and catalogue European swords of the medieval period based on physical form, including blade shape and hilt configuration. The typology also focuses on the smaller, and in some cases contemporary, single-handed swords such as the arming sword.[64]

Single and double-edged

As noted above, the terms longsword, broad sword, great sword, and Gaelic claymore are used relative to the era under consideration, and each term designates a particular type of sword.

Jian

In most Asian countries, a sword (jian 劍, geom (검), ken/tsurugi (剣), pedang) is a double-edged straight-bladed weapon, while a knife or saber (dāo 刀, do (도), to/katana (刀), pisau, golok) refers to a single-edged object.

Kirpan

In Sikh history, the sword is held in very high esteem. A single-edged sword is called a kirpan, and its double-edged counterpart a khanda or tega.[86]

Churika

The South Indian churika is a handheld double-edged sword traditionally used in the Malabar region of Kerala. It is also worshipped as the weapon of Vettakkorumakan, the hunter god in Hinduism.

Backsword and falchion

European terminology does give generic names for single-edged and double-edged blades but refers to specific types with the term 'sword' covering them all. For example, the backsword may be so called because it is single-edged but the falchion which is also single-edged is given its own specific name.[87]

Single vs two-handed use

Two-handed

Two-handed sword may be used to refer to any sword that usually requires two hands to wield. However, in its proper sense it should be used only to refer to the very large swords of the 16th century.[81]

Throughout history two-handed swords have generally been less common than their one-handed counterparts, one exception being their common use in Japan.

Hand and a half sword

A Hand and a half sword, colloquially known as a "bastard sword", was a sword with an extended grip and sometimes pommel so that it could be used with either one or two hands. Although these swords may not provide a full two-hand grip, they allowed its wielders to hold a shield or parrying dagger in their off hand, or to use it as a two-handed sword for a more powerful blow.[44] These should not be confused with a longsword, two-handed sword, or Zweihänder, which were always intended to be used with two hands.

Fictional types

See also



This article uses material from the Wikipedia article "Sword", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

History & Epochal Times

3D,model,library,rendering,Inca,Maya,Egypt,Pyramids,Bible, Quoran,Gizeh,Greek,Ancient,Medival Times, Stone Age