powered by CADENAS

Social Share

Knife (3387 views - Tooling)

A knife (plural knives) is a tool with a cutting edge or blade, hand-held or otherwise, with most having a handle. Some types of knives are used as utensils, including knives used at the dining table (e.g., butter knives and steak knives) and knives used in the kitchen (e.g., paring knife, bread knife, cleaver). Many types of knives are used as tools, such as the combat knife carried by soldiers, the pocket knife carried by hikers and the hunting knife used by hunters. Knives are also used as a traditional or religious implement, such as the kirpan. Some types of knives are used as weapons, such as daggers or switchblades. Some types of knives are used as sports equipment (e.g., throwing knives). Knives are also used in agriculture, food harvesting etc.; the sickle, the scythe and even the combine harvester are knives. Knife-like tools were used at least two-and-a-half million years ago, as evidenced by the Oldowan tools. Originally made of rock, bone, flint, and obsidian, knives have evolved in construction as technology has, with blades being made from bronze, copper, iron, steel, ceramics, and titanium. Many cultures have their unique version of the knife. Due to its role as humankind's first tool, certain cultures have attached spiritual and religious significance to the knife. Most modern-day knives follow either a fixed-blade or a folding construction style, with blade patterns and styles as varied as their makers and countries of origin. The word knife possibly descends from an old Norse word knifr for blade.
Go to Article

Explanation by Hotspot Model

Knife

Knife

Knife

Licensed under Creative Commons Attribution 3.0 (Carter Cutlery).

A knife (plural knives) is a tool with a cutting edge or blade, hand-held or otherwise, with most having a handle. Some types of knives are used as utensils, including knives used at the dining table (e.g., butter knives and steak knives) and knives used in the kitchen (e.g., paring knife, bread knife, cleaver). Many types of knives are used as tools, such as the combat knife carried by soldiers, the pocket knife carried by hikers and the hunting knife used by hunters. Knives are also used as a traditional or religious implement, such as the kirpan. Some types of knives are used as weapons, such as daggers or switchblades. Some types of knives are used as sports equipment (e.g., throwing knives). Knives are also used in agriculture, food harvesting etc.; the sickle, the scythe and even the combine harvester are knives.

Knife-like tools were used at least two-and-a-half million years ago, as evidenced by the Oldowan tools.[1][2] Originally made of rock, bone, flint, and obsidian, knives have evolved in construction as technology has, with blades being made from bronze, copper, iron, steel, ceramics, and titanium. Many cultures have their unique version of the knife. Due to its role as humankind's first tool, certain cultures have attached spiritual and religious significance to the knife.[3]

Most modern-day knives follow either a fixed-blade or a folding construction style, with blade patterns and styles as varied as their makers and countries of origin. The word knife possibly descends from an old Norse word knifr for blade.[4]

Parts

A modern knife consists of:

  1. the blade
  2. the handle
  3. the point – the end of the knife used for piercing
  4. the edge – the cutting surface of the knife extending from the point to the heel
  5. the grind – the cross section shape of the blade
  6. the spine – the thickest section of the blade; on a single-edged knife, the side opposite the edge; on a two-edged knife, more toward the middle
  7. the fuller – a groove added to make the blade lighter
  8. the ricasso – the flat section of the blade located at the junction of the blade and the knife's bolster or guard
  9. the guard – the barrier between the blade and the handle which prevents the hand from slipping forward onto the blade and protects the hand from the external forces that are usually applied to the blade during use
  10. the hilt or butt – the end of the handle utilized for blunt force
  11. the lanyard – a strap used to secure the knife to the wrist

The blade edge can be plain or serrated, or a combination of both. Single-edged knives may have a reverse edge or false edge occupying a section of the spine. These edges are usually serrated and are used to further enhance function.

The handle, used to grip and manipulate the blade safely, may include a tang, a portion of the blade that extends into the handle. Knives are made with partial tangs (extending part way into the handle, known as "stick tangs") or full tangs (extending the full length of the handle, often visible on top and bottom). The handle may include a bolster, a piece of heavy material (usually metal) situated at the front or rear of the handle. The bolster, as its name suggests, is used to mechanically strengthen the knife.

Blade

Knife blades can be manufactured from a variety of materials, each of which has advantages and disadvantages. Carbon steel, an alloy of iron and carbon, can be very sharp. It holds its edge well, and remains easy to sharpen, but is vulnerable to rust and stains. Stainless steel is an alloy of iron, chromium, possibly nickel, and molybdenum, with only a small amount of carbon. It is not able to take quite as sharp an edge as carbon steel, but is highly resistant to corrosion. High carbon stainless steel is stainless steel with a higher amount of carbon, intended to incorporate the better attributes of carbon steel and stainless steel. High carbon stainless steel blades do not discolor or stain, and maintain a sharp edge. Laminate blades use multiple metals to create a layered sandwich, combining the attributes of both. For example, a harder, more brittle steel may be sandwiched between an outer layer of softer, tougher, stainless steel to reduce vulnerability to corrosion. In this case, however, the part most affected by corrosion, the edge, is still vulnerable. Pattern-welding is similar to laminate construction. Layers of different steel types are welded together, but then the stock is manipulated to create patterns in the steel.[5]

Titanium is a metal that has a better strength-to-weight ratio, is more wear resistant, and more flexible than steel. Although less hard and unable to take as sharp an edge, carbides in the titanium alloy allow them to be heat-treated to a sufficient hardness. Ceramic blades are hard, brittle, and lightweight: they may maintain a sharp edge for years with no maintenance at all, but are as fragile as glass and will break if dropped on a hard surface. They are immune to common corrosion, and can only be sharpened on silicon carbide sandpaper and some grinding wheels. Plastic blades are not especially sharp and typically serrated. They are often disposable.[6]

Knife blades have different profiles

Steel blades are commonly shaped by forging or stock removal. Forged blades are made by heating a single piece of steel, then shaping the metal while hot using a hammer or press. Stock removal blades are shaped by grinding and removing metal. With both methods, after shaping, the steel must be heat treated. This involves heating the steel above its critical point, then quenching the blade to harden it. After hardening, the blade is tempered to remove stresses and make the blade tougher. Mass manufactured kitchen cutlery uses both the forging and stock removal processes. Forging tends to be reserved for manufacturers' more expensive product lines, and can often be distinguished from stock removal product lines by the presence of an integral bolster, though integral bolsters can be crafted through either shaping method.

Knives are sharpened in various ways. Flat ground blades have a profile that tapers from the thick spine to the sharp edge in a straight or convex line. Seen in cross section, the blade would form a long, thin triangle, or where the taper does not extend to the back of the blade, a long thin rectangle with one peaked side. Hollow ground blades have concave, beveled edges. The resulting blade has a thinner edge, so it may have better cutting ability for shallow cuts, but it is lighter and less durable than flat ground blades and will tend to bind in deep cuts.[citation needed] Serrated blade knives have a wavy, scalloped or saw-like blade. Serrated blades are more well suited for tasks that require aggressive 'sawing' motions, whereas plain edge blades are better suited for tasks that require push-through cuts (e.g., shaving, chopping, slicing).

Fixed blade features

A fixed blade knife, sometimes called a sheath knife, does not fold or slide, and is typically stronger due to the tang, the extension of the blade into the handle, and lack of moving parts.

Folding blade features

A folding knife connects the blade to the handle through a pivot, allowing the blade to fold into the handle. To prevent injury to the knife user through the blade accidentally closing on the user's hand, folding knives typically have a locking mechanism. Different locking mechanisms are favored by various individuals for reasons such as perceived strength (lock safety), legality, and ease of use. Popular locking mechanisms include:

  • Slip joint – Found most commonly on traditional pocket knives, the opened blade does not lock, but is held in place by a spring device that allows the blade to fold if a certain amount of pressure is applied.[7]
  • Lockback – Also known as the spine lock, the lockback includes a pivoted latch affixed to a spring, and can be disengaged only by pressing the latch down to release the blade.[6]
  • Linerlock – Invented by Michael Walker, a Linerlock is a folding knife with a side-spring lock that can be opened and closed with one hand without repositioning the knife in the hand. The lock is self-adjusting for wear.[8]
  • Compression Lock – A variant of the Liner Lock, it uses a small piece of metal at the tip of the lock to lock into a small corresponding impression in the blade. This creates a lock that doesn't disengage when the blade is torqued, instead becoming more tightly locked. It is released by pressing the tab of metal to the side, to allow the blade to be placed into its groove set into the handle.[8]
  • Frame Lock – Also known as the integral lock or monolock, this locking mechanism was invented by custom knifemaker Chris Reeve for the Sebenza as an update to the liner lock. The frame lock works in a manner similar to the liner lock but uses a partial cutout of the actual knife handle, rather than a separate liner inside the handle to hold the blade in place.[9][10]
  • Collar lock – found on Opinel knives.[11]
  • Button Lock – Found mainly on automatic knives, this type of lock uses a small push-button to open and release the knife.
  • Axis Lock – A locking mechanism exclusively licensed to the Benchmade Knife Company. A cylindrical bearing is tensioned such that it will jump between the knife blade and some feature of the handle to lock the blade open.[12]
  • Arc Lock – A locking mechanism exclusively licensed to SOG Specialty Knives. It differs from an axis lock in that the cylindrical bearing is tensioned by a rotary spring rather than an axial spring.[13]
  • Ball Bearing Lock – A locking mechanism exclusively licensed to Spyderco. This lock is conceptually similar to the axis and arc locks but the bearing is instead a ball bearing.[14]
  • Tri-Ad Lock – A locking mechanism exclusively licensed to Cold Steel. It is a form of lockback which incorporates a thick steel stop pin between the front of the latch and the back of the tang to transfer force from the blade into the handle.[15]
  • PickLock – A round post on the back base of the blade locks into a hole in a spring tab in the handle. To close, manually lift (pick) the spring tab (lock) off the blade post with your fingers, or in "Italian Style Stilettos" swivel the bolster (hand guard) clockwise to lift the spring tab off the blade post.

Another prominent feature on many folding knives is the opening mechanism. Traditional pocket knives and Swiss Army knives commonly employ the nail nick, while modern folding knives more often use a stud, hole, disk, or flipper located on the blade, all which have the benefit of allowing the user to open the knife with one hand.

The "wave" feature is another prominent design, which uses a part of the blade that protrudes outward to catch on one's pocket as it is drawn, thus opening the blade; this was patented by Ernest Emerson and is not only used on many of the Emerson knives, but also on knives produced by several other manufacturers, notably Spyderco and Cold Steel.[16]

Automatic or switchblade knives open using the stored energy from a spring that is released when the user presses a button or lever or other actuator built into the handle of the knife. Automatic knives are severely restricted by law in the UK and most American states.[17]

Increasingly common are assisted opening knives which use springs to propel the blade once the user has moved it past a certain angle. These differ from automatic or switchblade knives in that the blade is not released by means of a button or catch on the handle; rather, the blade itself is the actuator. Most assisted openers use flippers as their opening mechanism. Assisted opening knives can be as fast or faster than automatic knives to deploy.[18]

Common locking mechanisms

In the lock back, as in many folding knives, a stop pin acting on the top (or behind) the blade prevents it from rotating clockwise. A hook on the tang of the blade engages with a hook on the rocker bar which prevents the blade rotating counter-clockwise. The rocker bar is held in position by a torsion bar. To release the knife the rocker bar is pushed downwards as indicated and pivots around the rocker pin, lifting the hook and freeing the blade.

When negative pressure (pushing down on the spine) is applied to the blade all the stress is transferred from the hook on the blade's tang to the hook on rocker bar and thence to the small rocker pin. Excessive stress can shear one or both of these hooks rendering the knife effectively useless. Knife company Cold Steel uses a variant of the lock back called the Tri-Ad Lock which introduces a pin in front of the rocker bar to relieve stress on the rocker pin, has an elongated hole around the rocker pin to allow the mechanism to wear over time without losing strength and angles the hooks so that the faces no longer meet vertically.

The bolt in the bolt lock is a rectangle of metal that is constrained to slide only back and forward. When the knife is open a spring biases the bolt to the forward position where it rests above the tang of the blade preventing the blade from closing. Small knobs extend through the handle of the knife on both sides allowing the user to slide the bolt backwards freeing the knife to close. The Axis Lock used by knife maker Benchmade is functionally identical to the bolt lock except that it uses a cylinder rather than a rectangle to trap the blade.[12] The Arc Lock by knife maker SOG is similar to the Axis Lock except the cylinder follows a curved path rather than a straight path.[13]

In the liner lock, an "L"-shaped split in the liner allows part of the liner to move sideways from its resting position against the handle to the centre of the knife where it rests against the flat end of the tang. To disengage, this leaf spring is pushed so it again rests flush against the handle allowing the knife to rotate.[8] A frame lock is functionally identical but instead of using a thin liner inside the handle material uses a thicker piece of metal as the handle and the same split in it allows a section of the frame to press against the tang.[8]

Sliding blade features

A sliding knife is a knife that can be opened by sliding the knife blade out the front of the handle. One method of opening is where the blade exits out the front of the handle point-first and then is locked into place (an example of this is the gravity knife). Another form is an O-T-F (out-the-front) switchblade, which only requires the push of a button or spring to cause the blade to slide out of the handle and lock into place. To retract the blade back into the handle, a release lever or button, usually the same control as to open, is pressed. A very common form of sliding knife is the sliding utility knife (commonly known as a stanley knife or boxcutter).

Handle

The handles of knives can be made from a number of different materials, each of which has advantages and disadvantages. Handles are produced in a wide variety of shapes and styles. Handles are often textured to enhance grip.

  • Wood handles provide good grip and are warm in the hand, but are more difficult to care for. They do not resist water well, and will crack or warp with prolonged exposure to water. Modern stabilized and laminated woods have largely overcome these problems. Many beautiful and exotic hardwoods are employed in the manufacture of custom and some production knives. In some countries it is now forbidden for commercial butchers' knives to have wood handles, for sanitary reasons.[citation needed]
  • Plastic handles are more easily cared for than wooden handles, but can be slippery and become brittle over time.[3]
  • Injection molded handles made from higher grade plastics are composed of polyphthalamide, and when marketed under trademarked names such as Zytel or Grivory, are reinforced with Kevlar or fiberglass. These are often used by major knife manufacturers.
  • Rubber handles such as Kraton or Resiprene-C are generally preferred over plastic due to their durable and cushioning nature.
  • Micarta is a popular handle material on user knives due to its toughness and stability. Micarta is nearly impervious to water, is grippy when wet, and is an excellent insulator. Micarta has come to refer to any fibrous material cast in resin. There are many varieties of micarta available. One very popular version is a fiberglass impregnated resin called G-10.
  • Leather handles are seen on some hunting and military knives, notably the KA-BAR. Leather handles are typically produced by stacking leather washers, or less commonly, as a sleeve surrounding another handle material. Russian manufacturers often use birchbark in the same manner.
  • Skeleton handles refers to the practice of using the tang itself as the handle, usually with sections of material removed to reduce weight. Skeleton handled knives are often wrapped with parachute cord or other wrapping materials to enhance grip.
  • Stainless steel and aluminum handles are durable and sanitary, but can be slippery. To counter this, premium knife makers make handles with ridges, bumps, or indentations to provide extra grip. Another problem with knives that have metal handles is that, since metal is an excellent heat-conductor, these knives can be very uncomfortable, and even painful or dangerous, when handled without gloves or other protective handwear in (very) cold climates.

More exotic materials usually only seen on art or ceremonial knives include: Stone, bone, mammoth tooth, mammoth ivory, oosik (walrus penis bone), walrus tusk, antler (often called stag in a knife context), sheep horn, buffalo horn, teeth, and mop (mother of pearl or "pearl"). Many materials have been employed in knife handles.

Handles may be adapted to accommodate the needs of people with disabilities. For example, knife handles may be made thicker or with more cushioning for people with arthritis in their hands. A non-slip handle accommodates people with palmar hyperhidrosis.

Types

Weapons

As a weapon, the knife is universally adopted as an essential tool. It is the essential element of a knife fight. For example:

  • Ballistic knife: A specialized combat knife with a detachable gas- or spring-propelled blade that can be fired to a distance of several feet or meters by pressing a trigger or switch on the handle.
  • Bayonet: A knife-shaped close-quarters fighting weapon designed to attach to the muzzle of a rifle or similar weapon.
  • Butterfly knife: A folding pocket knife also known as a "balisong" or "batangas" with two counter-rotating handles where the blade is concealed within grooves in the handles.
  • Combat knife: Any knife intended to be used by soldiers in the field, as a general-use tool, but also for fighting.
  • Dagger: A double-edged combat knife with a central spine and edges sharpened their full length, used primarily for stabbing. Variations include the Stiletto and Push dagger. See List of daggers for a more detailed list.
  • Fighting knife: A knife with a blade designed to inflict a lethal injury in a physical confrontation between two or more individuals at very short range (grappling distance). Well known examples include the Bowie knife and the Fairbairn-Sykes Fighting Knife.
  • Karambit: A knife with a curved blade resembling a tiger's claw, and a handle with one or two safety holes.
  • Rampuri: An Indian gravity knife having a single-edged blade roughly 9 to 12 inches long.
  • Shiv: A crudely made homemade knife out of everyday materials, especially prevalent in prisons among inmates. An alternate name in some prisons is shank.
  • Throwing knife: A knife designed and weighted for throwing.
  • Trench knife: Purpose-made or improvised knives, intended for close-quarter fighting, particularly in trench warfare; some have a d-shaped integral hand guard.

Sports equipment

Utensils

A primary aspect of the knife as a tool includes dining, used either in food preparation or as cutlery. Examples of this include:

  • Bread knife: A knife with a serrated blade for cutting bread
  • Boning knife: A knife used for removing the bones of poultry, meat, and fish.
  • Butcher's Knife: A knife designed and used primarily for the butchering and/or dressing of animals.
  • Carving knife: A knife for carving large cooked meats such as poultry, roasts, hams
  • Chef's knife: Also known as a French knife, a cutting tool used in preparing food
  • Cleaver: A large knife that varies in its shape but usually resembles a rectangular-bladed hatchet. It is used mostly for hacking through bones as a kitchen knife or butcher knife, and can also be used for crushing via its broad side, typically garlic.
  • Electric knife: An electrical device consisting of two serrated blades that are clipped together, providing a sawing action when powered on
  • Kitchen knife: Any knife, including the chef's knife, that is intended to be used in food preparation
  • Oyster knife: Has a short, thick blade for prying open oyster shells
  • Mezzaluna: A two-handled arc-shaped knife used in a rocking motion as a herb chopper or for cutting other foods
  • Paring or Coring Knife: A knife with a small but sharp blade used for cutting out the cores from fruit.
  • Rocker knife is a knife that cuts with a rocking motion, which is primarily used by people whose disabilities prevent them from using a fork and knife simultaneously.[19]
  • Table knife or Case knife: A piece of cutlery, either a butter knife, steak knife, or both, that is part of a table setting, accompanying the fork and spoon

Tools

As a utility tool the knife can take many forms, including:[6]
  • Balisong: A folding knife also known as a "butterfly knife" or "batangas", with two handles counter-rotating around the tang such that, when closed, the blade is hidden within the handles.
  • Bowie knife: Commonly, any large sheath knife, or a specific style of large knife popularized by Jim Bowie.
  • Bushcraft knife: A sturdy, normally fixed blade knife used while camping in the wilderness.
  • Camping Knife: A camping knife is used for camping and survival purposes in a wilderness environment.
  • Karambit: A knife with a curved blade resembling a tigers claw, used as an agricultural tool then as a weapon.
  • Cobbler's knife or shoemaker's knife: A knife with a semicircular blade used by cobblers since antiquity to cut leather.
  • Crooked knife: Sometimes referred to as a "curved knife", "carving knife" or in the Algonquian language the "mocotaugan" is a utilitarian knife used for carving.
  • Diver's knife: A knife adapted for use in diving and water sports and a necessary part of standard diving dress.
  • Electrician's knife: A short-bladed knife used to cut electrical insulation.
  • Folding Knife: A folding knife is a knife with one or more blades that fit inside the handle that can still fit in a pocket. It is also known as a jackknife or jack-knife.
  • Hunting knife: A knife used to dress large game.
  • Kiridashi: A small Japanese knife having a chisel grind and a sharp point, used as a general-purpose utility knife.
  • Linoleum knife: is a small knife that has a short, stiff blade with a curved point and a handle and is used to cut linoleum or other sheet materials.
  • Machete: A large heavy knife used to cut through thick vegetation such as sugar cane or jungle undergrowth; it may be used as an offensive weapon.
  • Palette knife: A knife, or frosting spatula, lacking a cutting edge, used by artists for tasks such as mixing and applying paint and in cooking for spreading icing.
  • Paper knife: Or a "letter opener" it is a knife made of metal or plastic, used for opening mail.
  • Pocket knife: a folding knife designed to be carried in a pants pocket. Subtypes include:
    • Lockback knife: a folding knife with a mechanism that locks the blade into the open position, preventing accidental closure while in use
    • Multi-tool and Swiss Army knife, which combine a folding knife blade with other tools and implements, such as pliers, scissors, or screwdrivers
  • Produce knife: A knife with a rectangular profile and a blunt front edge used by grocers to cut produce.
  • Rigging knife: A knife used to cut rigging in sailing vessels.
  • Scalpel: A medical knife, used to perform surgery.
  • Straight razor: A reusable knife blade used for shaving hair.
  • Survival knife: A sturdy knife, sometimes with a hollow handle filled with survival equipment.
  • Switchblade: A knife with a folding blade that springs out of the grip when a button or lever on the grip is pressed.
  • Utility knife: A short knife with a replaceable triangular blade, used for cutting sheet materials including card stock, paperboard, and corrugated fiberboard
  • Wood carving knife and whittling knives: Knives used to shape wood in the arts of wood carving and whittling, often with short, thin replaceable blades for better control.
  • X-Acto knife: A scalpel-like knife with a long handle and a replaceable pointed blade, used for precise, clean cutting in arts and crafts

Traditional or religious implements

  • Athame: A typically black-handled and double-edged ritual knife used in Wicca and other derivative forms of Neopagan witchcraft. (see also Boline).
  • Katar: An Indian push dagger sometimes used ceremonially.
  • Kilaya: A dagger used in Tibetan Buddhism
  • Kirpan: A ceremonial knife that all baptised Sikhs must wear as one of the five visible symbols of the Sikh faith (Kakars)
  • Kris: A dagger used in Indo-Malay cultures, often by royalty and sometimes in religious rituals
  • Kukri: A Nepalese knife used as both tool and weapon
  • Puukko: A traditional Finnish or Scandinavian style woodcraft belt-knife used as a tool rather than a weapon
  • Seax: A Germanic single-edged knife, used primarily as a tool, but was also used as a weapon
  • Sgian Dubh: A small dagger traditionally worn with highland dress (kilt)
  • Ulu: An Inuit woman's all-purpose knife.
  • Yakutian knife: A traditional Yakuts knife used as a tool for wood carving and meat or fish cutting. Can be used as a part of yakutian ethnic costume.

Rituals and superstitions

The knife plays a significant role in some cultures through ritual and superstition, as the knife was an essential tool for survival since early man.[2] Knife symbols can be found in various cultures to symbolize all stages of life; for example, a knife placed under the bed while giving birth is said to ease the pain, or, stuck into the headboard of a cradle, to protect the baby;[20][21] knives were included in some Anglo-Saxon burial rites, so the dead would not be defenseless in the next world.[22][23][24] The knife plays an important role in some initiation rites, and many cultures perform rituals with a variety of knives, including the ceremonial sacrifices of animals.[25] Samurai warriors, as part of bushido, could perform ritual suicide, or seppuku, with a tantō, a common Japanese knife.[26] An athame, a ceremonial knife, is used in Wicca and derived forms of neopagan witchcraft.[27][28]

In Greece, a black-handled knife placed under the pillow is used to keep away nightmares.[29] As early as 1646 reference is made to a superstition of laying a knife across another piece of cutlery being a sign of witchcraft.[30] A common belief is that if a knife is given as a gift, the relationship of the giver and recipient will be severed. Something such as a small coin, dove or a valuable item is exchanged for the gift, rendering "payment."[31]

Legislation

Knives are typically restricted by law, although restrictions vary greatly by country or state and type of knife. For example, some laws prohibit carrying knives in public while other laws prohibit private ownership of certain knives, such as switchblades.

See also



This article uses material from the Wikipedia article "Knife", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Tooling

tooling,tool,drill,cam,manufacturing