Information for existing customers
The following changes appear in the license administration as of PARTsolutions V9.03:
A preselection for the license product to be used is available. See Section 1.8.3.4, “ "License product preselection" tabbed page ”.
The setting is not restrictive. The user can modify the setting inside the module.
You don't have to determine the hostid to be used manually anymore, because it is automatically detected. Also ports are automatically detected.
The "Administrator mode" is cancelled, exactly because no manual settings for the hostid have to be performed anymore.