In order for parts to be found via search for Order number or Type code, included those where CNSORDERNO and CNSTYPECODE are build by value range values, certain preconditions have to be fulfilled. If the number of possible combinations resulting from the value ranges is too big, no indexing will take place, but instead a Reverse Search is used, which enables finding of value range values as well.
The Resolve check checks if a catalog is resolvable in the full-text search index or if a Reverse Search is necessary. If the catalog is accordingly prepared, even in most complex cases searching for Order number or Type code will be successful.
The benefits of a Reverse Search are:
Always good search results since even order numbers (article numbers) or type codes built from complex value ranges (yellow fields) values are found.
Via order number / type code, articles on PARTcommunity portals can safely be found and correctly be ordered. Cross-links between portals are possible. External assistants can directly request geometry by calling order number / type code instead of using a complex list of deeplinks.
Initial article assignment of ERP numbers to PARTsolutions projects on the base of order number / type code is simplified, as numbers are absolutely unique.
(For details also see Section 3.2.18.2, “Benefits of classification according to CNSORDERNO and CNSTYPECODE”.)
Within the scope of a Resolve check following initial steps are required
Classification according to CNSORDERNO and CNSTYPECODE
This task can semi-automatically be performed for the whole catalog with the plugin "Batch classification of projects" (see Section 5.13.6, “ Batch classification of projects ”).
This then results in an entry under Variable with Order Number and/or Variable with Type Code.
Update the full-text search index.
See Section 1.3.8.6.2, “Context menu commands in detail ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
Performing a Resolve check (see next section)
|
If the catalog could not be completely resolved, adjustments for projects in the category "Manual creation of the reverse search necessary" have to be made.
-> Check
if respective projects can be resolved by structural changes (see Section 5.8.2.1.15.17.6, “Reverse Search
(automatic) - Avoid problematic constructs”).
Shouldn't this be possible, you have to manually create Reverse Configs
of the type pnoreverse.cfg
(see Section 5.8.2.1.15.20, “
Reverse TypeCode Rule Editor
”).
If the projects listed in the categories Automatic calculation of the reverse search, Inclusion in full text index up to max. 50,000 lines and Manual reverse search available shall be marked in the program, please click on .
In order for the functionality to be actually available, the flag "Auto reverse Search" has to be activated.
Optionally, the Reverse search (automatic) can be activated for PCOM portals.
Activation of Reverse Search (automatic) after catalog analysis / improvement
If the activation of Reverse Search (automatic) happens subsequently after a catalog analysis or improvement, the following steps are needed:
Analysis after catalog changes
For new or changed projects, Testmeta will check if the projects are resolvable and if ORDERNUMBER/TYPECODE are classified and will issue warnings / errors - if necessary.
What happens if a variable or variable value is changed?
For all projects, which can be resolved by Automatic calculation of the reverse search, in this case, no further adjustments have to be made apart from new publication of the catalog.
What happens if a variable is cancelled or added?
For all projects, which can be resolved by Automatic calculation of the reverse search, in this case, no further adjustments have to be made apart from new publication of the catalog.
If there are changes, this is the required approach:
Update the full-text search index.
See Section 1.3.8.6.2, “Context menu commands in detail ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
In the context menu of desired catalog, under Automation, call the command Reverse search ‒ Resolve check (automatic).
After finished process a respective message is displayed whether the catalog could be completely resolved or not.
An initial Resolve check may take some time depending on catalog size. At further processes, if there were no or only little changes, the result is displayed after a few seconds, because only changed projects are tested.
-> The results of the resolve check are displayed in detail.
All projects which can be resolved with the automatic reverse search are shown in the first category (Automatic calculation of the reverse search).
All projects which can be resolved with less than 50.000 variants are shown in category 2 (Inclusion in full text index up to max. 50,000 lines).
All projects which are resolved with the manual reverse are shown in category 3 (Manual reverse search available).
The rest is shown in category 4 (Manual creation of the reverse search necessary).
An effort estimation on realisation of highest search result quality is simply possible:
Category 4 is not empty -> (see below)
Under $CADENAS_DATA/23dlibs/<catalogname>
the file resolvecheck.cfg
is created
which centrally lists all results.
[REVERSEANALYSIS] path/project name.prj=GEOMDATE;table rows;variants;automatic search possible (0 or 1) z.B. project.prj=01.01.2019;1;10;1 ... ... very below [COMMON] REVERSEANALYSIS=Date of last run
![]() |
Note |
---|---|
A new initial check run can be forced via config setting. See below. |
Under Projects there are two main levels where the distinction is made if projects have value ranges at all. Then projects with value ranges are differentiated in 4 groups:
Automatic calculation of the reverse search: For projects listed here the reverse search could be automatically calculated. A heuristic check did not reveal any errors.
Under
$CADENAS_DATA/index/cat/cat_<catalogname>/graph
a file graphlookup.map
is
created. It contains all information cross-catalog down to project
level.
Manual creation of the reverse search necessary
May be an automatic resolving can still be achieved by some adjustments within the project structure. Notes on this can be found under Section 5.8.2.1.15.17.6, “Reverse Search (automatic) - Avoid problematic constructs”. Otherwise the reverse search has to be created manually. See Section 5.8.2.1.15.20, “ Reverse TypeCode Rule Editor ”.
Amount: Amount of variants per project. At Projects without value ranges the value means the number of table rows and at Projects with value ranges the number of variants or if empty then the variants are over 25.000 (limit value, no further check).
![]() |
One or several parts are not resolved yet. |
![]() |
An error message is displayed.
|
![]() |
The subarea is resolved in one way or another and does not need to be regarded. |
![]() |
For this project, a manual reverse configuration is saved. (<project name>_pnoreverse.cfg available) |
![]() |
Project will be resolved and written in the Lucene index. |
Exports all projects under Manual creation of the reverse search necessary.
Export csv file: All listed projects will be exported.
IS_COMPLEX: True, if there are yellow fields (object attribute or geometry attribute
RANGES = Number of yellow fields (if RANGES is 0 then under SUBTYPE there is also 0)
HASPNO = For this project a _pnoreverse.cfg file is already available (manual configuration solution)
HASFLAG = The VARSEARCHRESOLVEORDERNO flag is already set to 1 and the project is taken in the Lucene index. You have to regard not to exceed the limit of 50000 per catalog.
Apply: This function concerns the categories Automatic calculation of the reverse search, Inclusion in full text index up to max. 50,000 lines and Manual reverse search available.
Clicking on affects the setting of the resolve flag.[33]
When clicking on you confirm that the flag will be set for x potential projects.
When
performing the automatic calculation at the reverse search under
$CADENAS_DATA\index\cat\cat_resolve_check\graph
eine Datei graphlookup.map
is created. This
file will be ignored during the upload on online portals by default
and has to be explicitly unlocked by CADENAS.
Searching for Order number or type code only works in respective catalog on Online portals (in PARTdataManager over all catalogs as well).
Always a search should usefully be performed in the desired catalog. However, sometimes a catalog consists of subcatalogs (for example, the Standard catalog of DIN, ISO, EN, etc.). In such a case please perform the search in the respective subcatalog.
When
generating the CIP file of a catalog, in the catalog's file dir.prj
, the results of the
resolve check will be set in the form of following keys:
CATMETRICS_SEARCHABLE_PROJECTS
Number of projects which should be found (All visible projects and projects with SEARCHINDEX=ON)
Number of projects with a classified order number or type code variable
Number of projects with order numbers and type codes indexed by lucene
Number of projects which can be solved via auto reverse search
Number of projects which can't be found by the reverse search
Background
information: In order to create the information which shall be written
into the dir.prj
,
the configuration files resolvecheck.cfg
and
*.qacheck
are
evaluated. E.g., the ResolveChecker writes to
resolvecheck.cfg
for which projects an automatic Reverse Search is possible. For the
case that someone changed a project without executing the ResolveChecker the
information is read from *.qacheck
, where Testmeta is
writing to, and for changed projects Testmeta has to be called in any
case, because otherwise publication is not possible.
The
configuration file can be found under $CADENAS\libs\all\plugins\resolve_check.cfg
:
The quality of the heuristic check for the automatic calculation of the reverse search can be adjusted via the first three keys.
If NEVERSKIPGRAPH is set to 1 (default is 0) at each run a complete recalculation is performed. (May be makes sense on testing purposes if the automatic generation has been enhanced.)
[COMMON] # maximum graphsearch searches per project MAXHEURISTICS=10000 # maximum time in minutes to use when counting variants MAXTIME=15 # maximum time in minutes when checking graphsearch results MAXTIMETEST=15 # always recheck the graphsearch even if we already have a saved result NEVERSKIPGRAPH=0
Definitions for variable abbreviations
Following figure shows the setting area for above mentioned value range variables.
Example 1 - Indirect, calculated use of value range
The order number (NR) results from the string 'xyz' and an attribute algorithm.
NR=xyz ALG ALG=10*RNG
Problem: ALG can be allocated to a unique value, however, due to above restriction the value of RNG cannot be detected.
The same would apply for following slightly modified cases, because here, also an arithmetic operation is performed:
A solution possibly could be to determine the value range values in a way that a calculation via ALG could be omitted and to use RNG directly to determine NR.
Example 2 - Forward resolving with algorithm
ALG1: Forward to a value range
ALG1=RNG (ALG1 is based on a value range)
ALG2: IF Statement to determine the displayed order number value
If ALG1='xyz' then ALG2=123 Else If ALG1='abc' then ALG2=789 End if NR=DIN ALG2
ALG1 can be allocated to a unique value, however, the value cannot be set due to above restriction.
In the IF statement, directly use the value range instead of the algorithm variable.
If RNG='xyz' then ALG2=123 Else If RNG='abc' then ALG2=789 End if NR=DIN ALG2
Example 3 - No separator between value range variables
NR=RNG1RNG2
There is no separator between the two value ranges so that it doesn't become clear from which single value the order number / type code (NR) is combined.
For example, NR='3412' could be a combination of '341' and '2' or of '34' and '12'.
Solution: Set a separator between value range variables. Then it is clear, which element belongs to value range variable 1 and which to value range variable 2.
NR=RNG1-RNG2
Example 4 - No unique paths with same result
If a=1 then ALG='01' Else if a=2 then ALG='0$RNG.' End if
ALG has multiple options which are partial equal. In the first condition "01" and in the second condition "01" as well.
If ALG has the same value reverse resolving cannot be successful. It can not be determined if we have case "a=1" or "a=2". As a consequence a statement about RNG=1 is also wrong.
[33] Key
VARSEARCHRESOLVEORDERNO
.
On project level it is in the project file, on catalog level in
$CADENAS_DATA/23d-libs/<catalog
name>/dir.prj
. No GUI equivalent. Manual
intervention not needed.