Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The CADENAS Classification (CNS) is not directly visible in PARTdataManager, however multiple functions are controlled by assigned class attributes.
The Classification (CNS) is not only designed for parts, but also for part components like Connection points, for example.
Before assigning, in the list field under Filter, select the desired option.
Besides the option Classes, the option Connection points is used especially often.
Connection points (geometrical object) can also be classified in PARTproject, in the Preview. Working there is beneficial, because you have a direct relation to the part. For this also see Section 5.13.7, “Create Published elements ”.
When selecting the option Classes in the Filter, the following selection appears.
CNSCAX, Cax Basis: Marking for symbols and layouts, among others in the electrical field and BIM.
CNSELEK, Elektro: For specific use see Section 5.13.10, “Classify Electrical Parts ”.
CNSGEOMBASE, Geometrical Properties: General properties for all fields
Properties in detail-> see below
CNSPHYPROP, Physical Properties: General properties for all fields
Properties in detail-> see below
CNSERPBASE, Object Properties: General properties for all fields like order number, type code, descriptions for tender software, etc.
Properties in detail-> see below
![]() |
Note |
---|---|
The classes CNSERPBASE (object properties), CNSGEOMBASE (geometrical properties) and CNSPHYPROP (physical properties) contain general attributes which should always be set ideally, if possible. |
Class CNSERPBASE (Object Properties)
Feature | Description |
CNSUSECASE | Use case |
CNSORDERNO | Order Number -> Also displayed under menu item Variables |
CNS_DESCRIPTION_LONG | Description long |
CNS_DESCRIPTION_SHORT | Description short |
CNSEAN | EAN-Code |
CNSCCN | ECCN-Code |
CNSQUANTITY | Quantity Unit |
CNSPRICE | Price |
CNS_RAWMETERIAL | Raw Material |
CNSSTDDTIME | Standard delivery time |
CNSTYPECODE | Type Code -> Also displayed under menu item Variables |
CNSMNTINTV | Maintenance Intervals |
CNSCERTIFICATEDNV | Certificate DNV |
CNSCERTIFICATEEMAS | Certificate EMAS |
CNSCERTIFICATEEX | Certificate Explosion Protection |
CNSCERTIFICATEFSC | Certificate FSC |
CNSCERTIFICATEISO14001 | Certificate ISO14001 |
CNSCERTIFICATEPEFC | Certificate PEFC |
CNSCERTIFICATEPROP65 | Certificate Proposition 65 |
CNSCERTIFICATEREACH | Certificate REACH |
CNSCERTIFICATEROHS | Certificate RoHS |
CNSCERTIFICATEWEEE | Certificate WEEE |
CNSCTN | Customs Tariff Number |
Class CNSGEOMBASE (Geometrical Properties)
Feature | Description |
CNS_NOSECTION | No section in 2D |
CNSEXTRUSIONVAR | Extrusion Variable |
CNSLODDEST | LOD Destination |
CNSLODLEVEL | LOD Level |
Class CNSPHYPROP (Physical Properties)
When selecting the option Connection points in the Filter, the following selection appears.
CNS_CP|4, Elektro -> see Section 5.13.10, “Classify Electrical Parts ”
Information on how assignment of classes and attributes works in practice can be found under Section 5.13.5, “ Add projects to classification ”.