Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
![]() |
Note |
---|---|
The menu item Classification is only displayed on project level. Exception: Classification (By Alphabet) and Classification (By Categories) are only displayed on catalog level. |
General on the subject of classification
Via classifications, alternative folder structures are created which then will be displayed in PARTdataManager.
Into these folder structures, (new) projects can be added. Details on the classification process can be found under Section 5.13.5, “ Add projects to classification ”.
All installed classifications are listed under the menu item Classification. For each classification there are two rows. The first one for the determination of classes, the second one for the determination of attributes.
First click on the search button under Classification. -> The dialog box Classification is opened. Assign the desired classes. Then click on the related search button under Attributes. -> The dialog box Class variables is opened. Assign the desired attributes. Details on this can be found under Section 5.13.5, “ Add projects to classification ”.
For semi-automatic classifying, especially within the Classification (CNS) you have the function Batch classification of projects available.
Details on this can be found under Section 5.13.6, “ Batch classification of projects ”.
Currently[49] available classifications
Alphabetical index, classification according to countries and categories: Details can be found under Section 5.13.3.2, “Classification (By Categories) - (By Countries) - (By Alphabet)”.
CNS: For example, the CADENAS classification uses placing information, published elements and attributes for the CAD integration or order number, type code, certificate information. For details see Section 5.13.3.1, “Classification (CNS) ”.
eCl@ss: Standardized classification system for product groups and product attributes with the objective of enabling electronic trading of classified products.
eCl@ss is offered as standard for the exchange of information between supplier and customer and is characterized by a four-stage hierarchical classification key with a catchword index of thousands of terms.
Table variables from standard or supplier catalogs or fixed values can be assigned to eCl@ss attributes via dialog box Class variables. Later for these eCl@ss attributes (terms) can be searched in PARTdataManager.
ETIM (Electro-technical information model) 4.0: Classification designed to meet the requirements of the electrical industry
ICS (International Classification Standards): International classification system to classify all economic sectors and activities that use technical standards
IFC: Classification using an international open standard to describe building and construction industry data
PCon: PARTconnection: Connection information
Connection information is required (among others) for intelligent placing of parts in the CAD system (placement dialog). See Section 2.6.1, “ Insert 3D from the Standard and supplier parts library ” in PARTsolutions / PARTcommunity4Enterprise - User manual.
Standards: Standardization system provided by CADENAS. Structured in three parts according to DIN number.
UNSPSC: Product classification given by the United Nations. The standard shows an universal classification schema for different product groups for worldwide use.
![]() |
Note |
---|---|
Up-to-dateness of classifications is ensured directly before the release, however, it may happen that newer classifications are available at the moment of installation. So please check and update (if needed) via PARTadmin -> Catalog update -> Online. Details on this can be found under Section 1.3.4.1, “ Catalog update Online ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual. |
How to assign classes and attributes, please read under Section 5.13.5, “ Add projects to classification ”.