A kerosene lamp (usually called a paraffin lamp in some countries) is a type of lighting device that uses kerosene (paraffin) as a fuel. Kerosene lamps have a wick or mantle as light source, protected by a glass chimney or globe; lamps may be used on a table, or hand-held lanterns may be used for portable lighting. Like oil lamps, they are useful for lighting without electricity, such as in regions without rural electrification, in electrified areas during power outages, at campsites, and on boats. There are three types of kerosene lamp: flat wick, central draught (tubular round wick), and mantle lamp. Kerosene lanterns meant for portable use have a flat wick and are made in dead flame, hot blast, and cold blast variants.
Pressurized kerosene lamps have a gas generator and gas mantle; these are known as Petromax, Tilley lamps, or Coleman lamps, among other manufacturers. They produce more light per unit of fuel than wick-type lamps, but are more complex and expensive in construction, and more complex to operate. A hand-pump pressurizes air, which forces liquid fuel from a reservoir into a gas generator. Vapor from the gas generator burns, heating a mantle to incandescence and also providing heat to the gas generator.
The first description of a simple lamp using crude mineral oil was provided by Persian alchemist al-Razi (Rhazes) in 9th century Baghdad, who referred to it as the "naffatah" in his Kitab al-Asrar (Book of Secrets). In 1846 Abraham Pineo Gesner invented a substitute for whale oil for lighting, distilled from coal. Later made from petroleum, kerosene became a popular lighting fuel. Modern versions of the kerosene lamp were later constructed by the Polish inventor Ignacy Łukasiewicz in 1853 in Lviv.
Kerosene lamps are widely used for lighting in rural areas of Africa and Asia where electricity is not distributed, or is too costly. Kerosene lamps consume an estimated 77 billion litres of fuel per year, equivalent to 1.3 million barrels of oil per day, comparable to annual U.S. jet fuel consumption of 76 billion litres per year.