Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Kerosene, also known as paraffin, lamp oil, and coal oil (an obsolete term), is a combustible hydrocarbon liquid which is derived from petroleum. It is widely used as a fuel in industry as well as households. Its name derives from Greek: κηρός (keros) meaning wax, and was registered as a trademark by Canadian geologist and inventor Abraham Gesner in 1854 before evolving into a genericized trademark. It is sometimes spelled kerosine in scientific and industrial usage.[1] The term kerosene is common in much of Argentina, Australia, Canada, India, New Zealand, and the United States,[2][3] while the term paraffin (or a closely related variant) is used in Chile, eastern Africa, South Africa, Norway, and in the United Kingdom.[4] The term lamp oil, or the equivalent in the local languages, is common in the majority of Asia. Liquid paraffin (called mineral oil in the US) is a more viscous and highly refined product which is used as a laxative. Paraffin wax is a waxy solid extracted from petroleum.
Kerosene is widely used to power jet engines of aircraft (jet fuel) and some rocket engines and is also commonly used as a cooking and lighting fuel, and for fire toys such as poi. In parts of Asia, kerosene is sometimes used as fuel for small outboard motors or even motorcycles.[5] World total kerosene consumption for all purposes is equivalent to about 1.2 million barrels (50 million U.S. gallons; 42 million imperial gallons; 190 million liters) per day.[6]
To prevent confusion between kerosene and the much more flammable and volatile gasoline, some jurisdictions regulate markings or colorings for containers used to store or dispense kerosene. For example, in the United States, Pennsylvania requires that portable containers used at retail service stations for kerosene be colored blue, as opposed to red (for gasoline) or yellow (for diesel fuel).[7]
Kerosene is a low viscosity, clear liquid formed from hydrocarbons obtained from the fractional distillation of petroleum between 150 and 275 °C (300 and 525 °F), resulting in a mixture with a density of 0.78–0.81 g/cm3 (0.45–0.47 oz/cu in) composed of carbon chains that typically contain between 10 and 16 carbon atoms per molecule.[8] It is miscible in petroleum solvents but immiscible in water.
The American Society for Testing and Materials standard specification D-3699-78 recognizes two grades of kerosene: grades 1-K (less than 0.04% sulfur by weight) and 2-K (0.3% sulfur by weight). 1-K grade kerosene burns cleaner with fewer deposits, fewer toxins, and less frequent maintenance than 2-K grade kerosene, and is the preferred grade of kerosene for indoor kerosene heaters and stoves.[9]
Regardless of crude oil source or processing history, kerosene's major components are branched and straight chain alkanes and naphthenes (cycloalkanes), which normally account for at least 70% by volume. Aromatic hydrocarbons in this boiling range, such as alkylbenzenes (single ring) and alkylnaphthalenes (double ring), do not normally exceed 25% by volume of kerosene streams. Olefins are usually not present at more than 5% by volume.[10]
The flash point of kerosene is between 37 and 65 °C (100 and 150 °F), and its autoignition temperature is 220 °C (428 °F).[11] The pour point of kerosene depends on grade, with commercial aviation fuel standardized at −47 °C (−53 °F).
1-K grade kerosene freezes around −40 °C (−40 °F, 233 K).[12]
Heat of combustion of kerosene is similar to that of diesel fuel; its lower heating value is 43.1 MJ/kg (around 18,500 Btu/lb), and its higher heating value is 46.2 MJ/kg (19,900 Btu/lb).[13]
In the United Kingdom, two grades of heating oil are defined. BS 2869 Class C1 is the lightest grade used for lanterns, camping stoves, wick heaters, and mixed with gasoline in some vintage combustion engines as a substitute for tractor vaporising oil. BS 2869 Class C2 is a heavier distillate, which is used as domestic heating oil. Premium kerosene is usually sold in 5-or-20-liter (1.1 or 4.4 imp gal; 1.3 or 5.3 U.S. gal) containers from hardware, camping and garden stores and is often dyed purple. Standard kerosene is usually dispensed in bulk by a tanker and is undyed.
National and international standards define the properties of several grades of kerosene used for jet fuel. Flash point and freezing point properties are of particular interest for operation and safety; the standards also define additives for control of static electricity and other purposes.
The process of distilling crude oil/petroleum into kerosene, as well as other hydrocarbon compounds, was first written about in the 9th century by the Persian scholar Rāzi (or Rhazes). In his Kitab al-Asrar (Book of Secrets), the physician and chemist Razi described two methods for the production of kerosene, termed naft abyad ("white naphtha"), using an apparatus called an alembic. One method used clay as an absorbent, whereas the other method used ammonium chloride (sal ammoniac). The distillation process was repeated until most of the volatile hydrocarbon fractions had been removed and the final product was perfectly clear and safe to burn. Kerosene was also produced during the same period from oil shale and bitumen by heating the rock to extract the oil, which was then distilled.[14] During the medieval Chinese Ming Dynasty, the Chinese made use of kerosene through extracting and purifying petroleum and then converted it into lamp fuel.[15] The Chinese made use of petroleum for lighting lamps and heating homes as early as 1500 BC.[16]
Although "coal oil" was well known by industrial chemists at least as early as the 1700s as a byproduct of making coal gas and coal tar, it burned with a smoky flame that prevented its use for indoor illumination. In cities, much indoor illumination was provided by piped-in coal gas, but outside the cities, and for spot lighting within the cities, the lucrative market for fueling indoor lamps was supplied by whale oil, specifically that from sperm whales, which burned brighter and cleaner.[17]
Canadian geologist Abraham Gesner claimed that in 1846, he had given a public demonstration in Charlottetown, Prince Edward Island of a new process he had discovered.[note 1] He heated coal in a retort, and distilled from it a clear, thin fluid that he showed made an excellent lamp fuel. He coined the name "kerosene" for his fuel, a contraction of keroselaion, meaning wax-oil.[18] The cost of extracting kerosene from coal was high.
Gesner recalled from his extensive knowledge of New Brunswick's geology a naturally occurring asphaltum called albertite. He was blocked from using it by the New Brunswick coal conglomerate because they had coal extraction rights for the province, and he lost a court case when their experts claimed albertite was a form of coal.[19] In 1854, Gesner moved to Newtown Creek, Long Island, New York. There, he secured backing from a group of businessmen. They formed the North American Gas Light Company, to which he assigned his patents.
Despite clear priority of discovery, Gesner did not obtain his first kerosene patent until 1854, two years after James Young's United States patent.[20][21] Gesner's method of purifying the distillation products appears to have been superior to Young's, resulting in a cleaner and better-smelling fuel. Manufacture of kerosene under the Gesner patents began in New York in 1854 and later in Boston—being distilled from bituminous coal and oil shale.[18] Gesner registered the word "Kerosene" as a trademark in 1854, and for several years, only the North American Gas Light Company and the Downer Company (to which Gesner had granted the right) were allowed to call their lamp oil "Kerosene" in the United States.[22]
In 1848, Scottish chemist James Young experimented with oil discovered seeping in a coal mine as a source of lubricating oil and illuminating fuel. When the seep became exhausted, he experimented with the dry distillation of coal, especially the resinous "boghead coal" (torbanite). He extracted a number of useful liquids from it, one of which he named paraffine oil because at low temperatures, it congealed into a substance that resembled paraffin wax. Young took out a patent on his process and the resulting products in 1850, and built the first truly commercial oil-works in the world at Bathgate in 1851, using oil extracted from locally mined torbanite, shale, and bituminous coal. In 1852, he took out a United States patent for the same invention. These patents were subsequently upheld in both countries in a series of lawsuits, and other producers were obliged to pay him royalties.[18]
In 1851, Samuel Martin Kier began selling lamp oil to local miners, under the name "Carbon Oil". He distilled this by a process of his own invention from crude oil. He also invented a new lamp to burn his product.[23] He has been dubbed the Grandfather of the American Oil Industry by historians.[24] Since the 1840s, Kier's salt wells were becoming fouled with petroleum. At first, Kier simply dumped the useless oil into the nearby Pennsylvania Main Line Canal, but later he began experimenting with several distillates of the crude oil, along with a chemist from eastern Pennsylvania.[25]
Ignacy Łukasiewicz, a Polish pharmacist residing in Lviv, and his Hungarian partner Jan Zeh had been experimenting with different distillation techniques, trying to improve on Gesner's kerosene process, but using oil from a local petroleum seep. Many people knew of his work, but paid little attention to it. On the night of 31 July 1853, doctors at the local hospital needed to perform an emergency operation, virtually impossible by candlelight. They therefore sent a messenger for Łukasiewicz and his new lamps. The lamp burned so brightly and cleanly that the hospital officials ordered several lamps plus a large supply of fuel. Łukasiewicz realized the potential of his work and quit the pharmacy to find a business partner, and then travelled to Vienna to register his technique with the government. Łukasiewicz moved to the Gorlice region of Poland in 1854, and sank several wells across southern Poland over the following decade, setting up a refinery near Jasło in 1859.[26]
The petroleum discovery at the Drake Well in western Pennsylvania in 1859 caused a great deal of public excitement and investment drilling in new wells, not only in Pennsylvania, but also in Canada, where petroleum had been discovered at Oil Springs, Ontario in 1858, and southern Poland, where Ignacy Łukasiewicz had been distilling lamp oil from petroleum seeps since 1852. The increased supply of petroleum allowed oil refiners to entirely side-step the oil-from-coal patents of both Young and Gesner, and produce illuminating oil from petroleum without paying royalties to anyone. As a result, the illuminating oil industry in the United States completely switched over to petroleum in the 1860s. The petroleum-based illuminating oil was widely sold as Kerosene, and the trade name soon lost its proprietary status, and became the lower-case generic product "kerosene".[27] Because Gesner’s original Kerosene had been also known as "coal oil," generic kerosene from petroleum was commonly called "coal oil" in some parts of the United States well into the 20th century.
In the United Kingdom, manufacturing oil from coal (or oil shale) continued into the early 20th century, although increasingly overshadowed by petroleum oils.
As kerosene production increased, whaling declined. The American whaling fleet, which had been steadily growing for 50 years, reached its all-time peak of 199 ships in 1858. By 1860, just two years later, the fleet had dropped to 167 ships. The Civil War cut into American whaling temporarily, but only 105 whaling ships returned to sea in 1866, the first full year of peace, and that number dwindled until only 39 American ships set out to hunt whales in 1876.[28] Kerosene, made first from coal and oil shale, then from petroleum, had largely taken over whaling’s lucrative market in lamp oil.
Electric lighting started displacing kerosene as an illuminant in the late 19th century, especially in urban areas. However, kerosene remained the predominant commercial end-use for petroleum refined in the United States until 1909, when it was exceeded by motor fuels. The rise of the gasoline-powered automobile in the early 20th century created a demand for the lighter hydrocarbon fractions, and refiners invented methods to increase the output of gasoline, while decreasing the output of kerosene. In addition, some of the heavier hydrocarbons that previously went into kerosene were incorporated into diesel fuel. Kerosene kept some market share by being increasingly used in stoves and portable heaters.[29]
In 2013, kerosene made up about 0.1 percent by volume of petroleum refinery output in the United States.[30]
Fuels for heating |
At one time the fuel, also known as heating oil in the UK and Ireland, was widely used in kerosene lamps and lanterns. Although it replaced whale oil, the 1873 edition of Elements of Chemistry said, "The vapor of this substance [kerosene] mixed with air is as explosive as gunpowder."[31] This may have been due to the common practice of adulterating kerosene with cheaper but more volatile hydrocarbon mixtures, such as naphtha.[32] Kerosene was a significant fire risk; in 1880, nearly two of every five New York City fires were caused by defective kerosene lamps.[33]
In less-developed countries kerosene is an important source of energy for cooking and lighting. It is used as a cooking fuel in portable stoves for backpackers. As a heating fuel, it is often used in portable stoves, and is sold in some filling stations. It is sometimes used as a heat source during power failures.
Kerosene is widely used in Japan as a home heating fuel for portable and installed kerosene heaters. In Japan, kerosene can be readily bought at any filling station or be delivered to homes.[34] In the United Kingdom and Ireland, kerosene is often used as a heating fuel in areas not connected to a gas pipeline network. It is used less for cooking, with LPG being preferred because it is easier to light. Kerosene is often the fuel of choice for range cookers such as Rayburn. Additives such as RangeKlene can be put into kerosene to ensure that it burns cleaner and produces less soot when used in range cookers.[35]
The Amish, who generally abstain from the use of electricity, rely on kerosene for lighting at night.
More ubiquitous in the late 19th and early 20th centuries, kerosene space heaters were often built into kitchen ranges, and kept many farm and fishing families warm and dry through the winter. At one time, citrus growers used a smudge pot fueled by kerosene to create a pall of thick smoke over a grove in an effort to prevent freezing temperatures from damaging crops. "Salamanders" are kerosene space heaters used on construction sites to dry out building materials and to warm workers. Before the days of electrically lighted road barriers, highway construction zones were marked at night by kerosene fired, pot-bellied torches. Most of these uses of kerosene created thick black smoke because of the low temperature of combustion.
A notable exception, discovered in the early 19th century, is the use of a gas mantle mounted above the wick on a kerosene lamp. Looking like a delicate woven bag above the woven cotton wick, the mantle is a residue of mineral materials (mostly thorium dioxide), heated to incandescence by the flame from the wick. The thorium and cerium oxide combination produces both a whiter light and a greater fraction of the energy in the form of visible light than a black body at the same temperature would. These types of lamps are still in use today in areas of the world without electricity, because they give a much better light than a simple wick-type lamp does.[citation needed] Recently, a multipurpose lantern that doubles as a cook stove has been introduced in India in areas with no electricity.[36]
In countries such as India and Nigeria, kerosene is the main fuel used for cooking, especially by the poor, and kerosene stoves have replaced traditional wood-based cooking appliances. As such, increase in the price of kerosene can have a major political and environmental consequence. The Indian government subsidizes the fuel to keep the price very low, to around 15 U.S. cents per liter as of February 2007, as lower prices discourage dismantling of forests for cooking fuel.[37] In Nigeria an attempt by the government to remove a fuel subsidy that includes kerosene met with strong opposition.[38]
Kerosene is used as a fuel in portable stoves, especially in Primus stoves invented in 1892. Portable kerosene stoves earn a reputation of reliable and durable stove in everyday use, and perform especially well under adverse conditions. In outdoor activities and mountaineering, a decisive advantage of pressurized kerosene stoves over gas cartridge stoves is their particularly high thermal output and their ability to operate at very low temperature in winter or at high altitude. Wick stoves like Perfection's or wickless like Boss continue to be used by the Amish and off grid living and in natural disasters where there is no power available.
In the mid-20th century, kerosene or tractor vaporising oil (TVO) was used as a cheap fuel for tractors. The engine would start on gasoline, then switch over to kerosene once the engine warmed up. A heat valve on the manifold would route the exhaust gases around the intake pipe, heating the kerosene to the point where it was vaporized and could be ignited by an electric spark.
In Europe following the Second World War, automobiles were similarly modified to run on kerosene rather than gasoline, which they would have to import and pay heavy taxes on. Besides additional piping and the switch between fuels, the head gasket was replaced by a much thicker one to diminish the compression ratio (making the engine less powerful and less efficient, but able to run on kerosene). The necessary equipment was sold under the trademark "Econom".[39]
During the fuel crisis of the 1970s, Saab-Valmet developed and series-produced the Saab 99 Petro that ran on kerosene, turpentine or gasoline. The project, codenamed "Project Lapponia", was headed by Simo Vuorio, and towards the end of the 1970s, a working prototype was produced based on the Saab 99 GL. The car was designed to run on two fuels. Gasoline was used for cold starts and when extra power was needed, but normally it ran on kerosene or turpentine. The idea was that the gasoline could be made from peat using the Fischer–Tropsch process. Between 1980 and 1984, 3,756 Saab 99 Petros and 2,385 Talbot Horizons (a version of the Chrysler Horizon that integrated many Saab components) were made. One reason to manufacture kerosene-fueled cars was that in Finland kerosene was less heavily taxed than gasoline.[40]
Kerosene is used to fuel smaller-horsepower outboard motors built by Yamaha, Suzuki, and Tohatsu. Primarily used on small fishing craft, these are dual-fuel engines that start on gasoline and then transition to kerosene once the engine reaches optimum operating temperature. Multiple fuel Evinrude and Mercury Racing engines also burn kerosene, as well as jet fuel.[41]
Today, kerosene is mainly used in fuel for jet engines in several grades. One highly refined form of the fuel is known as RP-1, and is often burned with liquid oxygen as rocket fuel. These fuel grade kerosenes meet specifications for smoke points and freeze points. The combustion reaction can be approximated as follows, with the molecular formula C12H26 (dodecane):
2 C12H26(l) + 37 O2(g) → 24 CO2(g) + 26 H2O(g); ∆H˚ = -7513 kJ
In the initial phase of liftoff, the Saturn V launch vehicle was powered by the reaction of liquid oxygen with RP-1.[42] For the five 6.4 meganewton sea-level thrust F-1 rocket engines of the Saturn V, burning together, the reaction generated roughly 1.62 × 1011 watts (J/s) (162 gigawatt) or 217 million horsepower.[42]
Kerosene is sometimes used as an additive in diesel fuel to prevent gelling or waxing in cold temperatures.[43]
Ultra-low sulfur kerosene is a custom-blended fuel used by the New York City Transit Authority to power its bus fleet. The transit agency started using this fuel in 2004, prior to the widespread adoption of ultra-low-sulfur diesel, which has since become the standard. In 2008, the suppliers of the custom fuel failed to tender for a renewal of the transit agency's contract, leading to a negotiated contract at a significantly increased cost.[44]
JP-8, (for "Jet Propellant 8") a kerosene-based fuel, is used by the United States military as a replacement in diesel fueled vehicles and for powering aircraft. JP-8 is also used by the U.S. military and its NATO allies as a fuel for heaters, stoves, tanks and as a replacement for diesel fuel in the engines of nearly all tactical ground vehicles and electrical generators.
Kerosene is used as a diluent in the PUREX extraction process, but it is increasingly being supplanted by dodecane. In X-ray crystallography, kerosene can be used to store crystals. When a hydrated crystal is left in air, dehydration may occur slowly. This makes the color of the crystal become dull. Kerosene can keep air from the crystal.
It can be also used to prevent air from re-dissolving in a boiled liquid,[45] and to store alkali metals such as potassium, sodium, and rubidium (with the exception of lithium, which is less dense than kerosene, causing it to float).[46]
Kerosene is often used in the entertainment industry for fire performances, such as fire breathing, fire juggling or poi, and fire dancing. Because of its low flame temperature when burnt in free air, the risk is lower should the performer come in contact with the flame. Kerosene is generally not recommended as fuel for indoor fire dancing, as it produces an unpleasant (to some) odor, which becomes poisonous in sufficient concentration. Ethanol was sometimes used instead, but the flames it produces look less impressive, and its lower flash point poses a high risk.
As a petroleum product miscible with many industrial liquids, kerosene can be used as both a solvent, able to remove other petroleum products, such as chain grease, and as a lubricant, with less risk of combustion when compared to using gasoline. It can also be used as a cooling agent in metal production and treatment (oxygen-free conditions).[47]
In the petroleum industry, kerosene is often used as a synthetic hydrocarbon for corrosion experiments to simulate crude oil in field conditions.
Kerosene can be applied topically to hard-to-remove mucilage or adhesive left by stickers on a glass surface (such as in show windows of stores).[45]
It can be used to remove candle wax that has dripped onto a glass surface; it is recommended that the excess wax be scraped off prior to applying kerosene via a soaked cloth or tissue paper.[45]
It can be used to clean bicycle and motorcycle chains of old lubricant before relubrication.[45]
It can also be used to thin oil based paint used in fine art. Some artists even use it to clean their brushes; however, it leaves the bristles greasy to the touch.
Ingestion of kerosene is harmful or fatal. Kerosene is sometimes recommended as a folk remedy for killing head lice, but health agencies warn against this as it can cause burns and serious illness. A kerosene shampoo can even be fatal if fumes are inhaled.[48][49]
People can be exposed to kerosene in the workplace by breathing it in, swallowing it, skin contact, and eye contact. The US National Institute for Occupational Safety and Health (NIOSH) has set a recommended exposure limit of 100 mg/m3 over an 8-hour workday.[50]
This article uses material from the Wikipedia article "Kerosene", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht