Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Licensed under Creative Commons Attribution-Share Alike 3.0 (Roberta F.).
Jet Ski is the brand name of a personal watercraft[1] manufactured by Kawasaki,[2] a Japanese company.[3] The term is often used generically to refer to any type of personal watercraft used mainly for recreation, and it is also used as a verb to describe the use of this type of water vehicle.[4] Jet Skis typically can carry 1-2 people seated in a configuration like a typical bicycle or motorcycle.
It was the "first commercially successful" personal watercraft in America, having been released in 1972 (after reaching a license agreement with the inventor of the Jet Ski, Clayton Jacobson II when his license agreement with Bombardier expired).[2]
"Jet Ski" is a proper noun and registered trademark of Kawasaki.
There have been fatal accidents involving Jet Skis. In a notable case U.S. astronaut Alan G. Poindexter died in 2012 due to an accident with a Jet Ski in Florida.[5]
Wikimedia Commons has media related to Jetskis. |
Boardsports | |
---|---|
Motorsports | |
Water sports | |
Mountaineering | |
Free fall | |
Flying | |
Cycling | |
Roller | |
Skiing | |
Sliding | |
Food | |
Others | |
This article uses material from the Wikipedia article "Jet Ski", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia
3D,CAD,Model,Libary,Railway, Train, Ship, Marine, Submarine, Automotive, Locomotive, Bike, Car, Formula 1, Space, Aircraft, Aerospace, Satelite, Automobile, Yacht