Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In the following the single buttons are described:
Restores the original state in the Connection section and removes all selections.
The Load bolted connection dialog box is opened.
In the upper section the following options are available:
Via double-click the window is closed and you can create a new connection.
Own bolted connections (this user):
If you have already saved own connections, then these are displayed here (see next point).
Predetermined bolted connections (all users):
If some connections have been already preset, then these are displayed here.
|
-> Afterwards in the lower section a preview image and the respective components are displayed.[103]
The dialog box contains the following buttons:
With click on a buttons the Load configuration dialog box opens. Browse to the desired file and load it via .
In this way you make sure that you get the current view.
Database entries[104] are not automatically updated. For this purpose use the button.
Save
connections which are frequently needed. Via button (see above) you can load it
anytime.
The Save bolted connection dialog box opens.
In the upper list field select one of the following options:
Own bolted connections (this user)
Save your own connections here. Then these are later available to you.
Predetermined bolted connections (all users)
Connections saved here are available to all users.
Shouldn't you have writing permission for this option, then you will receive a respective error message.
If needed create a hierarchical structure:
In order to remove directories or connections proceed as follows:
Configure extended settings with this menu.
Here
you can configure the startup mode of the Connection
section.
The following options are available:
The Connection section opens with the lastly loaded connection.
The
Connection section opens with an
empty connection. All filters are removed. This corresponds to
the state after click on the button.
Bolted connection selection window
This is the preset option. You can change the selection anytime.
The Load bolted connection dialog box is opened in the foreground.
Select a connection from one of the
categories or double-click the New bolted connection button in
order to start with an empty connection.
Determine a concrete connection which is basically loaded when the dialog box opens. Hereto proceed as follows:
Now
whenever the dialog box is opened the chosen preferred
connection is loaded. If you want to configure another
connection, then simply click on .
This setting concerns the connection components washer, lock washer and nut.
This option determines if the holes are exported as actual parts.
|
Dialog Obsolete standard part/manufacturer part on/off
The same icon is also displayed in the index tree, if there is both an obsolete and a valid standard part/supplier part available. On this compare Section 3.1.19.3.3, “ Obsolete standard part/manufacturer part ”.
Saves the time to separately click on each single filter in the component and value range section.