The menuvisibilty configuration file controls the visibility of menu items, buttons and context menu commands.
You can create different modes. Each mode contains a specific amount of actions = UI elements.
There are two levels by default:
Specification of various modes
In the block [COMMON] the different modes are defined.
This are Beginner and Professional by default.[47]
[COMMON] MODE_BEGINNER=Beginner MODE_PROFESSIONAL=Professional
Each mode (key) stated in the block [Common] requires a same-named block, which contains the desired actions.
[MODE_BEGINNER] ViewPart=true View2D=true ExtrasPARTbom=true etc. [MODE_PROFESSIONAL] ViewPart=true View2D=true ExtrasPARTbom=true etc.
The explanations use the terms "key name" and "action name" synonymously.
The value range of keys is true (element visible) or false (element hidden).
If a key is missing in the list, then the state of visibility is "false".
The selection of the desired mode happens in PARTdataManager under Extras menu -> Select mode. The default mode is stated in $CADENAS_DEFAULTUSER/partsolu.cfg -> block [TWEAKMENU] -> key "PARTdataManager_Mode" or "PARTproject_Mode". The respective menu item is displayed, if the key ModePreferences is set on true in the respective block.
If you select mode Beginner you will see a lower amount of functions (menu items, buttons, context menu commands) in the user interface.
The selected mode shows a checkmark.
If ERP is available then the display of UI elements can be designed role-dependent (in addition).
In order to avoid redundant settings the declaration of the elements happens in two levels:
At first all needed roles are assigned to types.
[ROLES] DUMMY=TYP_A LOC1=TYP_B LOC2=TYP_A LOC3=TYP_A etc.
In a second step the desired actions (elements) are stated in the respective [TYP_] block.
[TYP_A] MODE_BEGINNER=false MODE_PROFESSIONAL=false Bugreport_Clicked=true din962=true ShowHideAvoidPartsButton=true prefcatalogs=true StartupPageClicked=true List view of parameters=true Table view of parameters=true etc.
[TYP_B] MODE_BEGINNER=false MODE_PROFESSIONAL=false Bugreport_Clicked=true din962=true ShowHideAvoidPartsButton=true prefcatalogs=true StartupPageClicked=true List view of parameters=true Table view of parameters=true etc.
If there is information in two different, valid blocks, then the information is merged.
![]() |
Tip |
---|---|
Scroll through the section and have a look on the figures. In connection with the figures you can find the corresponding action names. Also see the general notes on how to handle the config editor under User interface at a glance and Full-text search. |
The following shows figures of menus and toolbars with contained menu items and buttons. The corresponding action names (key names) can be found in connection with the respective figures.
In the following you can find a listing of the single functions with connected action name (key name):
Icon | Display text or tooltip |
Action name (key name) in menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
Open | FileMenuContent | ||
Save template as... | FileMenuContent | ||
[hasSubMenuAktions] AktionRecentFilesListName=
|
FileMenuContent and AktionRecentFilesListName | ||
Exit | FileMenuContent |
The creation of the structure happens in the configuration file menustructure_PARTdataManager.cfg.
In the following you can find a listing of the single functions with connected action name (key name):
Icon | Display text or tooltip |
Action name (key name) in menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
||||
ExportMenuContent | |||||||
Export to CAD (submenu item) | ExportMenuContent and ExportToolbarContent | ||||||
Not used | |||||||
|
ExportToolbarContent and ExportMenuContent | ||||||
currently not used | |||||||
As native file | ExportMenuContent | ||||||
ExportMenuContent | |||||||
ExportFileMenuStatic | ExportMenuContent |
Creation of
structure happens in the configuration file menustructure_PARTdataManager.cfg
.
For menu see here, for toolbar see here.
In the following you can find a listing of the single functions with connected action name (key name):
Icon | Display text or tooltip |
Action name (key name) in menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
|
LinkDbLogin | LinkDatabaseToolbarContent and ErpMenuContent | |
|
LinkDbChangeGroup | LinkDatabaseToolbarContent and ErpMenuContent | |
|
CallLinkMgr | LinkDatabaseToolbarContent and ErpMenuContent | |
|
LinkDbBackToMgr | LinkDatabaseToolbarContent and ErpMenuContent | |
|
LinkDbCancelBackToMgr | LinkDatabaseToolbarContent and ErpMenuContent | |
|
LinkDbSendMail | LinkDatabaseToolbarContent and ErpMenuContent | |
|
LinkDbAddToDb | LinkDatabaseToolbarContent and ErpMenuContent | |
|
LinkDbShowLegend | LinkDatabaseToolbarContent and ErpMenuContent | |
|
PreferredRanges | LinkDatabaseToolbarContent and ErpMenuContent | |
|
LinkDbClassify | LinkDatabaseToolbarContent and ErpMenuContent |
|
In the following you can find a listing of the single functions with connected action name (key name):
Icon | Display text or tooltip |
Action name (key name) in menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
|
erp_psol_mm_vars | LinkDatabaseToolbarContent and ErpMenuContent | |
|
Set the sorting order for currently opened project | SORTTABLE | LinkDatabaseToolbarContent and ErpMenuContent |
|
erp_dbedit | LinkDatabaseToolbarContent and ErpMenuContent | |
|
show_dbdata | LinkDatabaseToolbarContent and ErpMenuContent |
The creation
of the structure happens in the configuration file menustructure_PARTdataManager.cfg
.
For menu see ???, for toolbar see ???.
|
In the following you can find a listing of the single functions with connected action name (key name):
Icon | Display text or tooltip |
Action name (key name) in menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
|
SAP MM creation | sap or erp_sap_showdis | LinkDatabaseToolbarContent or AddSapToolbarContent |
|
Change material | ChangeMatButton | LinkDatabaseToolbarContent |
|
Display material | DisplayMatButton | LinkDatabaseToolbarContent |
|
Search material | SearchMatButton | LinkDatabaseToolbarContent |
The
creation of the structure happens in the configuration file menustructure_PARTdataManager.cfg
.
See LinkDatabaseToolbarContent or
AddSapToolbarContent.
View menu / Views toolbar / Assembly toolbar / Default toolbar
In the following you can find a listing of the single functions with connected action name (key name):
Automatic recalc on/off | |||
Display / hide options for DIN 962 standards | |||
Show/hide parts that should be avoided |
Functional control happens in partsol.cfg -> Block [EOLService]. |
||
Preferred Catalog | |||
First steps | |||
PARTsolutions User Portal | |||
PDF Datasheet | |||
Catalog Feedback |
Bug report can also be switched on and off via configuration file. On this see Section 1.7.5.4, “ bugreport.cfg - Catalog Feedback ”. |
||
"End of Life" for lines | |||
storage area |
The creation
of the structure happens in the configuration file menustructure_PARTdataManager.cfg
.
See Ansichten Toolbar / Ansicht
Menü / Extras Menü / Assembly
Toolbar / Standard Toolbar.
In the following you can find a listing of the single functions with connected action name (key name):
The creation
of the structure happens in the configuration file menustructure_PARTdataManager.cfg
.
See Section 1.7.9.2.2.1.1.1, “Menus”.
In the following you can find a listing of the single functions with connected action name (key name):
The creation
of the structure happens in the configuration file menustructure_PARTdataManager.cfg
.
See Section 1.7.9.2.2.1.1.1, “Menus”.
In the following you can find a listing of the single functions with connected action name (key name):
Icon | Display text or tooltip |
Action name (key name) in menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
PARTupdate | |||
PARTadmin | |||
PARTbom... | |||
Bill of material | |||
currently not used | ExtrasPARTbomSelected | ||
Physical properties of the part | |||
Purchineering |
To control subitems see below. |
|
|
Duplicates Report |
To control subitems see below. |
|
|
Unmachined / Finished part report |
To control subitems see below. |
|
|
Report generations on server... | ExtrasServerJobList | ||
Connect assemblies automatically | |||
Start VBS/VBB script... | |||
Select mode | ModePreferences | ||
Settings... |
The creation
of the structure happens in the configuration file menustructure_PARTdataManager.cfg
.
Submenus of Purchineering,Duplicates Report and Unmachined / Finished part report
In order to provide submenus the block [hasSubMenuAktions] is used.
The
subitems of the menu item Purchineering are created in the
configuration file menustructure_PARTdataManager.cfg
,
in the block [hasSubMenuAktions]
. See Section 1.7.9.2.2.1.2, “
Block
[hasSubMenuActions]
”.
Icon | Display text or tooltip |
Action name (key name) in
menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
![]() |
see [hasSubMenuActions] | ||
![]() |
Find suppliers -> Create report... | see [hasSubMenuActions] | |
![]() |
Cost mockup -> Create report... | see [hasSubMenuActions] | |
![]() |
Supplier branches -> Create report... | see [hasSubMenuActions] | |
![]() |
Kanban Report -> Create report... | see [hasSubMenuActions] |
Icon | Display text or tooltip |
Action name (key name) in
menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
![]() |
see [hasSubMenuActions] | ||
![]() |
Find suppliers -> Report management... | see [hasSubMenuActions] | |
![]() |
Cost mockup -> Report management... | see [hasSubMenuActions] | |
![]() |
Supplier branches -> Report management... | see [hasSubMenuActions] | |
![]() |
Kanban Report -> Report management... | see [hasSubMenuActions] |
The
subitems of the menu item Duplicates Report are created in the
configuration file menustructure_PARTdataManager.cfg
,
in the block [hasSubMenuAktions]
. See Section 1.7.9.2.2.1.2, “
Block
[hasSubMenuActions]
”.
Icon | Display text or tooltip |
Action name (key name) in
menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
see [hasSubMenuActions] | |||
see [hasSubMenuActions] |
Submenus of Unmachined / Finished part report
The
subitems of the menu item Unmachined / Finished part report
are created in the configuration file menustructure_PARTdataManager.cfg
,
in the block [hasSubMenuAktions]
. See Section 1.7.9.2.2.1.2, “
Block
[hasSubMenuActions]
”.
Icon | Display text or tooltip |
Action name (key name) in
menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
![]() |
see [hasSubMenuActions] | ||
![]() |
see [hasSubMenuActions] |
Icon | Display text or tooltip |
Action name (key name) in
menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
![]() |
see [hasSubMenuActions] | ||
![]() |
see [hasSubMenuActions] |
In the following you can find a listing of the single functions with connected action name (key name):
The creation of the structure happens in the configuration file menustructure_PARTdataManager.cfg.
In the following you can find a listing of the single functions with connected action name (key name):
Icon | Display text or tooltip |
Action name (key name) in menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
Manage views | LayoutMenuContent | ||
Recover standard | LayoutMenuContent |
The creation of the structure happens in the configuration file menustructure_PARTdataManager.cfg.
In the following you can find a listing of the single functions with connected action name (key name):
The
creation of the structure happens in the configuration file menustructure_PARTdataManager.cfg
.
In the following you can find a listing of the single functions with connected action name (key name):
Icon | Display text or tooltip |
Action name (key name) in menuvisibility_PARTdataManager.cfg
|
Occurrence in menu and toolbar (Respective specification under
|
ct_add_class | ClassificationToolbarContent | ||
Remove class | ct_delete_class | ClassificationToolbarContent | |
ct_edit_class | ClassificationToolbarContent | ||
ct_move_class | ClassificationToolbarContent | ||
ct_add_datasets | ClassificationToolbarContent | ||
ct_delete_datasets | ClassificationToolbarContent | ||
ct_edit_dataset | ClassificationToolbarContent | ||
ct_move_datasets | ClassificationToolbarContent | ||
ct_copy_dataset | ClassificationToolbarContent | ||
ct_edit_views | ClassificationToolbarContent | ||
ct_batch_update | ClassificationToolbarContent | ||
ct_move_geomsearch | ClassificationToolbarContent | ||
ct_update_tool | ClassificationToolbarContent | ||
ct_create_classification | ClassificationToolbarContent |
The creation of the structure happens in the configuration file menustructure_PARTdataManager.cfg.
In this section you can find the PARTdataManager action names for context menu commands.
![]() |
Note |
---|---|
All commands concerning the index tree start with the substring "IndexTree". Structural
layout of all context menu commands happens in The
visibility of commands (menu item, button, context menu command) has
to be changed in the configuration file |
![]() |
Tip |
---|---|
Scroll through the section and have a look on the figures. In connection with the figures you can find the corresponding action names and so the respective action names. Also see the general notes on how to handle the config editor under Benutzeroberfläche im Überblick and Volltextsuche. |
Additional context menu commands Favorites
Additional context menu commands on project level: / Part comparison:
Icon | Display text or tooltip |
Action name (key name) in menuvisibility_PARTdataManager.cfg
|
This action is only available in developer mode. On this see Section 1.7.4.3.3.1, “ Key "IsAdmin" - User mode ”. |
||
This action is only available in developer mode. On this see Section 1.7.4.3.3.1, “ Key "IsAdmin" - User mode ”. |
[47] You can enhance the amount of modes anytime. Simply add a new key in the block [COMMON] and then set the corresponding block with the desired actions.