![]() |
In the DIN, EN and ISO datasheets (as well as other country standards) certain sizes are sometimes considered to be avoided. If the option is activated, lines to be avoided are marked in the PARTdataManager Part view.
In order to show/hide parts uses the button Show/hide lines to be avoided.
Settings on this are carried out in the block [EOLService]:
LinkdbVariants: Show/hide LinkDB variants in the table
true:
LinkDB variants are not basically hidden and the visibility can be
controlled via .[42]
ShowLines: Show/hide the "to avoid" lines in the table
true:
Lines marked with "to avoid"[43] are not basically hidden and the visibility can be
controlled via .
ShowButton: Activation/Deactivation of the button
|
[42] With
existing ERP integration LinkDB variants can be created via
. On this see Section 4.7, “ERP toolbar
and menu
”.
[43] The markup happens on the side of catalog manufacturer. On this see Kennzeichnung zu vermeidender Teile.