![]() |
Note |
---|---|
For ECAD systems the connection between 3D coordinates and symbolic representation in 2 dimensions is essential. |
In the following
the procedure of classifying is described with the Phoenix relay terminal with order number
2964500
:
Set needed Connection points accordingly in PARTdesigner.
Assign connection points to the class CNS_CP|4|3 (Electrical Connection) and assign a Name and an Identifier.
The Identifier (in this figure exemplarily 3.1) has been named analogously to the naming in eCl@ss.
The name (in this figure 12) has been assigned analogously to the circuit diagram.
Via attribute Connection EclassSymbolMap, determine symbol (function code), function group and pin number to be used.
The syntax of attribute Connection EclassSymbolMap is as follows:
Function code || Function no. || Pin no.
For a correct classifying the respective string needs to be found. Following example shows function number 2 and pin number 1.
S00230 || 2 || 1
The function
code S00230 complies with a changeover .[53]
![]() |
Note |
---|---|
Carry out classifying carefully, so that errors are prevented. The respective interfaces cannot check the correctness of entries in attribute Connection EclassSymbolMap. |
[53] A table of CAx function symbols can be found on the website http://wiki.eclass.eu/wiki/CAx_Funktionssymbole (CADENAS-internally stored in the Excel table eCl@ss CAx_Funktionssymbole 24.02.2018.xlsx).