In this section
you can find details on the setting options of Text .
General: See Section 10.4.2, “General settings”.
Language: This function is not available. If you need the text in several languages, manage this via Media Variables. Then the translation has to be performed either in the Media editor (see ???) or in PARTproject (see Section 5.9.17.2, “Translate Media Variables ”).
Click on the desired icon in order to align text at top, middle or bottom.
Fonts displayed in the list field are not identical with fonts installed on the system, because only allowed fonts are shown and only these shall be used. As long as these fonts are used, it is ensured that they will be embedded in the template (partial embedding). If special, not supported font types shall be used, then please contact CADENAS.
Fallback: The fallback is currently only done for language charset problems. For example, the font only contains Latin1 characters (part of the Latin chars) and you export in Chinese which needs other characters, the fallback is performed. The last fallback in this chain is the Droid Sans.
Standard paragraph format / List formats:
In the list field of the paragraph formats you can find options like Standard, different bulleted list formats or numbered list formats. Via the little list field to the right you can control the indentation level (starting with 0 = no indent).
It is possible to use variables as text:
Project variables such as "$NB.", "$NENN.", "$LINA." for example
Media variables: On this see Section 10.6, “Edit Media Variables in the Media editor ”.
Special variables, which can be inserted via context menu. These are marked with "$$" (Example: $$MASS$$).