The Himalayas, or Himalaya ( or ), form a mountain range in Asia separating the plains of the Indian subcontinent from the Tibetan Plateau.
The Himalayan range has many of the Earth's highest peaks, including the highest, Mount Everest. The Himalayas include over fifty mountains exceeding 7,200 metres (23,600 ft) in elevation, including ten of the fourteen 8000m peaks. By contrast, the highest peak outside Asia – Aconcagua, in the Andes – is 6,961 metres (22,838 ft) tall.
The Himalayan range is bordered on the northwest by the Karakoram and Hindu Kush ranges, on the north by the Tibetan Plateau and on the south by the Indo-Gangetic Plain. The Himalayas are distinct from the other great ranges of central Asia, although sometimes the term Himalaya is loosely used to include the Karakoram and some of the other ranges. The Himalayas – inhabited by 52.7 million people – are spread across five countries: India, Nepal, Bhutan, China and Pakistan, with the first three countries having sovereignty over most of the range. Some of the world's major rivers, the Indus, the Ganges and the Tsangpo-Brahmaputra, rise in the Himalayas, and their combined drainage basin is home to roughly 600 million people. The Himalayas have profoundly shaped the cultures of the Indian subcontinent; many Himalayan peaks are sacred in Hinduism and Buddhism.
Lifted by the subduction of the Indian tectonic plate under the Eurasian Plate, the Himalayan mountain range runs, west-northwest to east-southeast, in an arc 2,400 kilometres (1,500 mi) long. Its western anchor, Nanga Parbat, lies just south of the northernmost bend of Indus river. Its eastern anchor, Namcha Barwa, is just west of the great bend of the Tsangpo river. From the north, the chain is limited by a 50–60 kilometres (31–37 mi) wide tectonic valley called the Indus-Tsangpo Suture. Towards the south the arc of the Himalaya is ringed by the very low Gangetic plain. The range varies in width from 350 kilometres (220 mi) in the west (Kashmir) to 150 kilometres (93 mi) in the east (Arunachal Pradesh).