A garden is a planned space, usually outdoors, set aside for the display, cultivation, or enjoyment of plants and other forms of nature. The garden can incorporate both natural and man-made materials. The most common form today is a residential garden, but the term garden has traditionally been a more general one. Zoos, which display wild animals in simulated natural habitats, were formerly called zoological gardens.[1][2] Western gardens are almost universally based on plants, with garden often signifying a shortened form of botanical garden. Some traditional types of eastern gardens, such as Zen gardens, use plants sparsely or not at all.
Gardens may exhibit structural enhancements including statuary, follies, pergolas, trellises, stumperies, dry creek beds and water features such as fountains, ponds (with or without fish), waterfalls or creeks. Some gardens are for ornamental purposes only, while some gardens also produce food crops, sometimes in separate areas, or sometimes intermixed with the ornamental plants. Food-producing gardens are distinguished from farms by their smaller scale, more labor-intensive methods, and their purpose (enjoyment of a hobby or self-sustenance rather than producing for sale). Flower gardens combine plants of different heights, colors, textures, and fragrances to create interest and delight the senses.
Gardening is the activity of growing and maintaining the garden. This work is done by an amateur or professional gardener. A gardener might also work in a non-garden setting, such as a park, a roadside embankment, or other public space.
Landscape architecture is a related professional activity with landscape architects tending to specialise in design for public and corporate clients.
Etymology
The etymology of the word gardening refers to enclosure: it is from Middle English gardin, from Anglo-French gardin, jardin, of Germanic origin; akin to Old High German gard, gart, an enclosure or compound, as in Stuttgart. See Grad (Slavic settlement) for more complete etymology.[3] The words yard, court, and Latin hortus (meaning "garden," hence horticulture and orchard), are cognates—all referring to an enclosed space.[4]
The term "garden" in British English refers to a small enclosed area of land, usually adjoining a building.[5] This would be referred to as a yard in American English.
Design
Garden design is the process of creating plans for the layout and planting of gardens and landscapes. Gardens may be designed by garden owners themselves, or by professionals. Professional garden designers tend to be trained in principles of design and horticulture, and have a knowledge and experience of using plants. Some professional garden designers are also landscape architects, a more formal level of training that usually requires an advanced degree and often a state license.
Elements of garden design include the layout of hard landscape, such as paths, rockeries, walls, water features, sitting areas and decking, as well as the plants themselves, with consideration for their horticultural requirements, their season-to-season appearance, lifespan, growth habit, size, speed of growth, and combinations with other plants and landscape features. Consideration is also given to the maintenance needs of the garden, including the time or funds available for regular maintenance, which can affect the choices of plants regarding speed of growth, spreading or self-seeding of the plants, whether annual or perennial, and bloom-time, and many other characteristics. Garden design can be roughly divided into two groups, formal and naturalistic gardens.[6]
The most important consideration in any garden design is how the garden will be used, followed closely by the desired stylistic genres, and the way the garden space will connect to the home or other structures in the surrounding areas. All of these considerations are subject to the limitations of the budget. Budget limitations can be addressed by a simpler garden style with fewer plants and less costly hard landscape materials, seeds rather than sod for lawns, and plants that grow quickly; alternatively, garden owners may choose to create their garden over time, area by area.
Elements
Most gardens consist of a mix of natural and constructed elements, although even very 'natural' gardens are always an inherently artificial creation. Natural elements present in a garden principally comprise flora (such as trees and weeds), fauna (such as arthropods and birds), soil, water, air and light. Constructed elements include paths, patios, decking, sculptures, drainage systems, lights and buildings (such as sheds, gazebos, pergolas and follies), but also living constructions such as flower beds, ponds and lawns.
Uses
A garden can have aesthetic, functional, and recreational uses:
- Cooperation with nature
- Observation of nature
- Relaxation
- Family dinners on the terrace
- Children playing in the garden
- Reading and relaxing in the hammock
- Maintaining the flowerbeds
- Pottering in the shed
- Cottaging in the bushes
- Basking in warm sunshine
- Escaping oppressive sunlight and heat
- Growing useful produce
- Flowers to cut and bring inside for indoor beauty
- Fresh herbs and vegetables for cooking
Types
Gardens may feature a particular plant or plant type(s):
Gardens may feature a particular style or aesthetic:
Other types:
Environmental impacts
Gardeners may cause environmental damage by the way they garden, or they may enhance their local environment.
Damage by gardeners can include direct destruction of natural habitats when houses and gardens are created; indirect habitat destruction and damage to provide garden materials such as peat, rock for rock gardens, and by the use of tapwater to irrigate gardens; the death of living beings in the garden itself, such as the killing not only of slugs and snails but also their predators such as hedgehogs and song thrushes by metaldehyde slug killer; the death of living beings outside the garden, such as local species extinction by indiscriminate plant collectors; and climate change caused by greenhouse gases produced by gardening.
Irrigation
Some gardeners manage their gardens without using any water from outside the garden, and therefore do not deprive wetland habitats of the water they need to survive. Examples in Britain include Ventnor Botanic Garden on the Isle of Wight, and parts of Beth Chatto's garden in Essex, Sticky Wicket garden in Dorset, and the Royal Horticultural Society's gardens at Harlow Carr and Hyde Hall.
Rain gardens absorb rainfall falling onto nearby hard surfaces, rather than sending it into stormwater drains.[7]
For irrigation, see rainwater, sprinkler system, drip irrigation, tap water, greywater, hand pump and watering can.
Climate change
Climate change will have many impacts on gardens, most of them negative, and these are detailed in 'Gardening in the Global Greenhouse' by Richard Bisgrove and Paul Hadley.[8] Gardens also contribute to climate change. Greenhouse gases can be produced by gardeners in many ways. The three main greenhouse gases are carbon dioxide, methane, and nitrous oxide. Gardeners produce carbon dioxide directly by overcultivating soil and destroying soil carbon, by burning garden 'waste' on bonfires, by using power tools which burn fossil fuel or use electricity generated by fossil fuels, and by using peat. Gardeners produce methane by compacting the soil and making it anaerobic, and by allowing their compost heaps to become compacted and anaerobic. Gardeners produce nitrous oxide by applying excess nitrogen fertiliser when plants are not actively growing so that the nitrogen in the fertiliser is converted by soil bacteria to nitrous oxide.
Gardeners can help to prevent climate change in many ways, including the use of trees, shrubs, ground cover plants and other perennial plants in their gardens, turning garden 'waste' into soil organic matter instead of burning it, keeping soil and compost heaps aerated, avoiding peat, switching from power tools to hand tools or changing their garden design so that power tools are not needed, and using nitrogen-fixing plants instead of nitrogen fertiliser.[9]
Other similar spaces
Other outdoor spaces that are similar to gardens include:
- A landscape is an outdoor space of a larger scale, natural or designed, usually unenclosed and considered from a distance.
- A park is a planned outdoor space, usually enclosed ('imparked') and of a larger size. Public parks are for public use.
- An arboretum is a planned outdoor space, usually large, for the display and study of trees.
- A farm or orchard is for the production of food stuff.
- A botanical garden is a type of garden where plants are grown both for scientific purposes and for the enjoyment and education of visitors.
- A zoological garden, or zoo for short, is a place where wild animals are cared for and exhibited to the public.
- A Kindergarten is a preschool educational institution for children and in the very sense of the word should have access or be part of a garden.
- A Männergarten is a temporary day-care and activities space for men in German-speaking countries while their wives or girlfriends go shopping. Historically, the expression has also been used for gender-specific sections in lunatic asylums, monasteries and clinics.[10]
See also