powered by CADENAS

Social Share

Amazon

Jade (1930 views - Nature)

Jade is an ornamental mineral, mostly known for its green varieties, which is featured prominently in ancient Asian art. The term jade is applied to two different minerals: Nephrite consists of a microcrystalline interlocking fibrous matrix of the calcium, magnesium-iron rich amphibole mineral series tremolite (calcium-magnesium)-ferroactinolite (calcium-magnesium-iron). The middle member of this series with an intermediate composition is called actinolite (the silky fibrous mineral form is one form of asbestos). The higher the iron content, the greener the colour. Jadeite is a sodium- and aluminium-rich pyroxene. The precious form of jadeite jade is a microcrystalline interlocking growth of jadeite crystals.
Go to Article

Explanation by Hotspot Model

Youtube


    

Jade

Jade

Jade is an ornamental mineral, mostly known for its green varieties, which is featured prominently in ancient Asian art. The term jade is applied to two different minerals:

  • Nephrite consists of a microcrystalline interlocking fibrous matrix of the calcium, magnesium-iron rich amphibole mineral series tremolite (calcium-magnesium)-ferroactinolite (calcium-magnesium-iron). The middle member of this series with an intermediate composition is called actinolite (the silky fibrous mineral form is one form of asbestos). The higher the iron content, the greener the colour.
  • Jadeite is a sodium- and aluminium-rich pyroxene. The precious form of jadeite jade is a microcrystalline interlocking growth of jadeite crystals.

Etymology

Jade
Chinese

The English word jade is derived (via French l'ejade and Latin ilia "flanks, kidney area")[1] from the Spanish term piedra de ijada (first recorded in 1565) or "loin stone", from its reputed efficacy in curing ailments of the loins and kidneys. Nephrite is derived from lapis nephriticus, a Latin translation of the Spanish piedra de ijada.[2]

Overview

Nephrite and jadeite

Nephrite and jadeite were used from prehistoric periods for hardstone carving. Jadeite has about the same hardness as quartz. Nephrite is slightly softer but tougher (more resistant to breakage) than jadeite. It was not until the 19th century that a French mineralogist, Alexis Damour (1808–1902), determined that "jade" was in fact two different minerals.[citation needed]

Among the earliest known jade artifacts excavated from prehistoric sites are simple ornaments with bead, button, and tubular shapes.[3] Additionally, jade was used for adze heads, knives, and other weapons, which can be delicately shaped. As metal-working technologies became available, the beauty of jade made it valuable for ornaments and decorative objects. Jadeite measures between 6.0 and 7.0 Mohs hardness, and nephrite between 6.0 and 6.5, so it can be worked with quartz or garnet sand, and polished with bamboo or even ground jade.[citation needed]

Unusual varieties

Nephrite can be found in a creamy white form (known in China as "mutton fat" jade) as well as in a variety of light green colours, whereas jadeite shows more colour variations, including blue, red, black, dark green, lavender and white.[4] Of the two, jadeite is rarer, documented in fewer than 12 places worldwide. Translucent emerald-green jadeite is the most prized variety, both historically and today. As "quetzal" jade, bright green jadeite from Guatemala was treasured by Mesoamerican cultures, and as "kingfisher" jade, vivid green rocks from Burma became the preferred stone of post-1800 Chinese imperial scholars and rulers. Burma (Myanmar) and Guatemala are the principal sources of modern gem jadeite. In the area of Mogaung in the Myitkyina District of Upper Burma, jadeite formed a layer in the dark-green serpentine, and has been quarried and exported for well over a hundred years.[5] Canada provides the major share of modern lapidary nephrite. Nephrite jade was used mostly in pre-1800 China as well as in New Zealand, the Pacific Coast and the Atlantic Coast of North America, Neolithic Europe, and Southeast Asia. In addition to Mesoamerica, jadeite was used by Neolithic Japanese and European cultures.

History

Prehistoric and historic China

Large "mutton fat" nephrite jade displayed in Hotan Cultural Museum lobby.

During Neolithic times, the key known sources of nephrite jade in China for utilitarian and ceremonial jade items were the now depleted deposits in the Ningshao area in the Yangtze River Delta (Liangzhu culture 3400–2250 BC) and in an area of the Liaoning province and Inner Mongolia (Hongshan culture 4700–2200 BC).[6] Dushan Jade was being mined as early as 6000 BC. In the Yin Ruins of the Shang Dynasty (1600 to 1050 BC) in Anyang, Dushan Jade ornaments were unearthed in the tomb of the Shang kings. Jade was used to create many utilitarian and ceremonial objects, from indoor decorative items to jade burial suits. Jade was considered the "imperial gem". From the earliest Chinese dynasties to the present, the jade deposits most in use were not only those of Khotan in the Western Chinese province of Xinjiang but other parts of China as well, such as Lantian, Shaanxi. There, white and greenish nephrite jade is found in small quarries and as pebbles and boulders in the rivers flowing from the Kuen-Lun mountain range eastward into the Takla-Makan desert area. The river jade collection is concentrated in the Yarkand, the White Jade (Yurungkash) and Black Jade (Karakash) Rivers. From the Kingdom of Khotan, on the southern leg of the Silk Road, yearly tribute payments consisting of the most precious white jade were made to the Chinese Imperial court and there worked into objects d'art by skilled artisans as jade had a status-value exceeding that of gold or silver. Jade became a favourite material for the crafting of Chinese scholars' objects, such as rests for calligraphy brushes, as well as the mouthpieces of some opium pipes, due to the belief that breathing through jade would bestow longevity upon smokers who used such a pipe.[7]

Jadeite, with its bright emerald-green, pink, lavender, orange and brown colours was imported from Burma to China only after about 1800. The vivid green variety became known as Feicui (翡翠) or Kingfisher (feathers) Jade. It quickly became almost as popular as nephrite and a favorite of Qing Dynasty's nouveau riche, while scholars still had strong attachment to nephrite (white jade, or Khotan), which they deemed to be the symbol of a nobleman.

In the history of the art of the Chinese empire, jade has had a special significance, comparable with that of gold and diamonds in the West.[8] Jade was used for the finest objects and cult figures, and for grave furnishings for high-ranking members of the imperial family.[8] Due to that significance and the rising middle class in China, today the finest jade when found in nuggets of “mutton fat” jade – so-named for its marbled white consistency – can sell for $3,000 an ounce, a tenfold increase from a decade ago.[9]

The Chinese character 玉[10] (yù) is used to denote the several types of stone known in English as "jade" (e.g. 玉器, jadewares), such as jadeite (硬玉, 'hard jade', another name for 翡翠) and nephrite (軟玉, 'soft jade'). But because of the value added culturally to jades throughout Chinese history, the word has also come to refer more generally to precious or ornamental stones,[11] and is very common in more symbolic usage as in phrases like 拋磚引玉/抛砖引玉 (lit. 'casting a brick (i.e. the speaker's own words) to draw a jade (i.e. pearls of wisdom from the other party)'), 玉容 (a beautiful face; 'jade countenance'), and 玉立 (slim and graceful; 'jade standing upright'). The character has a similar range of meanings when appearing as a radical as parts of other characters.

Prehistoric and historic India

The Jain temple of Kolanpak in the Nalgonda district, Andhra Pradesh, India is home to a 5-foot (1.5 m) high sculpture of Mahavira that is carved entirely out of jade. It is the largest sculpture made from a single jade rock in the world. India is also noted for its craftsman tradition of using large amounts of green serpentine or false jade obtained primarily from Afghanistan in order to fashion jewellery and ornamental items such as sword hilts and dagger handles.[5]

Prehistoric and early historic Korea

The use of jade and other greenstone was a long-term tradition in Korea (c. 850 BC – AD 668). Jade is found in small numbers of pit-houses and burials. The craft production of small comma-shaped and tubular "jades" using materials such as jade, microcline, jasper, etc., in southern Korea originates from the Middle Mumun Pottery Period (c. 850–550 BC).[12] Comma-shaped jades are found on some of the gold crowns of Silla royalty (c. 300/400–668 AD) and sumptuous elite burials of the Korean Three Kingdoms. After the state of Silla united the Korean Peninsula in 668, the widespread popularisation of death rituals related to Buddhism resulted in the decline of the use of jade in burials as prestige mortuary goods.

Southeast Asia

Today, it is estimated that Burma is the origin of upwards of 70 percent of the world's supply of high-quality jadeite. Most of the jadeite mined in Burma is not cut for use in Burma, instead being transported to other nations, primarily in Asia, for use in jewelry and other products. The jadeite deposits found in Kachinland, in Burma’s northern regions is the highest quality jadeite in the world, considered precious by sources in China going as far back as the 10th century. Jadeite in Burma is primarily found in the “Jade Tract” located in Lonkin Township in Kachin State in northern Burma which encompasses the alluvial region of the Uyu River between the 25th and 26th parallels. Present-day extraction of jade in this region occurs at the Phakant-gyi, Maw Se Za, Tin Tin, and Khansee mines. Khansee is also the only mine that produces Maw Sit Sit, a type of jade.[3] Mines at Tawmao and Hweka are mostly exhausted. From to 1964 to 1981, mining was exclusively an enterprise of the Myanmar government. In 1981, 1985, and 1995, the Gemstone laws were modified to allow increasing private enterprise. In addition to this region, there are also notable mines in the neighboring Sagaing District, near the towns of Nasibon and Natmaw and Hkamti. Sagaing is a district in Myanmar proper, not a part of the ethic Kachin State. Archaeologists have discovered two forms of jade that can be found across Taiwan through the Philippines, East Malaysia, central and southern Vietnam, and even extending to eastern Cambodia and peninsular Thailand. These two forms are called linling-o penannular earring with three pointed circumferential projections and the double animal-headed ear pendant. The forms are very similar in size and range from about 30–35mm in diameter. Furthermore, radiocarbon dates have dated these forms in Southeast Asia from around 500 BC to 500 AD.[13] The electron probe microanalysis shows that the raw material of these two types of artifacts was nephrite jade from Taiwan called Fengtian nephrite. Evidence recovered from multiple sites from Taiwan, the Philippines, and the mainland southeast Asia suggests that Taiwan was the main source of the exchange of this kind jade. During the Iron Age of Southeast Asia, there may have been skilled craftsmen traveling from Taiwan to southeast Asia along the coastline of the South China Sea, making jade ornaments for local inhabitants.[14]

Māori

Nephrite jade in New Zealand is known as pounamu in the Māori language (often called "greenstone" in New Zealand English), and plays an important role in Māori culture. It is considered a taonga, or treasure, and therefore protected under the Treaty of Waitangi, and the exploitation of it is restricted and closely monitored. It is found only in the South Island of New Zealand, known as Te Wai Pounamu in Māori—"The [land of] Greenstone Water", or Te Wahi Pounamu—"The Place of Greenstone".

Pounamu taonga increase in mana (prestige) as they pass from one generation to another. The most prized taonga are those with known histories going back many generations. These are believed to have their own mana and were often given as gifts to seal important agreements.

Tools, weapons and ornaments were made of it; in particular adzes, the 'mere' (short club), and the hei-tiki (neck pendant). Nephrite jewellery of Maori design is widely popular with locals and tourists, although some of the jade used for these is now imported from British Columbia and elsewhere.[15]

Pounamu taonga include tools such as toki (adzes), whao (chisels), whao whakakōka (gouges), ripi pounamu (knives), scrapers, awls, hammer stones, and drill points. Hunting tools include matau (fishing hooks) and lures, spear points, and kākā poria (leg rings for fastening captive birds); weapons such as mere (short handled clubs); and ornaments such as pendants (hei-tiki, hei matau and pekapeka), ear pendants (kuru and kapeu), and cloak pins.[16][17] Functional pounamu tools were widely worn for both practical and ornamental reasons, and continued to be worn as purely ornamental pendants (hei kakï) even after they were no longer used as tools.[18]

Canada

Jade was first identified in Canada by Chinese settlers in 1886 in British Columbia. At this time jade was considered worthless as they were searching for gold. Jade was not commercialized in Canada until the 1970s. The mining business Loex James Ltd., which was started by two Californians, began commercial mining of Canadian jade in 1972.[19]

Mining

Mining is done from large boulders that contain bountiful deposits of jade. Jade is exposed using diamond-tipped core drills in order to extract samples. This is done to ensure that the jade meets requirements. Hydraulic spreaders are then inserted into cleavage points in the rock so that the jade can be broken away. Once the boulders are removed and the jade is accessible, it is broken down into more manageable 10-tonne pieces using water-cooled diamond saws. The jade is then loaded onto trucks and transported to the proper storage facilities.[20]

Mesoamerica

Jade was a rare and valued material in pre-Columbian Mesoamerica. The only source from which the various indigenous cultures, such as the Olmec and Maya, could obtain jade was located in the Motagua River valley in Guatemala.[citation needed] Jade was largely an elite good, and was usually carved in various ways, whether serving as a medium upon which hieroglyphs were inscribed, or shaped into symbolic figurines. Generally, the material was highly symbolic, and it was often employed in the performance of ideological practices and rituals.

Enhancement

Jade may be enhanced (sometimes called "stabilized"). Some merchants will refer to these as grades, but degree of enhancement is different from colour and texture quality. In other words, Type A jadeite is not enhanced but can have poor colour and texture. There are three main methods of enhancement, sometimes referred to as the ABC Treatment System:[21]

  • Type A jadeite has not been treated in any way except surface waxing.
  • Type B treatment involves exposing a promising but stained piece of jadeite to chemical bleaches and/or acids and impregnating it with a clear polymer resin. This results in a significant improvement of transparency and colour of the material. Currently, infrared spectroscopy is the most accurate test for the detection of polymer in jadeite.
  • Type C jade has been artificially stained or dyed. The effects are somewhat uncontrollable and may result in a dull brown. In any case, translucency is usually lost.
  • B+C jade is a combination of B and C: it has been both impregnated and artificially stained.
  • Type D jade refers to a composite stone such as a doublet comprising a jade top with a plastic backing.

See also



This article uses material from the Wikipedia article "Jade", which is released under the Creative Commons Attribution-Share-Alike License 3.0. There is a list of all authors in Wikipedia

Nature

3d,model,rendering,library,tree,bush,flower,landscape,design,architecure