powered by CADENAS

Manual

Manual

3.1.1.6.11.6. Settings

In the following the setting options are explained:

  • Search type

    The search type (Text search, Geometric Search, etc.) can be optionally colored.

  • Percent

    For the display of the geometrical similarity you have the following options:

    • Off

    • black/white

    • Color

  • Preview Image

  • Similar Nodes

    The red number in the downright corner shows the number of similar nodes. When you click on the node, then all other similar nodes are displayed with red frame.

  • Company Logo

  • Icons

    The same icons of the standard view are also displayed in the CloudNavigator.

    Parts transferred to the part comparison are marked with a special icon .

    Part has been transferred to the part comparison

    Part has been transferred to the part comparison

    With ERP integration in the Single parts mode ERP icons are displayed.

    With ERP integration

    With ERP integration

    With ERP integration in the parts and part families mode the index tree colors are overtaken.

    With ERP integration

    With ERP integration

    [Note] Note

    When the mouse cursor is moved over an icon, a tooltip is displayed.

  • Title

  • Details

  • Mark new Results

    Optionally you can display the "New" tab top right.

  • Part information displayed enlarged

    If the results in the Cloud Navigator are zoomed out in order to keep the overview, then to display the part information enlarged is helpful. Move the mouse cursor over the desired part.

  • Search settings

    • Number search results: Number of displayed search results. Change the setting by direct input of the desired number or via arrow keys.

      In the following figure you can see the actual number of results top right.