powered by CADENAS

Manual

Manual

2.6.6.  Replace

The following describes how single parts from the standard and supplier part library can be replaced through alternatives.

  1. Mark the desired object in the CAD system.

  2. Click on Replace.

    --> The display switches to PARTdataManager.

  3. In Part selection or only in Part view select the object which should replace the original one.

  4. Click on .

    -> The display switches back to the CAD system.

PARTsolutions
Insert 3D
Seamless
Replace
Extras
Execute Geometric Search
Insert Connection
User library
Settings
Info

Should the selected part appear several times, a query shows up whether all instances of the part or only the selected ones should be replaced.

After confirming with Yes or No, replacement begins.

Replace parts

Replace all occurrences (Yes) or only selected ones (No)?

Yes No