Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
The Search for unmachined parts detects fitting unmachined parts for the production of finished parts or finished parts which can be produced from a certain unmachined part.
An engineer is looking for a special flange. Then he wants to search for already existing unmachined parts, from which the flange can be produced, in order to avoid the redundant creation of a new unmachined part (material master). This process is very time consuming, because the parts have to be overlaid in the CAD one after another
With PARTsolutions Search for unmachined parts this can be solved much quicker.
The search detects, whether a part is completely contained in another part: The finished part has to be smaller than the unmachined part, so that it can be produced by removing wasted material. As soon as the extensions of the finished part exceed the ones of the unmachined part only at a certain point, it cannot be used at all or at least badly.
The search calculates the volume of the material to remove (waste). The less material to remove, the higher the ranking in the result list, because this criterion is determining for the manufacturing costs.
Further information on the "Search for unmachined parts" is found under Section 3.1.1.6.4.7, “ Search for unmachined parts ” and information on the other search methods, which can possibly be used in combination, is found under Section 3.1.1.6.4, “ Search methods ”.