Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Where do data records in LinkDB come from and how do they get there?
Via Add dataset to link database in PARTdataManager.
In the dialog box the ERP_PDM_NUMBER must be assigned - if the default setting in the configuration file has not been changed.
This window can optionally be extended so that "Strengths" and "Surface" e.g. can also already be specified at this point[92].
Via Add row in PARTlinkManager.
This dataset is composed of an ERP_PDM_NUMBER and must be linked with another part. See Section 5.9.1.4, “Menu buttons ”.
Import into the LinkDB from the directory tree via Import this project in database . See Section 5.8.7.2.2, “Import a project into LINKDB – Assign ERP number ”.
These datasets do not yet contain ERP_PDM_NUMBER and are thus displayed as a red row after import.
Usually during initial loading with PARTdataCenter. See Section 5.8.7.3, “ PARTdataCenter ”.