Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
5.9.2.5. "Roles" dialog
- Tabbed pages
5.9.2.5.8.
Tabbed
pages "Standard name", "Standard name (short)" and "BOM name"
|
|
---|---|
Prev | Next |
You can assign own Standard name, Standard name (short) and BOM name to each role. May be this could make sense, if roles are assigned to different projects.
Note | |
---|---|
Usually the role-specific definition of Standard name Standard name (short) and BOM name will not be useful but the overall definition under PARTlinkManager -> Extras -> Configure ERP environment [100] used preferably. |
In the following you find three examples concerning this subject:
Example 1: NB creation is default. (The result is the same without entry.)
Example 2: A condition is used.
If there is no ERP-number available, then the NB (Standard name) creation is default. Otherwise the ERP-number is used.
Example 3: The project version is attached to the Standard name.
The text areas for Standard name (short) and BOM name are selectable by the tabs on the right , as well as Standard name. The editing is analogous to Standard name.