Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
In order to read data into a CSV file, the columns must be available analogously in the ERP table.
The following description shows how you can add any additional columns to the standard configuration.
The ERP_PDM_NUMBER, MAT_NAME and DESCRIPTION are applied with the standard installation.
You reach the dialog Change database column in the PARTlinkManagerviaExtras -> Database -> Modify/create database columns.
How to configure added columns can be found in Section 5.9.1.3.3.2, “ Configure ERP environment ”.
So that the column is shown in PARTdataManager two requirements must be fulfilled.
Once a column has been successfully added, it is displayed in the Configure dialog box.
In the Modify column display section the respective column has to be set on visible via Visible entry is Yes.
In the columns Variable DB and Variable the assigned column name is shown.
The entry under Variable DB is fixed.
The entry under Variable can be adjusted if needed.
Results in the PARTdataManager
You reach the respective dialog box in PARTlinkManager via Extras --> Database --> Modify/create database columns -> Remove tabbed page. In the list field under Column name all existing database columns are listed. |
Note | |
---|---|
If the database does not support deleting of columns (such as SQLite for example), the Remove tabbed page is hidden. |
You can have the columns in the LINKTABLE and ERPTABLE displayed.
To do so, click on the Extras menu and then Database, Show database columns.
--> The window Database columns opens.
In order to save the database either use the corresponding database-own administration tools or possibly the PARTsolutions internal dialog under PARTlinkManager -> Extras -> Database -> Save/restore database. Under Action, select the option Save database or Restore database. Under Settings, select the option Use CSV file or Use external command. |
|
In the PARTlinkManager you have the option not only to edit the ERPTABLE and LINKTABLE, but also edit any number of other tables within the LINKDB.
Indicate the
tables to be changed in the file %CADENAS_SETUP%/plinkcommon.cfg
under the section ADDITIONALTABLES
.
[ADDITIONALTABLES] #:VALS_S #:HELP;default;this table is used to store references concerning PLM-systems t0=PLMTABLE #:VALS_S #:HELP;default;this table is used to store Assembly-structures with ERP-information t1=DATATABLE #:HELP;default;this table is used to store project-specific data (ie. project specific partnames for CAD-files) t2=PLMTABLE2
Add the key "t" followed by a continuously increasing number. As the value for the key, enter the database table.
Start the PARTlinkManagerconnect to the database (File -> Connect).
Select the following: Extras -> Database -> Edit additional tables.
Choose the desired table in the selection list under Select table.
--> The table is displayed in the right half of the window and can now be edited.