powered by CADENAS

Manual

Manual

4.13.1.  Creation of ERP numbers

Where do data records in LinkDB come from and how do they get there?

  1. Via Add dataset to link database in PARTdataManager.

    In the dialog box new ident-no., an ERP_PDM_NUMBER either has to be manually applied or it is created automatically with a timestamp number.[80]

    The window can optionally be extended so that material, prices or any other fields from the LinkDB can also already be specified at this point.[81]

    This figure shows a dialog box where the ERP number is automatically created.

    This figure shows a dialog box where the ERP number is automatically created.

  2. Via Add row in PARTlinkManager.

    This dataset is composed of an ERP_PDM_NUMBER and must be linked with a part. See Section 4.13.1.2.1, “Enter ERP number with PARTlinkManager ”.

  3. Via import into the LinkDB from the directory tree using Import this project in database.

    These datasets do not yet contain an ERP_PDM_NUMBER and are thus displayed as a red row after import.

    See Section 4.13.1.2.2, “Import a project into LINKDB – Assign ERP number ”.

  4. Via initial article assignment (initial filling) with PARTdataCenter. See Section 1.1, “ Article assignment (initial filling of LinkDB) ” in PARTwarehouse Manual.