Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
You can always and at any time post-install or update EDM/PDM/PLM integrations.
PDM
interface updates are occasionally made available under "www.cadenas.de -> Service ->
Download/Update -> update -> v9 -> pdm-interfaces
"
as executable programs (*.exe).
In order to start the update process, double-click on the *.exe file.
-> The installation routine is opened. Click on until you reach the EDM/PDM/PLM integrations selection dialog window.
The selection must be set to Update.
For a single workstation installation the update has now been completed.
Since during a Client-Server installation th dlls of the PDM integrations are located on the server drive, an action (for example new registration of dll) is only occasionally necessary on the client. During the next PDM restart, the updated dll is usually directly loaded.
Note | |
---|---|
Detailed information about PDM integration in general can be found under Chapter 3, PARTsolutions - PDM Integration in PARTsolutions / PARTcommunity4Enterprise - Administration Manual. |