If you want to
create a new variable, proceed as follows:
Click on
New.
-> The
input fields are cleared.
Under
Name, enter the new variable's
name.
Note
If the variable already exists,
it is automatically selected in the list und the single
parameters are shown.
Specify all other
parameters.
Note
In Designer mode, some input
fields (not needed currently) are disabled (grayed
out).
Confirm
your entries by clicking on the Commit button.
-> The
new variable is added to the list.
Commit
Note
If the name already exists, the
respective variable is automatically selected in the list
and when clicking on Commit the values or settings
are adopted. If the name is not yet existing, a new line is
created.
Rename
Select the
desired variable in the list.
Click on
the Rename
button.
-> The
dialog box Rename variable is opened.
Enter the
new variable name.
Note
Only characters and numbers are
allowed, all other tokens (e.g. !,“,§,$,%,&,/, etc.)
are ignored.
Confirm
with OK.
-> The
variable is renamed.
Note
When renaming
variables, variables in equations (calculating the 3d
object) are automatically renamed as well!
So Variables variables can be
renamed „globally“.
Variable entries under
Identification data data
or for Description of geometry have
to be adjusted accordingly.
Delete
Select the
desired variable in the list.
Click on
the Delete
button.
Note
However, deleting is only
possible, if all design elements which have been created
with the help of this variable, have been deleted
before. So variables which are used in the sketch,
cannot be deleted. In such a case the following message
is displayed: Variable is still in use..
Entries of this variable under
Identification data or
Description of geometry have
to be adjusted accordingly.