Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
PARTsolutions offers the possibility to connect ERP systems via link-database. This results in the potential to represent customer-specific business processes.[62]
Precondition is, that the value range variables are tagged by the categories of the Identification type. Only then a faultless processing of these or the resulting NB and LINA is ensured in the ERP system.
Under Identification type, the following options are given:
Values that are necessary for dimension and/or product standards.
For order numbers or technical specifications, etc. (Characteristics that do not have anything to do with geometry or function)
|
There is no functional difference between geometry and object attribute. Currently these are handled equally.
Dimension attributes are used with half-finished products and profiles that do not have fixed dimensions. The length (L) can be cleared within the default value range before export. |
With the customizing of PARTsolutions, in accordance with ERP guidelines, it is decided whether a part with different lengths obtains different identification numbers, or if the identification number remains the same. In the first case, the corresponding field will be pinned (white background), in the later, not.
[62] On this see Section 4.17.3, “ Pinning Dimension attribute OnOff / plinkcommon.cfg -> Block [PARTdataManager] -> Key "LockDimRange" ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.