Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Create the needed variables with their respective values. You can find them above in the dimensioning diagram and table.
Description: As the variable name is limited to 10 characters, you can add a brief Description in the respective field.
If no Value ranges and no Attribute algorithms and no specific settings such as Identification type shall be set, you can model a part completely in the Designer mode.
Table mode is required, in order to create Table, Value ranges and Attribute algorithms.
If variables had been created only in the Designer mode initially (just to use them for a quick creation of the 3D model), later it is necessary to save them in the tab/tac file, in order to link them with the table and fill them dynamically.
If at first only the table is created, it is sufficient to save the variables in the Table mode. Later those variables have to be saved in the Designer mode in addition, which are required for the creation of the model (in the sketcher).
Therefor save the variables in the Dual mode. Then they are saved both in the 3db file and in the tab/tac file.
You can change the Mode anytime, when selecting a variable, changing the mode in the list field and clicking on .
Detailed information on this can be found under Section 6.8.4, “ Designer mode | Table mode | Dual mode ”.
Equation: Enter a variable value (e.g. 4.6 for the variable DA).
Assign a certain Value (from the table) to the variable or predicate the content on other variables (2*D1, D1+D2, etc.).
After all specifications concerning the variable are made, confirm with a click on .
--> The variable is taken into the list above.
Change: To redefine the equation value or the description, precede as you did when you defined a variable.