Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
PARTupdate automatically informs you on catalog
updates via icon PARTupdate displayed in the task bar.
When double-clicking on the icon the PARTupdate short info opens.
The number of downloadable catalogs and which in detail is displayed here.
When clicking
on the button the dialog box PARTsolutions - Available catalogs opens with a list of all downloadable catalogs
and catalogs which can be updated
.
When clicking on the button PARTadmin opens in the category Catalog update -> Online.
Detailed information on the Catalog update can be found under Section 1.3.4, “ Catalog update ”.
When clicking on the button PARTadmin opens in the category Catalog update -> Online.
Detailed information on the Catalog update can be found under Section 1.3.4, “ Catalog update ”.
If the option PARTupdate automatically start with Windows? had been activated in the installation, the icon is automatically displayed.[a] |
|
[a] At the end of the installation the PARTupdate settings wizard is automatically launched. |
Otherwise you can launch PARTupdate via Start menu (Start -> All Programs -> CADENAS -> PARTsolutions -> PARTupdate) anytime.
At the very first start the PARTupdate settings wizard is automatically launched so that you can determine certain modalities here.
Context menu
commands on the icon or
.
-> The short info is displayed. The same can be reached by a double-click on the icon.
-> The PARTupdate settings wizard opens. Here you can change settings at a later time if needed.
-> PARTupdate is finished and the icon in the task bar is not displayed anymore. You can start PARTupdate at a later time via Start menu.