A newly created or changed table can only be saved and left, if Identification data have been given.
![]() |
Note |
---|---|
|
Details on single fields of the dialog box Identification data
The Standard name (NB) is composed of Standard number, Standard title and variable values, which are dynamically read from the table.
![]() |
Important |
---|---|
Please absolutely regard the guidelines under Section 7.12.7.3, “ Guideline for NB, SHORTNB, LINA definition and Identification type ”. |
NB='ISO xy Bolt $D.x$L.'
|
When loading a part, the (translated) term of Standard name (NB) is displayed in PARTdataManager in the title bar of 3D view.
Once opening the dialog box Identification data, the expression NB= '' is already set, however, can be inserted via button as well.
Insert IF function in conditions. For mode of operation see Section 7.8.11, “ Attribute algorithms ”.
Insert ELSEIF function in conditions. For mode of operation see Section 7.8.11, “ Attribute algorithms ”.
Via you can have the expression (syntactic) checked for correctness.
The BOM name (LINA) is also transferred to the CAD system when exporting a part and there, is displayed in the bom list.
![]() |
Important |
---|---|
Please absolutely regard the guidelines under Section 7.12.7.3, “ Guideline for NB, SHORTNB, LINA definition and Identification type ”. |
Your company / company name where model / table has been created.