Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Proceed as follows, in order to download a CAD model:
Make sure that you are in the dialog area 3D CAD CATALOGS. (Note only applies for B2B Portal.)
In the dialog area Download CAD models under Edit CAD formats -> Add CAD formats, select the desired CAD formats and the transfer mode into the CAD system. Detailed information on this can be found under Section 4.5, “How can I select a CAD format? | How can I define the transfer mode into the CAD system?”.
Now in the dialog area CAD model selection, click on .
-> The information dialog Generating CAD models opens.
As soon as the generation has completed you can download the CAD models in this window, or directly transfer to the CAD system or you will get informed by a note that the component was sent by e-mail.
You can close the window during the generation and select further CAD models because all generated CAD models are also available for download under Download CAD models.
Under Download CAD models, in the Actions column, the following links are displayed:
Detailed information about the individual modes you can find in the following subchapters.
Download: See Section 4.11.1, “How can I download the chosen CAD model and import it into the CAD system?”.
Direct integration: See Section 4.11.2, “How can I directly integrate the chosen CAD model into the CAD system? (PART2cad) ”.
E-mail delivery: See Section 4.11.3, “How can I send the chosen CAD model to my e-mail address and import it into the CAD system?”.