Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Show window 'project selection' at program start : Option field to show/hide part selection dialog areas of the PARTdataManager. By clicking on Part selection you show the respective dialog area in case the option is not activated.
Show bitmaps during selection of project: ...shows part bitmaps. Otherwise only neutral folders or symbols are used.
Show vector graphics in project selection : ...shows vector graphics of parts. Otherwise only folder or bolt symbols are used.
Show small logos in project selection
show company logos in favorites and links: ...shows the company logo (if available) of the respective catalog.
Do not show empty classifications: Classifications, whose projects were allocated, are not displayed in the directory tree
Selection with single click: Without this option the directories must be double-clicked to be opened.
Option activated: If standards ran out, were replaced or changed, the validity date is displayed.
Especially when Preview and Company logo are small it is helpful to move the mouse over the preview images in order to get an enlarged view via tooltip.
The feature is available both in the Details view in Part selection and in the Search dialog of the complex search.
If the option 3D Tooltip is enabled (see next item) then this option will not come into effect.
Also compare Navigation mittels Registerseiten "Kataloge", "Symbole", "Details" and Suchergebnisspalten - Reihenfolge und Sichtbarkeit.
In the project selection (or also in the dialog box Links) 3D Tooltips are available. Drawing the mouse over a 3D preview image, the tooltip is displayed. In the down right corner, this has an icon, where you can draw up the size.
Show extended project and catalog information
You can display catalog and project data directly in the part selection on directory and project level at the bottom right.
In the Links dialog similar parts are shown. Determine which classification should underlie during the comparison.
Max. search results: ...restricts the number of search results to the value set here.
Font for project selection: Via Browse the menu to select the font for the Part selection opens.
Project filter: Set up a filter [111],with which you can reduce the selection of projects.
[111] This filter is defined in PARTproject. See Section 4.7.2.1.14.7, “ Check out catalog ” in eCATALOGsolutions Manual.