Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
If colors have been used in catalogs for the part depiction, the Color search can be used, either as only search method or in combination with other methods in order to enhance the result quality.
The Color search contains two options: You can determine colors via color palette or load a picture, where the relevant colors are automatically scanned from. In the case of complicated dye distribution using an image file is advantageous.
In the following both options are described with the help of an example part:
Select the Colors tabbed page.
The "Edit" button is only displayed in Admin mode. On this see under Section 1.1.7.5.3.5, “ Define search template ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.
Select the desired color or color combination in the displayed list of the History section or select the desired color in the color range. (Multiple selection with Ctrl key).
If you cannot find an appropriate color click on Add color and determine the adequate color in the color picking dialog box.
In the case of our example file you would simply choose red.
Adjust the minimum similarity, meaning how exact the level of color matching shall be. Parts which do not meet the condition are not regarded.
Select image for color comparison:
In the case of complicated dye distribution using an image file is advantageous.
|
The color search can also be used for own part catalogs.
Sketch search (2D) with colors
The Sketch search (2D) can also use colors (see Section 3.1.1.6.4.5, “ Sketch search (2D) ”).