Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Note | |
---|---|
Via the Generate image data/preview images command two basic functions are available:
|
In the Part selection, a preview image is located in each catalog on catalog, directory and project level.
In the following the complete procedure for preview image creation is explained.
The function is located at project and directory level in PARTdataManager [117], as well as in PARTproject:
In the list field, select the desired format. You have three formats available for creating a preview image:
If under Format the option BMP is selected, after confirming the selection by clicking , the dialog box Export in BMP format opens.
A detailed description of the settings can be found under Section 3.1.2.1.2.4.1, “BMP GIF JPEG PNG TIFF ”.
If under Format the selection Maxwell Render is made, after confirming the settings by clicking on , the dialog box Export Maxwell Render format opens.
A detailed description of the settings is found under Section 3.1.2.1.2.4.3, “Maxwell Render 3D ”. If under Render the selection Transfer to server is made, then the generation is running, supported by the module PARTrenderManager, which is also described in this section.
Create your preview images in high quality with POV-Ray Rendering.
If under Format the selection POV-Ray is made, after confirming the settings by clicking on , the dialog box Export in POV-Ray format opens.
A detailed description of the settings can be found under Section 3.1.2.1.2.4.4, “POV-Ray 3D ”.
From the list field, select whether the batch run is to access project or directory level or both.
View: In the list field select the desired perspective for the preview images.
All parts are oriented to the X axis with their longest side. If there are two "longest" sides, then one side is randomly selected.
With the help of the option Export files project files can be exported in a certain file format (CAD specific, image format, etc.) via batch run.
In the following the setting options are explained in detail:
Select the desired format in the list field. (At certain formats the format can be specified via Version).
All native and neutral formats, image formats and special formats are available: Compare selectable formats in PARTdataManager, Export menu.
Detailed information on export formats is found under Section 3.1.2.1.2, “ Export to CAD systems without PARTsolutions interface - Export in file ”.
Select a background from the list field for the preview image.
Among others, you have the following available: 8.1, 9.0, Purist, blank, Metal, Wood and backgrounds close to the CAD system.
When the option Export mode, Export files is selected, then this setting is inactive.
View: In the list field select the desired perspective for the preview images.
Determine a target directory for the export files via browse button .
You can include subdirectories for the generation of the export files optionally.
Process only one row per project:
Limit the read table lines to one characteristic per project file.
Project files with value ranges can be splitted by the declaration of a Stepping width. If this option is deactivated, only the currently set value (meaning one characteristic) is read.
Select the desired option for the naming convention in the list field.
The file name of the export file is composed according to the defined syntax. You can find some examples in the list field:
E.g. Standard name NB, followed by VIEWNAME (e.g. Front view) and the file extension SUFFIX. Of course you can adjust this composition according to your preferences.
When all settings are made, then click on .
When all settings are made, click on .
[116] Under PARTsolutions V8.1, the command was called "Use view as preview image".
[117] Only in developer mode. You can find detailed information on mode setting under Section 1.1.7.5.3.4, “User mode ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.