powered by CADENAS

Manual

Manual

3.1.14.4.3.  Report management... - Call up created reports later
Labeling of directories, projects and table lines / call up created reports

Reports are marked by a special icon :

  • In index tree

    When moving the mouse over the icon, a tooltip with already available reports is displayed.

    When moving the mouse over the icon, a tooltip with already available reports is displayed.

  • In the table (if the report only concerns a special line; this is only the case at the search for unmachined part.

    Table with report icon

    Table with report icon

When clicking on the icon the respective report opens. If there is more than one available, a dialog box opens where you can select the desired report (see Section 3.1.14.4.3, “ Report management... - Call up created reports later ”).

Call up created reports later

Created reports are saved and can be called up anytime later via:

  • Extras menu -> desired type of report -> Report management...

  • Context menu of a directory -> desired type of report -> Report management...

The dialog box Generated reports opens.

If a report had been created based on a line (Search for unmachined parts), then the standard name (NB) is displayed, otherwise the standard text (NT).

If a report had been created based on a line (Search for unmachined parts), then the standard name (NB) is displayed, otherwise the standard text (NT).

Select the desired report.

Afterwards the following functions are available:

Button Function
Display The report is opened.
Delete The report is deleted.
Open report folder

The respective directory under $CADENAS_DATA\shared\reports\Analyses\ is opened.

Select index directory The directory where the report is based on, is marked in the index tree.
Import report...

Communicate cross-departmental. Simply import other's reports.

An Explorer window opens. Select the report to import.

On this also see the function Search part... under Section 3.1.14.1.11, “Buttons ”.

Close The dialog box is closed.