powered by CADENAS

Manual

Manual

3.1.6.8.1. Docking window "Details"

Catalog or project information is displayed on the tabbed page Part selection, in the docking window Details by default.

"Details" Docking window

"Details" Docking window

  • On catalog and directory level, general catalog information is displayed:

    • Last change

    • Categories

    • Languages

    • Branch offices

      At catalogs with worldwide branch offices countries and locations are selectable via list field (if provided).

  • On project level additional information is displayed:

    • Description

    • Unit

    • Last change

    • Expiration date

      (if set by catalog supplier)

    • Classifications

      If several classifications are available they can be selected via list field.

  • On all levels the TagCloud is displayed.

    Die TagCloud contains the most frequent catalog terms of selected project or directory. When clicking on a term a full-text search is performed. If an ERP integration is available the link database is searched through in addition.

    By default the first 20 terms of the TagCloud with at least 3 characters are displayed.[66]



[66] Adjustable via configuration file. See Section 1.7.4.7.6, “ Block [InfoPane] - TagCloud ” in PARTsolutions / PARTcommunity4Enterprise - Administration Manual.