Our 3D CAD supplier models have been moved to 3Dfindit.com, the new visual search engine for 3D CAD, CAE & BIM models.
You can log in there with your existing account of this site.
The content remains free of charge.
Settings for subdirectories (without specified projects) is also possible.
Once a project within the given path is opened, the respective message is displayed.
In this way the administration or standardization department can block catalog subtrees for a specific reason or provide certain information (given in the key INFOTEXT).
As section name, insert the complete path, beginning with the catalog, down to the desired directory.
[norm/ansi/inch/bolts/binding_screws] ALLOW_OLD=0 CREATENR_OLD=0 EXPORT_OLD=0 INFOTEXT=This folder is not used at our company. If you need those files please contact name@yourCompany.de [_geom_search_imported_02_] ALLOW_OLD=1 CREATENR_OLD=0 EXPORT_OLD=1 INFOTEXT=This catalog should not been used. Please try to avoid using it. If you need those files please contact name@yourCompany.de [norm] INFOTEXT=This catalog is nice!
ALLOW_OLD = (Value range 0 or 1)
0: All parts within the set path are displayed with the icon (if under TREEICONS the value '1' is set [see Section 1.7.3.3.1, “General settings”]).
When opening the part, the following message is displayed:
This part is marked as 'replaced' and 'locked' and will not be opened.
1: When opening the part the following message is displayed:
This part is marked as 'replaced'. Part will still be opened.
CREATENR_OLD = (Value range 0 or 1)
If set on 1, the button Add dataset to link database is grayed out.
INFOTEXT: Below the standard message that text appears, which you inserted under INFOTEXT. Compare Fig. „Example: ALLOW_OLD=0“.